ROHM at electronica 2024
12.-15. November

ROHM at electronica 2024
As the world's leading trade fair for the electronics industry, electronica has taken up the cause of being the place where the All Electric Society will gather in 2024. ROHM Semiconductor will once more be among the exhibitors in Munich in November shaping a sustainable, livable future. In continuation of our motto “empowering growth, inspiring innovation” ROHM will present a portfolio designed to meet the evolving needs of various sectors. Visit us at Booth 520 in Hall C3 to explore how our high-quality semiconductor technologies are driving sustainability and innovation. From November 12th to 15th our international team will showcase state-of-the-art solutions for the big challenges of our time - such as decarbonization and the optimization of energy efficiency. See you in Munich!

“Our goal is to provide electronic solutions for the future and support our customers as a competent partner and consultant. Apart from technical support, for example, via our European Power Lab or QA Center, personal exchange with our partners is key. Electronica is a great opportunity to deepen personal contacts and listen carefully to our customers´needs. Intensive exchange is the basis for developing customised solutions ”
Wolfram Harnack,
President ROHM Semiconductor Europe

E-powertrain
ROHM will show a different applications example integrating ROHM TRCDRIVEpack™ .
TRCDRIVEpack™ is 2-in-1 SiC molded modules and optimized for xEVtraction inverters.
This supports up to 300kW and features high power density and a optimal terminal configuration.
More Detail

Off Board Charger
ROHM will show an application example with 1200V SiC Power Module adopted.
Discrete and module solutions support customers to choose out of ROHM's wide SiC portfolio, driving the expansion of EV charging applications.

ADAS & Zonal Computing
ROHM is showcasing newest generation SerDes for Camera Connectivity supporting up to 8MPix@30Hz resolution and plug-in platform board for ADAS SoC.

Power Conversion
ROHM's NEW EcoGaN™ Power stage ICs will be extended with higher integrated PFC & QR flyback converter ICs, providing an optimum solution for all electronics systems that requires high power density and efficiency.
New discrete packages like TOLL and top side colling (TOLT) for GaN HEMTs and new developed GaN Controller such as Totem Pole PFC and LLC, support compact ACDC power supply applications.

Lighting
Digital Cockpit
Showcasing Dual Display control for super high-resolution digital cockpit is supporting freeform super-frame, OSD and ASIL-B support.
Local Dimming for very high contrast and brightness displays are supported by direct LED drivers with highest power density. Exterior Lighting platform includes Boost, Buck and Linear LED Drivers as well as Motor Drivers for high power lamps with pixel animation and leveling or ADB.

Motor & Pump solution
ROHM will show a Motor Driver Technology demo including BD64701.
This products supports FOC control for high speed rotation and smooth sine wave.
and also BD67871 is involved into this demo and this product supports TriC3™ patented technology that is improving efficiency compared to standard constant current drive.

PV & Heatpump
ROHM has extended its 4G SiC-MOSFET lineup, to suit the needs of every design.
ROHM will show a success story of industry cooperation in PV space with SMA, Semikron Danfoss and Vincotech.

Take your development project to the next level:
We are giving away 45 evaluation boards absolutely free at electronica 2024.
Which one is your favorite? You have 17 different options to choose from.
Sign up now & confirm the opt-in email for your chance to win (registration ends Oct. 31).
Lucky winners will be notified and can pick up their board at our electronica booth (hall C3, stand 520) or have it shipped directly to them.
| Category | EVK Name |
|---|---|
| ACDC | BM2P060MF-EVK-001 |
| ACDC | BM2P061MF-EVK-001 |
| ACDC | BM2SC121FP2-EVK-001 |
| ACDC | BM2SC123FP2-EVK-001 |
| DCDC | BD9A201FP4-EVK-001 |
| DCDC | BD9F500QUZ-EVK-001 |
| DCDC | BD9F800MUX-EVK-001 |
| DCDC | BD9G101G-EVK-101 |
| DCDC | BD9G201EFJ-EVK-001 |
| DCDC | BD9G341AEFJ-EVK-101 |
| DCDC | BD9G401EFJ-EVK-001 |
| DCDC | BD9G500EFJ-EVK-001 |
| DCDC | BD9E304FP4-EVK-001 |
| DCDC | BD9E304FP4-EVK-002 |
| DCDC | BD9E304FP4-EVK-003 |
| SiC | P04SCT4018KE-EVK-001 |
| SiC | P05SCT4018KR-EVK-001 |
You may to our booth (C3-520): Visit us!