Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
ROHM Launches 2-in-1 SiC Molded Module “DOT-247” Achieves high design flexibility and power density
September 16th, 2025
ROHM has developed the "DOT-247," a 2-in-1 SiC molded module (SCZ40xxDTx, SCZ40xxKTx), ideal for industrial applications such as PV inverters, UPS systems, and semiconductor relays. The module retains the versatility of the widely adopted "TO-247" package while achieving high design flexibility and power density.
The DOT-247 features a combined structure consisting of two TO-247 packages. This design enables the use of large chips, which were structurally difficult to accommodate in the TO-247 package, and achieves low on-resistance through an unique internal structure. Additionally, through optimized package structure, thermal resistance has been reduced by approximately 15% and inductance by approximately 50% compared to the TO-247. This enables a power density 2.3 times higher than the TO-247 in a half-bridge configuration –achieving the same power conversion circuit in approximately half the volume.
The new products featuring the DOT-247 package are available in two topologies: half-bridge and common-source. Currently, two-level inverters are the mainstream in PV inverters, but there is growing demand for multi-level circuits such as three-level NPC, three-level T-NPC, and five-level ANPC to meet the need for higher voltages. In the switching sections of these circuits, topologies such as half-bridge and common-source are mixed –making custom products necessary in many cases when using conventional SiC modules.
To address this challenge, ROHM has developed each of these two topologies—the smallest building blocks of multi-level circuits—into a 2-in-1 module. This enables flexibility to support various configurations such as NPC circuits and DC-DC converters, while significantly reducing the number of components and mounting area, and achieving circuit miniaturization compared to discrete components.
Evaluation boards will also be made available progressively to facilitate evaluation during application design. For more information, please contact a sales representative or visit the contact page on ROHM’s website.
☆:Under Development
AEC-Q101 is an automotive electronics reliability standard established by the Automotive Electronics Council (AEC). The Q101 standard is specifically focused on discrete semiconductor components.
Application Examples
PV inverters, semiconductor relays, UPS (uninterruptible power supply), ePTO, and boost converters for FCVs (fuel cell vehicles).
AI servers (eFuse), EV charging stations, etc.
Sales Information
Pricing: $140/unit (samples, excluding tax)
Availability: ROHM construct mass production (September 2025)
Products compliant with the automotive reliability standard AEC-Q101 are scheduled to begin sample shipments in October 2025.
Comprehensive Support
ROHM is committed to providing application-level support, including the use of in-house motor testing equipment. A variety of supporting materials are also offered, such as simulations and thermal designs that enable quick evaluation and adoption of DOT-247 products. An evaluation kit for double-pulse testing is already available, allowing immediate testing, while an evaluation kit for 3-phase inverters is currently under preparation, with reference designs scheduled to be released from November 2025.
• About the DOT-247 design models
SPICE models: Available on the product web pages for each part number
LTspice® models: Scheduled to be available for three-level NPC from October 2025 on the web pages
LTspice® is a registered trademark of Analog Devices, Inc.
When using third-party trademarks, please adhere to the usage guidelines specified by the rights holder.
EcoSiC™ is a brand of devices that utilize silicon carbide (SiC), which is attracting attention in the power device field for performance that surpasses silicon (Si). ROHM independently develops technologies essential for the evolution of SiC, from wafer fabrication and production processes to packaging, and quality control methods. At the same time, we have established an integrated production system throughout the manufacturing process, solidifying our position as a leading SiC supplier.
• EcoSiC™ is a trademark or registered trademark of ROHM Co., Ltd.
Terminology
Half-bridge/ Common-source
A basic configuration of a power conversion circuit consisting of two MOSFETs. In a half-bridge configuration, the MOSFETs are connected in series, one above the other, and the output is taken from the connection point. By switching the upper and lower MOSFETs alternately, the output voltage can be switched between positive and negative, making this configuration widely used as the basic structure for high-efficiency power conversion in inverters and motor drive circuits.
Common Source is a configuration where the source terminals of the two MOSFETs are connected, and the output is taken from each drain. By grouping the source terminals, the gate drive circuit can be simplified, making it suitable for applications such as multilevel inverters.
Types of NPC-type multi-level circuits
NPC (Neutral Point Clamped) is a multi-level circuit configuration that divides the output voltage into three levels (+, 0, and -) to reduce voltage stress on the switching devices. The "0V" state is created by the neutral point, which is the contact point located between the positive and negative voltages.
T-NPC (T-type NPC) replaces the diode used to stabilize the neutral point with switching devices such as MOSFETs, enabling more efficient operation. ANPC (Active NPC) actively controls the potential of the neutral point itself using a switch, achieving smoother output waveforms and high-precision power conversion. T-NPC and ANPC are suitable for applications requiring higher output and efficiency.
ePTO (electric Power Take-Off)
A system that uses the power from an electric vehicle's motor or battery to drive external work machinery or equipment (such as hydraulic pumps or compressors). This is an electrified version of the PTO (Power Take-Off) used in conventional engine vehicles, and its adoption is advancing in environmentally friendly commercial vehicles and work vehicles.
ROHM Launches 2-in-1 SiC Molded Module “DOT-247”
Achieves high design flexibility and power density
September 16th, 2025
ROHM has developed the "DOT-247," a 2-in-1 SiC molded module (SCZ40xxDTx, SCZ40xxKTx), ideal for industrial applications such as PV inverters, UPS systems, and semiconductor relays. The module retains the versatility of the widely adopted "TO-247" package while achieving high design flexibility and power density.
The DOT-247 features a combined structure consisting of two TO-247 packages. This design enables the use of large chips, which were structurally difficult to accommodate in the TO-247 package, and achieves low on-resistance through an unique internal structure. Additionally, through optimized package structure, thermal resistance has been reduced by approximately 15% and inductance by approximately 50% compared to the TO-247. This enables a power density 2.3 times higher than the TO-247 in a half-bridge configuration –achieving the same power conversion circuit in approximately half the volume.
The new products featuring the DOT-247 package are available in two topologies: half-bridge and common-source. Currently, two-level inverters are the mainstream in PV inverters, but there is growing demand for multi-level circuits such as three-level NPC, three-level T-NPC, and five-level ANPC to meet the need for higher voltages. In the switching sections of these circuits, topologies such as half-bridge and common-source are mixed –making custom products necessary in many cases when using conventional SiC modules.
To address this challenge, ROHM has developed each of these two topologies—the smallest building blocks of multi-level circuits—into a 2-in-1 module. This enables flexibility to support various configurations such as NPC circuits and DC-DC converters, while significantly reducing the number of components and mounting area, and achieving circuit miniaturization compared to discrete components.
Evaluation boards will also be made available progressively to facilitate evaluation during application design. For more information, please contact a sales representative or visit the contact page on ROHM’s website.
Product Lineup
Sheet
(Tj=25°C)
Diagram
Qualified
[V]
[mΩ]
[A]
DOT-247-7L
[41.0mm × 31.5mm × 5.0mm]
☆:Under Development
AEC-Q101 is an automotive electronics reliability standard established by the Automotive Electronics Council (AEC).
The Q101 standard is specifically focused on discrete semiconductor components.
Application Examples
PV inverters, semiconductor relays, UPS (uninterruptible power supply), ePTO, and boost converters for FCVs (fuel cell vehicles).
AI servers (eFuse), EV charging stations, etc.
Sales Information
Pricing: $140/unit (samples, excluding tax)
Availability: ROHM construct mass production (September 2025)
Products compliant with the automotive reliability standard AEC-Q101 are scheduled to begin sample shipments in October 2025.
Comprehensive Support
ROHM is committed to providing application-level support, including the use of in-house motor testing equipment. A variety of supporting materials are also offered, such as simulations and thermal designs that enable quick evaluation and adoption of DOT-247 products. An evaluation kit for double-pulse testing is already available, allowing immediate testing, while an evaluation kit for 3-phase inverters is currently under preparation, with reference designs scheduled to be released from November 2025.
• About the DOT-247 design models
SPICE models: Available on the product web pages for each part number
LTspice® models: Scheduled to be available for three-level NPC from October 2025 on the web pages
LTspice® is a registered trademark of Analog Devices, Inc.
When using third-party trademarks, please adhere to the usage guidelines specified by the rights holder.
For details, please contact a sales representative or visit the contact page on ROHM’s website.
EcoSiC™ Brand
EcoSiC™ is a brand of devices that utilize silicon carbide (SiC), which is attracting attention in the power device field for performance that surpasses silicon (Si). ROHM independently develops technologies essential for the evolution of SiC, from wafer fabrication and production processes to packaging, and quality control methods. At the same time, we have established an integrated production system throughout the manufacturing process, solidifying our position as a leading SiC supplier.
• EcoSiC™ is a trademark or registered trademark of ROHM Co., Ltd.
Terminology
Common Source is a configuration where the source terminals of the two MOSFETs are connected, and the output is taken from each drain. By grouping the source terminals, the gate drive circuit can be simplified, making it suitable for applications such as multilevel inverters.
T-NPC (T-type NPC) replaces the diode used to stabilize the neutral point with switching devices such as MOSFETs, enabling more efficient operation. ANPC (Active NPC) actively controls the potential of the neutral point itself using a switch, achieving smoother output waveforms and high-precision power conversion. T-NPC and ANPC are suitable for applications requiring higher output and efficiency.
Featured Products
2-in-1 SiC Molded Modules
DOT-247
SCZ40xx series (PDF:1.3MB)
Video
Latest News