Monitor equipment with AI on a single chip Solist-AI™ Fully Autonomous AI Solution for Edge Computing
Monitor equipment with AI on a single chip
Solist-AI™ Fully Autonomous AI Solution for Edge Computing
- Solist-AI™ is the brand name for ROHM's on-device AI solution designed for edge computing applications. This innovative solution enables real-time learning and inference directly on standalone edge devices without relying on cloud servers. Solist-AI™ contributes to the expansion of sustainable AI innovation.
Features of Solist-AI™
ROHM’s Solist-AI™ solution brings AI-driven capabilities such as condition monitoring and degradation prediction to a wide range of edge computing devices. On-site learning in standalone operation is supported, allowing systems to be easily deployed by simply connecting sensors - even in environments without network connectivity.
In this demo video, the AI learns the fan’s outlet states (open/blocked) on site and detects anomalies during Monitoring (Inference). Status is indicated by LEDs (orange = learning (blinking), green = monitoring (on), yellow = anomaly (on)).
Comparison Between Conventional Solutions and Solist-AI™
Technology
Overview
At the core of the Solist-AI™ is the Solist-AI™ MCU, which incorporates ROHM’s proprietary AI processing hardware accelerator AxlCORE-ODL, complemented by dedicated utility software that streamlines implementation.
Features of Solist-AI™ Microcontroller
Solist-AI™ offers key capabilities such as standalone AI operation, on-device and incremental learning, and concurrent execution of non-AI processes, all made possible by the Solist-AI™ microcontroller equipped with the AxlCORE-ODL accelerator.
Development Environment & Utility Software
Solist-AI™ provides an integrated development environment, driver software, and evaluation boards to enable immediate software development. In addition, utility tools required for AI operation analysis are available on the web.
Ecosystem
The Solist-AI™ solution is a collaborative effort between ROHM and a network of ecosystem partners. We provide comprehensive support from hardware and software development to the design and provision of foundational infrastructure, allowing customers to implement the solution immediately.
To further advance AI innovation through Solist-AI™, we are actively expanding our ecosystem and welcome inquiries from prospective partners. Please don't hesitate to contact us if interested.
Use Cases
Solist-AI™ Use Case 1: Predictive Maintenance
Detecting Motor Bearing Damage: Utilized in condition-based monitoring (CBM) to enable predictive maintenance of production equipment/machinery
This includes various peripheral drivers, AI libraries, and other resources for the Solist-AI™ MCU.
Background and Challenges
- Predictive maintenance is required to detect anomalies and potential failures in production equipment and machinery before they occur
- A shortage of skilled personnel (experienced engineers) capable of performing regular inspections remains a significant challenge
Uses of Solist-AI™
- During initial equipment installation, on-site learning is conducted using accelerometers to capture vibration data under constant-speed operation, establishing a reference profile for normal conditions.
- The vibration state during normal operation is continuously compared to the learned baseline data, and when deviations beyond a certain threshold are detected, the system issues an alert indicating a potential anomaly (= 'different from usual').
Expected Benefits
- Leverage AI to detect ‘different than usual’ at an early stage and facilitate root cause analysis
⇒ Helps prevent unexpected equipment repairs/replacements as well as both minor and major unplanned downtimes - Shift from manual TBM to AI-driven CBM
⇒Significantly reduces overall maintenance costs
*The above is one example of predictive maintenance. Applicability extends beyond motor systems to various other types of systems as well.
Solist-AI™ Use Case 2: Condition/Degradation/Parameter Prediction
Battery Degradation Prediction/Condition Change Detection: Used to forecast future indicators of product degradation and estimate parameters that cannot normally be measured
Background and Challenges
- Customers operate battery-powered devices under a wide range of scenarios
- The inability to track degradation of the battery’s full charge capacity imposes limitations on how devices can be used
Uses of Solist-AI™
- Standard degradation profiles (SOH) are pre-trained prior to shipment. Supplementing the model with real-world usage data (SOH) enables high accuracy prediction of battery degradation
- The standard charge/discharge characteristics of each battery cell are pre-learned before shipment. Additional learning is performed during actual use to detect changes in condition, taking individual cell variations into account.
Expected Benefits
- Learn customer-specific usage patterns and environmental conditions
⇒Predict future degradation to extend the operational lifespan - Incorporate cell-to-cell variations into the learning process
⇒Enable early detection of charge capacity loss, imbalance anomalies, and condition changes
*This example illustrates a use case in condition/degradation prediction, which can be extended beyond battery systems to various other applications.
Solist-AI™ Use Case Portfolio
Beyond use cases like motor anomaly detection and battery degradation, we have compiled comprehensive documentation covering a broad spectrum of implementation examples spanning industrial equipment, electrical devices, and production systems. Please refer to this as a resource when evaluating and implementing Solist-AI™.
Solist-AI™ Solution Overview Materials
A full set of support materials is available. Please refer to them when considering our products.
Contact Us / Join Solist-AI™ Ecosystem
We welcome companies that share our vision for the Solist-AI™ ecosystem and aspire to drive technological innovation together. Will you join us as a Solist-AI™ ecosystem partner and create new value side by side?
Note: Solist-AI™ is a trademark or registered trademark of ROHM Co., Ltd.