ROHM News Detail

New EMARMOUR™ 2 Channel High-Speed Op Amp

December 17th, 2020

BD77502FVM | MSOP8 Package

ROHM introduces the availability of a 2 channel high-speed ground sense CMOS op amp, BD77502FVM, optimized for consumer and industrial equipment requiring high-speed sensing – such as industrial measurement and control systems.

The proliferation of the Internet of Things (IoT) in recent years has led to a significant increase in the number of electronic components used for advanced control in a variety of applications. This trend towards greater electronics density is leading to noisier environments, making it extremely difficult to implement designs with electromagnetic compatibility (EMC). Op amps play a critical point role because they quickly amplify small signals (from sensors) in many detection systems that provide safety. In addition, printed circuit board design can also be problematic for conventional op amps that are susceptible to oscillation due to capacitive loads (i.e. from wiring).

To mitigate noise issues common with conventional op amps, ROHM has developed the EMARMOUR™ series featuring superior noise tolerant op amps. The first groundbreaking member of the EMARMOUR family was the BD77501G single channel high-speed CMOS op amp that leveraged the original Nano Cap™ technology to prevent oscillation caused by load capacitance. This product has been well-received by many engineers in a variety of fields and regions, and our latest 2 channel version was developed to meet increasing market demands.

The newest BD77502FVM integrates two op amp devices that prevent oscillation (i.e. due to wiring) while providing high-speed amplification with slew rates up to 10V/µs and breakthrough immunity to electromagnetic interference (EMI). The output voltage across the entire noise frequency band is limited to under ±20mV, which is 10x lower than a conventional op amp. High-speed signal amplification is now achievable without being affected by external noise or load capacitance when used in devices that output small signals such as sensors, thus improving reliability while simplifying circuit designs.

ROHM's EMARMOUR™ Series Achieves Breakthrough Noise Immunity High-Speed Op Amp Utilizes Original Ultra-Stable Control Technology to Prevent Oscillation EMARMOUR™ Brand Logo

What is EMARMOUR™?

EMARMOUR™ is ROHM’s unique brand to identify its products that leverage proprietary technologies covering layout, processes, and circuit design to achieve ultra-high noise immunity. This technology limits output voltage fluctuation to less than ±300mV across the entire noise frequency band during noise evaluation testing under the international ISO11452-2 standard. This unprecedented noise immunity reduces design resources while improving reliability by solving issues related to noise in the development of a variety of systems.

Impact of EMARMOUR™ on Design and Development Load

Key Features

The BD77502FVM, which expands the EMARMOUR™ lineup that delivers unmatched noise tolerance, builds upon the 1ch ground sense CMOS op amp BD77501G widely adopted in the industrial equipment market by offering high-speed operation and preventing oscillation due to load capacitance. And in addition to the following features, the 2ch design supports market demands for more compact board designs.

1. No oscillation and high-speed op amps that minimizes design time related to load capacitance
Original Nano Cap™ power supply technology is used to achieve extremely stable control, making it possible to completely eliminate oscillation caused by load capacitance (i.e. due to wiring) while supporting high-speed amplification (high slew rate: 10V/µs) required in anomaly detection and other systems. Unlike standard op amps that can be difficult to use due to restrictions imposed on the wiring and peripheral components resulting from instability caused by load capacitance, ROHM’s new op amp prevents oscillation to ensure stable operation and facilitate application design.

 

2. Superior noise immunity facilitates noise design requirements (EMARMOUR™ exclusive)

Achieves Superior Noise Immunity

Whereas the output voltage of conventional products can fluctuate by ±200mV or more across the entire noise frequency band, ROHM’s latest EMARMOUR™ series op amp achieves unprecedented noise immunity that limits variation to less than ±20mV. This eliminates the need for countermeasures (filter circuits) for each noise frequency, reducing the noise design resources for sensors (which play an important role in a variety of systems) while improving system reliability.

 

3. Eliminates 16 parts required for noise suppression (EMARMOUR™ exclusive)
The BD77502FVM provides superior noise immunity that eliminates the need for external noise countermeasure components conventionally required for standard products (i.e. RC filters for the power supply, input, and output pins). For example, in the case of a 2ch op amp, ROHM’s new product uses 16 fewer external components than conventional solutions.

Comparison of External Parts for Noise (2ch Op Amp)

Application Examples

 
  • Facility management equipment such as abnormal current and gas detectors
  • Motors requiring high-speed control (signal transmission)
  • Inverter control equipment
  • Pre-drive buffers for driving transistors
 

...and other industrial and consumer applications requiring high-speed signal transmission and amplification without worrying about load capacitance.

EMARMOUR™ CMOS Op Amp Lineup

 
Part No.No. of CircuitsMax. Operating Voltage (V)Input Offset Voltage (mV) (Typ.)Bias Current (nA)Slew Rate (V/µs) (Typ.)Circuit Current (mA) (Typ.)Nano Cap™
Technology (Stable Output)
Package
BD77501G1ch1540.00110.01.3✓SSOP5
BD77502FVMNEW2ch2.6✓MSOP8
BD87581YG-C1ch1413.52.3—SSOP5
BD87582YFVM-C2ch5.0—MSOP8
 

Pricing: From 0.61USD/unit (samples, excluding tax)

Availability: In mass production

What is Nano Cap™?

Nano Cap™ refers to extremely stable control technology achieved by combining advanced analog expertise covering circuit design, processes, and layout utilizing ROHM’s vertically integrated production system. Stable control eliminates the problem of unstable operation related to capacitors in analog circuits, contributing to a reduction in design resources for a wide range of applications in the automotive, industrial equipment, consumer, and other fields.

Terminology

Op Amps

Op amps (operational amplifiers) are designed to amplify input signals. They are typically used to amplify minute signals, such as those output from sensors, to a voltage level that can be recognized by an MCU.

Comparators, which are often introduced with op amps, are commonly employed to determine the threshold value of input signals. They output a High/Low signal after performing threshold judgment of the sensor output signal.

The ROle of Op Amps/Comparators

EMI (Electromagnetic Interference)

EMI immunity is a parameter indicating the degree of tolerance to ambient noise. Noise generated in the environment can cause malfunction in systems with low EMI immunity, making it necessary to take protective measures such as incorporating filters (i.e. resistors/capacitors) or shields (metal plates). In contrast, high EMI immunity ensures stable operation without worrying about the effects of noise, providing a significant advantage by virtually eliminating the design resources for noise countermeasures.

*Nano Cap™ and EMARMOUR™ are trademarks or registered trademarks of ROHM Co., Ltd.