ROHM News Detail

ROHM Launches 600V Super Junction MOSFETs in Surface-Mount Package with High Thermal Performance

*ROHM July 9th, 2026 study

DFN8080-5L/TOLL Package

ROHM has developed a new lineup of 600V Super Junction MOSFETs, the R60xxXNx and R60xxWNx series.

In the data center and industrial equipment fields, power demand continues to increase as processing loads grow, driving strong demand for higher power supply efficiency to reduce both power consumption and heat generation. At the same time, as applications become smaller, power supply circuits must achieve higher power density and space savings while delivering higher output within limited space.

To meet these requirements, Super Junction MOSFETs must deliver even lower loss and improved thermal performance, driving the rising adoption of surface-mount packages with excellent heat dissipation. In addition, from the perspective of reducing procurement risk, support for multi-sourcing and securing second sources have become essential in recent years, making high compatibility with existing standard products an important requirement.

The new products - R60xxXNx series and PrestoMOS™ R60xxWNx series - add surface-mount DFN8080-5L (8.0 × 8.0 × 0.85mm) and TOLL (11.68 × 9.9 × 2.3mm) packages to the existing package lineup. With compact, low-profile designs and excellent heat dissipation, these packages are ideal for applications that require space savings and higher power density, including power supplies for AI servers and industrial equipment.

In terms of characteristics, the gate threshold voltage (VGS(th)) required to turn on the MOSFET is set to a 3V to 5V range widely used in standard products, supporting a broad range of drive conditions. In addition, improved admittance characteristics deliver greater versatility and lower loss, compared with conventional R60xxYNx series and PrestoMOS™ R60xxVNx series. Surface-mount packages having market common footprint ensure excellent versatility while making it easier to consider replacement in existing power supply circuits and select second sources.

The lineup consists of 21 models in the high-speed switching R60xxXNx series and 11 models in the PrestoMOS™ R60xxWNx series that offers class-leading* high-speed recovery characteristics. Users can select the optimal product according to their application needs, from products suited for designs prioritizing compatibility to those suited for designs emphasizing lower loss.

Mass production began sequentially in June 2026 (sample price: $7.0/unit, excluding tax). Online sales have also started with TOLL package products (Applicable Part No: R6020XNJ2, R6038XNJ2, R6049XNJ2, R6055XNJ2, R6024WNJ2, R6035WNJ2), which are available through online distributors such as DigiKey.

Online Distributors

ROHM will continue to expand its Super Junction MOSFET lineup, with plans to begin mass production of 650V products and next-generation products as well.

Product Lineup

VDSS
[V]
Series RDS(ON)
(Max.)
[mΩ]
Package
DFN8080-5L Data
Sheet
TOLL Data
Sheet
TO-220AB Data
Sheet
TO-220FM Data
Sheet
TO-247 Data
Sheet
600 R60xxXNx 185 New R6020XNJ3 PDF New R6020XNJ2 PDF New R6020XNX PDF
165 New R6022XNJ3 PDF ☆R6022XNJ2 -
135 New R6027XNJ3 PDF New R6027XNX PDF
96 New R6038XNJ3 PDF New R6038XNJ2 PDF New R6038XNX3 PDF New R6038XNX PDF New R6038XNZ4 PDF
82 New R6049XNJ3 PDF New R6049XNJ2 PDF New R6049XNX PDF
69 New R6055XNJ2 PDF
60 New R6061XNJ3 PDF New R6061XNX PDF New R6061XNZ4 PDF
44 New R6086XNZ4 PDF
26 New R60A4XNZ4 PDF
R60xxWNx 204 ☆R6018WNJ2 -
153 New R6024WNJ3 PDF New R6024WNJ2 PDF
114 New R6035WNJ3 PDF New R6035WNJ2 PDF
74 ☆R6050WNJ2 -
73 New R6055WNJ3 PDF New R6055WNZ4 PDF
63 New R6059WNJ3 PDF
51 New R6077WNZ4 PDF
27 ☆R60A3WNZ4 -

☆ : Under Development

Application Examples

• Power supplies for AI servers and data centers
• Power supplies for industrial and consumer equipment (LLC, PFC, Flyback, etc.)
• Motors and inverters for fans, AC servos, and other applications

EcoMOS™ Brand

EcoMOS™ is ROHM's brand of silicon MOSFETs designed for energy-efficient applications in the power device sector.
Widely utilized in applications such as home appliances, industrial equipment, and automotive systems, EcoMOS™ provides a diverse lineup that enables product selection based on key parameters such as noise performance and switching characteristics to meet specific requirements.

EcoMOS™ Brand Logo

EcoMOS™ is a trademark or registered trademark of ROHM Co., Ltd.

PrestoMOS™

“Presto” is an Italian musical term meaning “very fast.”
PrestoMOS™ is ROHM’s original power MOSFET that maintains the high withstand voltage and low ON resistance of Super Junction MOSFETs while speeding up the reverse recovery time of the built-in diode. Reducing switching losses makes it ideal for a wider range of applications with inverter circuits, such as air conditioners and refrigerators.

*PrestoMOS™ is a trademark or registered trademark of ROHM Co., Ltd.

Terminology

Super Junction MOSFET (Metal Oxide Semiconductor Field Effect Transistor)
A type of transistor, high voltage MOSFETs can be divided by device structure into planar, and super junction topologies. Super Junction MOSFETs deliver superior breakdown voltage and output current than planar types, featuring lower loss when handling large power.
Admittance Characteristics
Characteristics indicating how easily current flows in response to the gate voltage input to a MOSFET. Improving these characteristics enhances responsiveness to gate control, reducing switching loss and improving versatility by supporting a wider range of circuit conditions.