ROHM's New High-Reliability 1608-Size White Chip LED

Contributes to the Long-Term Design Quality of Displays in Industrial and Consumer Applications

SMLD12WBN1W - ROHM's New High-Reliability 1608-Seiz White Chip LED

ROHM today announced the availability of the SMLD12WBN1W, a White chip LED with 1608 (1.6x0.8mm) size that achieves class-leading reliability. This new package offers superior mountability and long operational life, which makes it ideal for use in display panels (e.g. temperature control displays) in industrial and compact consumer equipment.

In recent years, the need to improve both design quality and visibility of industrial equipment has increased the use of White LEDs for numerical displays and visual indicators in these applications. High-reliability LEDs are required to guarantee no degradation in luminosity even with continuous operation for over 10 years. However, achieving this has not been possible until now due to the use of epoxy or silicone resins for molding of typical White chip LEDs. These types of material could not provide enough reliability to prevent degradation in luminosity or provide enough package strength to facilitate mounting on circuit boards.

ROHM has been providing 1608-size chip LEDs in colors ranging from Red to Green, and now it is adding White to this product range to meet market demand. The adoption of a new material that combines the benefits of epoxy and silicone resins made it possible to achieve class-leading reliability of White chip LED in such a small package.

ROHM’s tests have demonstrated that the SMLD12WBN1W maintained 100% of its luminosity after operating for 1,000 hours (@25°C, IF=20mA). This represents an improvement of 20x in operational life when compared to other similar products available in the market. Additional tests showed that the package strength was improved 25 times with the new material when compared to products using silicone resin. This will contribute to significantly reducing the occurrence of failures during fabrication when mounting on circuit boards.

ROHM is committed to continue developing highly reliable LEDs and to strengthen its product lineup while focusing on increasing usability.

SMLD12WBN1W Advantages

Availability: Now
Pricing: $0.41/pcs

Key Features

1. Successfully maintained 100% luminous intensity during operational testing (25°C, IF=20mA, 1,000hrs)

Energization Test Results

Traditionally, Red and Green LEDs used in display panels of industrial equipment are less prone to cause yellowing of the resin due to light energy. Therefore, luminosity degradation has not been regarded as a problem. Epoxy resins with high mold hardness are commonly adopted for compact molded type LEDs. However, in the case of LEDs with a short wavelength (λD<527nm) such as White, the resin may turn yellow due to the energy of the light.

To address this issue, the SMLD12WBN1W utilizes a new material for the sealing resin that maintains 100% luminosity during operational testing (25ºC, IF=20mA, 1,000hrs). This results in approx. 20x longer life when compared to the residual luminosity shown under the same conditions by similar products available in the market.

2. 25x higher package strength than those using silicone resin

Molded Strength Measurement Results

Although light intensity degradation can be improved by adopting silicone resin, the molding becomes easier to detach from the substrate. Measures to enhance mounting strength such as adding reflectors to compact LEDs cannot be used, and damage to the molding section remains a challenge.

The use of a new resin material improves the molding strength by 25x when compared to products using silicone resin even at high temperatures (Ta=150ºC). This minimizes defects during mounting on circuit boards, thus achieving superior mountability.

Lineup

 
Part No.Emitting ColorForward Voltage [VF]Dominant Wavelength [λD]BrightnessPackage Size
Typ. (V)IF(mA)Min. (nm)Typ. (nm)Max. (nm)IF(mA)Min. (mcd)Typ. (mcd)IF (mA)
SML-D12V8WRED2.220625630635201640201.6 X 0.8 mm
SML-D12U8W6156206252563
SML-D12D8WOrange60260560840100
SML-D12Y8WYellow5875905932563
SML-D12M8WYellow Green5695725751025
SML-D12P8WGreen5575605632.56.3
SML-D12EN1W3.055205275355561405
SMLD12E2N1WBlue Green2.9500505512120
SMLD12E3N1W49049650285
SMLD12BN1WBlue4654704751440
SMLD12WBN1WNEWWhite(x,y) (0.295, 0.280)56120