ROHM has developed the “AG16xFNxx Series,” a lineup of 80V power MOSFETs designed for 48V power supply systems, which are becoming increasingly common in automotive applications.
In the automotive sector, power demand is increasing, particularly in high-end vehicle models. 48V power supply systems are gaining attention as a highly efficient alternative to conventional 12V power supply systems. With widespread adoption expected around 2030, there is a growing need for 80V power MOSFETs that can achieve even lower power losses than standard 100V devices.
ROHM’s new products are expected to enable downsizing compared to standard automotive MOSFET packages such as the TO-252 (6.6 × 10.0mm) by adopting the HPLF5060 (4.9 × 6.0mm) and DFN3333 (3.3 × 3.3mm) packages.
The HPLF5060 features Gull-Wing Leads, while the DFN3333 features Wettable Flank Technology, contributing to improved reliability on PCBs (Printed Circuit Boards). Furthermore, by adopting Copper Clip Junction Technology to enhance heat dissipation, these devices are capable of handling high currents. All models comply with the automotive reliability standard AEC-Q101, ensuring high reliability.
Mass production of new products began in April 2026 for the AG160FNS4FRA (HPLF5060) and the AG166FNH7FRA (DFN3333) (sample price: $3.5/unit, excluding tax). Online sales have also started, and the products are also available for online purchase through online distributors such as DigiKey and Farnell.
The product lineup of these packages will be further expanded in the near future. In addition, development of TOLG (TO-Leaded with Gullwing, 9.9 × 11.7mm) packaged products has begun, with continued expansion of the lineup of high-power, high-reliability 80V MOSFETs.
ROHM Launches AG16xFNxx Series MOSFETs for Automotive 48V Power Supply Systems
ROHM has developed the “AG16xFNxx Series,” a lineup of 80V power MOSFETs designed for 48V power supply systems, which are becoming increasingly common in automotive applications.
In the automotive sector, power demand is increasing, particularly in high-end vehicle models. 48V power supply systems are gaining attention as a highly efficient alternative to conventional 12V power supply systems. With widespread adoption expected around 2030, there is a growing need for 80V power MOSFETs that can achieve even lower power losses than standard 100V devices.
ROHM’s new products are expected to enable downsizing compared to standard automotive MOSFET packages such as the TO-252 (6.6 × 10.0mm) by adopting the HPLF5060 (4.9 × 6.0mm) and DFN3333 (3.3 × 3.3mm) packages.
The HPLF5060 features Gull-Wing Leads, while the DFN3333 features Wettable Flank Technology, contributing to improved reliability on PCBs (Printed Circuit Boards). Furthermore, by adopting Copper Clip Junction Technology to enhance heat dissipation, these devices are capable of handling high currents. All models comply with the automotive reliability standard AEC-Q101, ensuring high reliability.
Mass production of new products began in April 2026 for the AG160FNS4FRA (HPLF5060) and the AG166FNH7FRA (DFN3333) (sample price: $3.5/unit, excluding tax). Online sales have also started, and the products are also available for online purchase through online distributors such as DigiKey and Farnell.
The product lineup of these packages will be further expanded in the near future. In addition, development of TOLG (TO-Leaded with Gullwing, 9.9 × 11.7mm) packaged products has begun, with continued expansion of the lineup of high-power, high-reliability 80V MOSFETs.
Online Distributors
Product Lineup
Sheet
[V]
[A]
(Max.)
(10V)
[mΩ]
(10V)
[nC]
[pF]
qualified
HPLF5060
DFN3333
☆ : Under Development
Application Examples
Automotive 48V systems: Main inverter control circuits, electric motors, electric water pumps, etc
EcoMOS™ Brand
EcoMOS™ is ROHM's brand of silicon power MOSFETs designed for energy-efficient applications in the power device sector.
Widely utilized in applications such as home appliances, industrial equipment, and automotive systems, EcoMOS™ provides a diverse lineup that enables product selection based on key parameters such as noise performance and switching characteristics to meet specific requirements.
・EcoMOS™ is a trademark or registered trademark of ROHM Co., Ltd.
Terminology
Latest News