common_css

ai-server_title

Special Dialogue: HVDC for AI servers

ir_navi

ai-server_main

Special Dialogue: HVDC for AI servers

With AI adoption accelerating worldwide, data center power consumption is surging at an unprecedented pace—triggering two acute challenges: a tightening power supply and growing difficulty delivering that power efficiently within the data center. To address both, Delta Electronics, Inc. (Delta) and ROHM have strengthened their collaboration. In this interview, Ares Chen, Vice President and General Manager of Delta’s Power and System Business Group, and Kazuhide Ino, Member of the Board and Senior Managing Executive Officer in charge of ROHM’s Power Devices Business, discuss the technologies shaping the next era of data center power.

Q: Why are data centers actively evaluating the adoption of high-voltage power transmission and delivery using HVDC (High Voltage Direct Current)?

Ares Chen

Chen

The primary driver is the rapid rise in GPU (Graphics Processing Unit) power consumption—the “brain” of AI servers—which is forcing a major step-up in the output power required from data center power racks (Figure 1).

 

For conventional CPU (Central Processing Unit) servers, a power rack output of roughly 10 kW was typically sufficient. But for AI server racks equipped with the latest GPUs require 120–130 kW of power. Looking further ahead, AI server racks built on next‑generation platforms are expected to demand 300 kW, 600 kW, or even 1 MW. In short, the required power rack output is poised to jump from 10 kW to 1 MW—a 100 times increase. Because electrical power is the product of voltage and current, maintaining the traditional 50 V DC supply while delivering 100 times more power would mean 100 times more current. That level of current makes copper cabling run dangerously hot—and in the worst case, could lead to cable failure. The practical solution is clear: increase voltage to reduce current. This is why HVDC is now being seriously considered.

Rapidly increasing data center power consumption
Figure 1 Rapidly increasing data center power consumption
Kazuhide Ino

Ino

The logic is straightforward: when transmitting large amounts of power, higher voltage is advantageous. The key question, however, is where the industry converges—1,000 V, 800 V, or 400 V. Ultimately, what matters is the de facto standard. Companies must accurately identify which voltage will become dominant and ensure they are aligned with that ecosystem.
Delta is a global leader in power systems and has close relationships with stakeholders who influence standard-setting, giving it strong visibility into the market’s direction. For ROHM, partnering with Delta helps ensure access to critical information related to standardization, an essential element of executing our strategy.

Also Looking Ahead to a Transition to “±800 VDC”

Q: Two architectures are currently being proposed—“800 VDC” and “±400 VDC.” Could you walk us through the advantages and disadvantages of each?

Chen

Certainly. There are three key perspectives to consider. First is the overall power-system configuration (Figure 2). An 800 VDC system is built around two power lines—+800 V and ground (GND)—which keeps the architecture relatively straightforward. In contrast, ±400 VDC requires three lines—+400 V, –400 V, and GND—making the configuration inherently more complex.

HVDC in data centers: Top= 800 VDC, Bottom= ±400 VDC system configuration
Figure 2 HVDC in data centers: Top= 800 VDC, Bottom= ±400 VDC system configuration

 

Second is safety. With 800 VDC, the potential difference relative to GND can reach 800 V. If a person were to come into contact with that voltage, the consequences could be extremely serious, which means the risk profile is higher. With ±400 VDC, by comparison, the maximum potential difference to GND is 400 V. Relative to 800 VDC, that reduces the hazard level and can be seen as offering a higher safety margin.
Third is the maturity and availability of components used across the power system. Next-generation architectures rely on devices such as GaN HEMTs and SiC MOSFETs. In particular, ±400 VDC can leverage certain Si-based power MOSFETs, whereas 800 VDC generally requires higher-voltage devices such as SiC power MOSFETs. As a result, it can be said that components applicable to ±400 VDC is currently more widely established.

Q: Which approach do you see as more promising—800 VDC or ±400 VDC?

Chen

From the standpoint of maximum potential difference, both ±400 VDC and 800 VDC have a maximum of 800 V, so the total power deliverable is effectively the same. That said, based on GPU trends, it is highly likely that 800 VDC will eventually reach its limit. When that happens, ±800 VDC becomes the next step—because it can double the power delivery compared with 800 VDC. We are not there yet: the component ecosystem for ±800 VDC is not fully established. But over time, we expect momentum to build in that direction.
A similar shift is already visible in EVs: battery systems once centered on 400 V are increasingly moving toward 800 V, primarily to enable faster charging. If 800 VDC becomes mainstream across both EVs and AI servers, the ecosystem will mature—and that progression can eventually pave the way for ±800 VDC.

Q: When do you expect ±800 VDC to become practical?

Chen

Given the pace of GPU power growth, we believe it could be realized within the next 10 years. Without an evolution in architecture, the industry will struggle to solve data center power constraints.

Ino

In solar power generation systems, DC 1,500 V is already used. It is possible that data centers will eventually debate whether 1,500 VDC or ±800 VDC is the better long-term path. However, if 800 VDC becomes widely adopted and its ecosystem is established, moving forward to ±800 VDC as an extension is a realistic scenario.

Chen

I agree. From an ecosystem standpoint, transitioning to ±800 VDC should be smoother than jumping directly to 1,500 VDC.

Q: While 800 VDC and ±400 VDC are being actively evaluated, how does ROHM view this shift from the semiconductor side?

Ino

From ROHM’s standpoint, in the conventional data center market, our core devices were Si MOSFETs and analog ICs. However, with the emergence of 800 VDC and ±400 VDC, the needs for power devices expand from the mid-voltage range into the high-voltage range, creating major business opportunities for SiC power devices, and further for GaN power devices as well. This shift has significant meaning for ROHM.

 

ROHM began R&D on SiC power devices at an early stage and has honed performance and solutions within the global competitive environment of the EV market. The technical capabilities and track record cultivated there will be put to use in the AI data center market.
In particular, one challenge for SiC has been that the share of the EV market has been extremely high. With the rise of AI data centers as a rapidly growing new market, the application base expands substantially. At present, the market size for SiC power devices is around ¥500 billion. Forecasts suggest this could expand toward a ¥1 trillion market around 2030, and we expect that, for data center applications, an additional market—projected to reach ¥200 billion in five years and potentially expand to as much as ¥500 billion—could be added.

Mass Production to Start in Q2–Q3 2026

Q: What is the latest on practical deployment for ±400 VDC and 800 VDC?

Chen

Today, 800 VDC is being pushed aggressively by GPU vendors, while ±400 VDC is being advanced rapidly by OCP (Open Compute Project), led by data center operators. One of the biggest reasons operators favor ±400 VDC is cost performance. A data center infrastructure ecosystem already exists, and ±400 VDC can leverage much of it without requiring a full reset, which keeps transition costs comparatively lower.
We do not believe this will become a winner-takes-all scenario. Rather than one approach displacing the other, 800 VDC and ±400 VDC are likely to coexist. That is why we intend to develop both power system architectures.

Q: How do power system manufacturers and semiconductor manufacturers engage differently in developing 800 VDC and ±400 VDC systems?

Chen

The engagement model differs meaningfully. In the ±400 VDC case, data center operators typically begin by sharing their desired outcomes rather than delivering a finalized specification. We then iterate through discussions, and we ultimately propose concrete specifications back to the operator. In the process, we also engage semiconductor partners to shape a power specification that is as optimized as possible.
By contrast, 800 VDC is generally driven by GPU vendors rather than data center operators. For operators, the power system is something they use directly, so they tend to favor specifications that maximize direct operational benefit. For GPU vendors, however, the power system is something the data center operator will procure alongside AI servers built around the vendor’s GPUs. That places a premium on broad applicability and versatility. As a result, GPU vendors typically provide an initial specification draft first; we then refine and finalize it together through deeper technical discussion. The need to preserve high versatility also tends to make those specifications significantly more complex.

Q: What is the current status of development, and when will mass production begin?

Chen

We are currently advancing development of power systems compatible with both 800 VDC and ±400 VDC. We plan to begin mass production in Q2–Q3 2026, and the timing for 800 VDC and ±400 VDC should be broadly similar. That said, we expect shipment volumes to reach their peak after entering 2027.

Q: GPU vendors and data center operators are likely working with multiple power system manufacturers—not only Delta—to develop 800 VDC and ±400 VDC systems. Compared with other suppliers, where does Delta’s advantage lie?

Chen

We see three key strengths. The first is R&D capability. We prioritize advanced development and consistently invest 8% to 10% of annual revenue each year. Over time, that continuous investment has built a wide base of knowledge and technical depth inside the company, which has become a direct differentiator in fast-evolving markets.
The second is speed. The AI server market changes exceptionally quickly, and power manufacturers must respond at pace. That speed has two dimensions. One is development speed: customers demand power products on extremely short timelines, and without that responsiveness, it is difficult to win programs. The other is supply speed: the market not only moves quickly but also scales quickly. The ability to deliver large volumes within short windows becomes a decisive factor.
The third is quality. Development cycles are short, and production lead times are also compressed. The challenge is how to consistently deliver high quality products within those constraints. This is an area where we have put significant focus and engineering discipline, so customers can rely on performance and stability even as timelines accelerate.

Chosen as an Asian Partner

Q: Why did Delta choose ROHM as a partner?

Chen

There are three reasons. First, ROHM is a company we can trust. Our corporate cultures, policies, and underlying philosophies are highly aligned, which makes it easier to build strong collaboration. Over time, that trust has become a solid working relationship.
Second, ROHM is an Asian company located close to us geographically. Delta has partnerships with multiple semiconductor manufacturers, but many of them are based in Europe or the United States. We had long believed that we also needed a strong partner in Asia. ROHM stood out because it offers comprehensive server-relevant semiconductor coverage—from power devices such as SiC, Si, and GaN to control ICs.
Third, our strategic direction is aligned. For example, ROHM positions EV and automotive applications as important, and Delta shares that emphasis. When strategies point in the same direction, it becomes easier to work in step and execute consistently over the long term.

Q: How do you hope ROHM will contribute from a technology perspective?

Chen

We have built a deep relationship with ROHM over a long period, and we hope ROHM will engage even more actively from the earliest stages of advanced development. By developing together earlier, we believe we can create better technologies and significantly shorten the time it takes to bring new products to customers. We also place high importance on stable, flexible supply. AI server demand is expected to expand rapidly, and the required volumes of power semiconductors can increase suddenly. We hope ROHM can respond to that volatility with flexibility and short lead times.

Q: From ROHM’s perspective, what are the benefits of collaborating with Delta?

Ino

Delta is not a typical power supply manufacturer. Its portfolio is broad. In data centers, for example, Delta develops not only power supply units but also racks and cooling units. Even within power, Delta can support the full range—from high-voltage entry stages such as a Solid-State Transformer (SST) built with high-voltage-capable SiC power MOSFETs, all the way to the final stage where sub-1 V, high-current power is delivered to GPUs. In other words, Delta is a manufacturer that can optimize the entire power system end-to-end. Collaborating with a partner that can design and optimize at the system level allows us to participate at the leading edge and contribute to the advancement of this field.
There is also a second benefit: using this collaboration as a catalyst to enter the AI server power supply market more meaningfully. We are a late entrant in this space, but the AI server power market changes quickly, and that creates openings even for latecomers. To seize that opportunity, we chose to collaborate with Delta, which is technologically ahead in this domain. Moreover, we have a long history of exchange through joint development of GaN power devices, and through that we have confirmed strong alignment in foundational thinking and corporate cultures, something we consider critical for long-term collaboration.

Differentiation Through “Folk-Craft-Style ICs”

Q: What value can ROHM offer to Delta?

Ino

We are confident that ROHM’s power semiconductors and analog ICs are technically competitive against peers. In SiC power MOSFETs, for example, we continuously develop devices we believe set a high bar in performance (Figure 3), and for DrMOS as well, we plan to introduce products that exceed competitor performance levels (Figure 4). Providing these devices to Delta is a clear form of value.

DrMOS: integrates power semiconductor + gate driver in one package (“Doctor MOS” / “Driver MOS”)
Figure 3 History of SiC power MOSFET performance improvements (on-resistance reduction across generations)
History of SiC power MOSFET performance improvements (on-resistance reduction across generations)
Figure 4 DrMOS: integrates power semiconductor + gate driver in one package (“Doctor MOS” / “Driver MOS”)

 

In addition, our analog ICs are designed to closely match customer requirements—what we have sometimes described as “ICs that reach the itchy spot,” and we even used to call them “folk-craft-style ICs” as a lighthearted expression of that strength. Especially with high-speed power devices such as GaN, if a tailor-made mindset is applied to driver pairing and system-level optimization, it can create meaningful differentiation. By building a close relationship with Delta as our customer and responding precisely to their needs, we believe we can deliver distinctive value through power-related IC solutions.
At the same time, fully custom products can narrow the customer base and increase cost. The challenge is to preserve common platforms where appropriate while still expanding the lineup in a way that addresses customer needs. We intend to apply not only technical capability, but also product planning strength, to deliver solutions that earn Delta’s trust.

Q: Will ROHM products be adopted in the 800 VDC and ±400 VDC power systems scheduled for mass production in Q2–Q3 2026?

Chen

The power supply units (PSUs) planned for mass production in Q2–Q3 2026 are AC-DC power supplies built on a two-stage architecture consisting of a power factor correction circuit, or PFC (Power Factor Correction), followed by a DC-DC converter stage. Within these systems, we plan to adopt ROHM products such as Si power MOSFETs and SiC power MOSFETs.
Beyond the PSUs, we also plan to deliver total power solutions for AI servers—covering the entire power path from the grid to the chip (GPU). In that broader system scope, we plan to incorporate ROHM products not only for power semiconductors, but also for power control ICs and DrMOS.

Innovation in HVDC Safety Measures

Q: Is HVDC safety already adequately ensured?

Chen

HVDC requires deliberate safety design, and there are five key considerations. First, we must minimize human contact as much as possible. This becomes especially critical with 800 VDC, where the voltage differential is large, and our products incorporate measures intended to reduce the likelihood of accidental contact.
Second, we must limit impact in the unlikely event that contact occurs. For that purpose, we incorporate a function we call an “eBreaker (electronic breaker).” It enables power to be shut down in 10 microseconds, helping minimize potential impact on the human body in an emergency scenario. SiC is used extensively in that area as well.
Third, we incorporate protective devices. The concept of a data center power-side rack is similar to the concept of an EV charging station that utilizes 800 VDC. In EV charging stations, protective mechanisms are designed so charging does not begin if a person is in contact. In data center HVDC systems, we adopt the same type of protective concept.
Fourth, we look toward using robots for maintenance. Maintenance performed by humans inherently increases risk, so having robots perform maintenance instead is an idea that could become practical over time, even if it remains at a conceptual stage today.
Fifth, we consider physical separation of spaces, such as separating rooms for power racks and IT racks. For example, equipment handling high AC voltages—on the order of 10 kV to 30 kV—can be concentrated in a dedicated room. This approach reduces the chance of accidental contact and supports safer operational design.

Q: Data centers consume enormous power. Some suggest that future single data centers may require co-located gas or nuclear power plants. In that context, what role can power manufacturers and semiconductor manufacturers play?

Chen

This has been discussed continuously through the lens of “sustainable AI,” and it is a challenge the industry must address collectively. From Delta’s perspective, we are prioritizing two areas. The first is the raising power conversion efficiency—focusing on how to reduce power loss as much as possible. Conversion efficiency for data center power supplies was around 96.5% roughly two years ago, but the latest systems have improved to around 98%. The numerical gain may appear small, but because power systems operate at extremely large scale, even incremental efficiency gains translate into significant reductions in absolute energy loss. We intend to continue advancing technology to push conversion efficiency higher.
The second is power infrastructure development. We recognize that power supply has become a limiting factor in data center construction. Whether gas or nuclear, new generation capacity can require five to ten years from start to operation. That timeline is simply too slow to match the pace of AI server evolution, and it also raises environmental concerns. Therefore, we are placing strong emphasis on renewable energy, particularly solar power. We are advancing R&D on infrastructure approaches such as microgrids, enabling electricity generated by solar systems to be supplied to data centers.

Ino

Power demand is rising rapidly, centered on data centers, and the question of how to supply that incremental demand makes the sustainability perspective essential. It is expected that much of the growth will be covered by renewable energy. Semiconductor manufacturers can contribute by using power devices to improve efficiency, increase power density, and enhance reliability across generation, transmission, and power delivery, and we intend to focus strongly on that contribution.
At the same time, stepping back slightly, there are additional areas where we can contribute. AI servers learn from input data, perform inference, and output results, and GPU vendors worldwide are competing on improving computational efficiency. ROHM aims to contribute not by developing GPUs themselves—which are not within our business domain—but, but by improving signal transmission efficiency—specifically through “optical-electrical convergence,” shifting data transmission from electrical signals to optical signals. ROHM’s semiconductor business includes optical devices such as LEDs and lasers, and we are currently advancing R&D on optical devices to support this direction.

New_company localNavi.js

New_company common.js