ROHM has developed bidirectional TVS (ESD protection) diodes compatible with CAN FD (CAN with Flexible Data rate) high-speed in-vehicle communication. Such protocols are seeing an increased demand in line with the ongoing advancement in autonomous driving and advanced driver assistance systems (ADAS). CAN FD is a crucial communication technology for safe, real-time data transmission between ECUs (Electronic Control Units) in vehicles. The new products achieve high-quality in-vehicle transmission by protecting electronic devices such as ECUs from surges and electrostatic discharge (ESD) while maintaining signal integrity in high-speed communication systems such as CAN FD.
The rapid evolution of autonomous driving technology and ADAS is boosting the demand for faster, more reliable automotive communication. Autonomous driving in particular requires quick and accurate processing of vast amounts of data from sensors such as cameras, LiDAR and radar - leading to the adoption of CAN FD that enables faster, higher capacity data transfer compared to traditional CAN used in automotive communication.
At the same time, to achieve high-speed in-vehicle communication, it is necessary to ensure stable transmission even under harsh environments. This has led to a growing demand for protection components that offer low terminal capacitance along with superior surge current rating and clamping voltage performance. As a result, the market for TVS diodes for automotive communication is expected to continue to grow in the future.
To meet market needs, ROHM developed the ESDCANxx series that combines low terminal capacitance with excellent surge tolerance. Two package types are available: SOT-23 (2.9mm × 2.4mm) and DFN1010 (1.0mm × 1.0mm), both supporting standoff voltages (VRWM) of 24V and 27V. The SOT-23 package includes four models: 24V ESDCAN24HPY / ESDCAN24HXY and 27V ESDCAN27HPY / ESDCAN27HXY. Similarly, the DFN1010 package is also offered in four models: 24V ESDCAN24YPA / ESDCAN24YXA and 27V ESDCAN27YPA / ESDCAN27YXA, totaling 8 products in the lineup.
The new products feature an optimized element structure that reduces terminal capacitance to a maximum of 3.5pF, preventing signal degradation during high-speed communication. High surge tolerance is also achieved, significantly improving the protection of electronic devices in automotive environments. For example, the 27V products of the DFN1010 package delivers approx. 3.2 times higher surge current rating and 16% lower clamping voltage compared to standard CAN FD-compatible products. This effectively safeguards expensive surge-sensitive electronic devices such as in-vehicle ECUs, ensuring high reliability even under harsh automotive environments. Going forward, ROHM will continue to develop products that support even faster in-vehicle communication in autonomous driving and communication environments - contributing to realizing a safer, more advanced mobility society.
	
 
ROHM’s New TVS Diodes: Supporting High-Speed CAN FD In-Vehicle Communication Systems for Autonomous Driving
The low-capacitance design prevents signal degradation, while high surge current rating provides enhanced protection for automotive electronic devices
February 19th, 2025
ROHM has developed bidirectional TVS (ESD protection) diodes compatible with CAN FD (CAN with Flexible Data rate) high-speed in-vehicle communication. Such protocols are seeing an increased demand in line with the ongoing advancement in autonomous driving and advanced driver assistance systems (ADAS). CAN FD is a crucial communication technology for safe, real-time data transmission between ECUs (Electronic Control Units) in vehicles. The new products achieve high-quality in-vehicle transmission by protecting electronic devices such as ECUs from surges and electrostatic discharge (ESD) while maintaining signal integrity in high-speed communication systems such as CAN FD.
The rapid evolution of autonomous driving technology and ADAS is boosting the demand for faster, more reliable automotive communication. Autonomous driving in particular requires quick and accurate processing of vast amounts of data from sensors such as cameras, LiDAR and radar - leading to the adoption of CAN FD that enables faster, higher capacity data transfer compared to traditional CAN used in automotive communication.
At the same time, to achieve high-speed in-vehicle communication, it is necessary to ensure stable transmission even under harsh environments. This has led to a growing demand for protection components that offer low terminal capacitance along with superior surge current rating and clamping voltage performance. As a result, the market for TVS diodes for automotive communication is expected to continue to grow in the future.
To meet market needs, ROHM developed the ESDCANxx series that combines low terminal capacitance with excellent surge tolerance. Two package types are available: SOT-23 (2.9mm × 2.4mm) and DFN1010 (1.0mm × 1.0mm), both supporting standoff voltages (VRWM) of 24V and 27V. The SOT-23 package includes four models: 24V ESDCAN24HPY / ESDCAN24HXY and 27V ESDCAN27HPY / ESDCAN27HXY. Similarly, the DFN1010 package is also offered in four models: 24V ESDCAN24YPA / ESDCAN24YXA and 27V ESDCAN27YPA / ESDCAN27YXA, totaling 8 products in the lineup.
The new products feature an optimized element structure that reduces terminal capacitance to a maximum of 3.5pF, preventing signal degradation during high-speed communication. High surge tolerance is also achieved, significantly improving the protection of electronic devices in automotive environments. For example, the 27V products of the DFN1010 package delivers approx. 3.2 times higher surge current rating and 16% lower clamping voltage compared to standard CAN FD-compatible products. This effectively safeguards expensive surge-sensitive electronic devices such as in-vehicle ECUs, ensuring high reliability even under harsh automotive environments. Going forward, ROHM will continue to develop products that support even faster in-vehicle communication in autonomous driving and communication environments - contributing to realizing a safer, more advanced mobility society.
Product Lineup
Sheet
-Q101
Qualified
[mm]
(tp=8/20μs)
PPP Max.
[W]
[Surge Current Rating]
(tp=8/20μs)
IPP Max.
[A]
(C=150pF,
R=330Ω)
VESD Max.
[kV]
Temp.
Tj
Max.
[°C]
Voltage
VRWM
Max.
[V]
Voltage
(IR=1mA)
VBR [V]
Voltage
(tp=8/20μs)
VCL Max. [V]
Capacitance
(VR=0V)
Ct Max.
[pF]
SOT-23
[2.9 ×
2.4 ×
0.95]
DFN1010
[1.0 ×
1.0 ×
0.4]
Application Examples
• Autonomous driving and Advanced Driver Assistance Systems (ADAS)
• Automotive electric powertrain systems
• In-vehicle infotainment systems
Online Distributor Information
Sales Launch Date: December 2024
Pricing: $0.9/unit (excluding tax)
Online Distributors: DigiKey™, Mouser™ and Farnell™
The products will be offered at other online distributors as they become available.
Online Distributors
Target Products
SOT23 Package: ESDCAN24HPY, ESDCAN24HXY, ESDCAN27HPY, ESDCAN27HXY
DFN1010 Package: ESDCAN24YPA, ESDCAN24YXA, ESDCAN27YPA, ESDCAN27YXA
Terminology
Note: DigiKey™, Mouser™ and Farnell™ are trademarks or registered trademarks of their respective companies.
Latest News