*ROHM November 7th, 2024 study
ROHM has developed automotive-grade AEC-Q101 qualified 4th Generation 1200V IGBTs that combine class-leading* low loss characteristics with high short-circuit resistance. This makes the devices ideal for vehicle electric compressors and HV heaters as well as industrial inverters. The current lineup includes four models - RGA80TRX2HR / RGA80TRX2EHR / RGA80TSX2HR / RGA80TSX2EHR - in two discrete package types (TO-247-4L and TO-247N), along with 11 bare chip variants - SG84xxWN - with plans to further expand the lineup in the future.
The increasing use of higher voltages in automotive systems and industrial equipment has led to a growing demand for power devices capable of handling high voltages in applications such as vehicle electric compressors, HV heaters, and inverters for industrial equipment. At the same time, there is a strong push for high efficiency power devices to improve energy conservation, simplified cooling mechanisms, and smaller form factors for a decarbonized society. Automotive electrical components must also comply with automotive reliability standards, while power devices for inverter and heater circuits are required to provide current interruption capabilities during short circuits, necessitating high short-circuit tolerance.
In response, ROHM redesigned the device structure and adopted an appropriate package to develop new 4th Generation IGBTs suitable for high voltage by delivering industry-low loss characteristics with superior short-circuit tolerance. These devices achieve an industry-leading* short-circuit withstand time of 10µs (Tj=25°C) together with low switching and conduction losses while maintaining a high withstand voltage of 1200V and meeting automotive standards by reviewing the device structure, including the peripheral design. At the same time, the new TO-247-4L package products, which feature 4 terminals, can accommodate an effective voltage of 1100V in a ‘Pollution Degree 2 environment’ by ensuring adequate creepage distance between pins. This enables support for higher voltage applications than conventional products.

Implementing creepage distance measures on the device side alleviates the design burden for manufacturers. On top, the TO-247-4L package achieves high-speed switching by including a Kelvin emitter terminal, resulting in even lower losses. In fact, when comparing the efficiency of the new TO-247-4L packages with conventional and standard products in a 3-phase inverter, loss is reduced by about 24% compared to standard products and by 35% over conventional products - contributing to higher efficiency in drive applications.
ROHM will continue to expand its lineup of high-performance IGBTs that contribute to greater miniaturization and high efficiency drive in automotive and industrial equipment applications.
Product Lineup - Discretes
Bare Chips
| Part No. |
Collector-
Emitter Voltage
VCES [V] |
Collector Current
IC(TC=100°C) [A] |
Conduction Loss
VCE(sat)
(Typ.) [V] |
Short-Circuit Withstand Time
TSC
[µs] |
Chip Size |
X [mm] |
Y [mm] |
Thickness [µm] |
SG8405WN |
1200 |
10 |
1.55 |
10 |
3.94 |
3.94 |
130 |
SG8411WN |
15 |
4.49 |
4.49 |
SG8410WN |
25 |
5.40 |
5.40 |
SG8415WN |
30 |
5.69 |
5.69 |
SG8409WN |
35 |
6.00 |
6.00 |
SG8401WN |
40 |
6.35 |
6.35 |
SG8406WN |
50 |
7.00 |
7.00 |
SG8408WN |
75 |
8.49 |
8.49 |
SG8407WN |
100 |
9.36 |
9.36 |
SG8412WN |
150 |
11.23 |
11.23 |
SG8403WN |
200 |
12.84 |
12.84 |
Application Examples
◇ Automotive electric compressors
◇ Automotive HV heaters (PTC/coolant heaters)
◇ Inverters for industrial equipment
EcoIGBT™ Brand
EcoIGBT™ is ROHM’s brand of IGBTs consisting of both devices and modules designed to meet the needs of high-voltage applications in the power device field. ROHM independently develops technologies essential for the evolution of power devices, from wafer fabrication and production processes to packaging and quality control methods. At the same time, we have established an integrated production system throughout the manufacturing process, solidifying our position as a leading power device supplier.
EcoIGBT™ is a trademark or registered trademark of ROHM Co., Ltd.
Terminology
- AEC-Q101 Automotive Reliability Standard
- AEC stands for Automotive Electronics Council, a reliability standard for automotive electronic components established by major automotive manufacturers and US electronic component makers. AEC-Q101 is a standard that specifically applies to discrete semiconductor products (i.e. transistors, diodes).
- Short-Circuit Tolerance
- The time that a power device can withstand a short-circuit without being destroyed.
- IGBT (Insulated Gate Bipolar Transistor)
- A power transistor that combines the high-speed switching characteristics of a MOSFET with the low conduction loss of a bipolar transistor.
- Creepage Distance
- The shortest distance along the surface of an insulator between two conductors. In semiconductor design, insulation measures with such creepage and space distances must be taken to prevent electric shocks, leakage currents, and short-circuits in semiconductor products.
- Pollution Degree 2 Environment
- Pollution Degree 2 corresponds to typical environments such as homes and offices where only dry, non-conductive contaminants are present. Pollution Degree is the grade of the environment that influences the determination of the spatial and creepage distances of components, classified from 1 to 4 according to the presence, amount, and condition of pollutants.
- Kelvin Emitter Terminal
- An emitter terminal dedicated to voltage measurement. By separating this from the emitter through which current flows, the effects of voltage drop during current flow can be minimized, allowing for fast, stable switching.
DigiKey™, Mouser™ and Farnell™ are trademarks or registered trademarks of their respective companies.
ROHM’s New 1200V IGBTs Achieve Industry-Leading* Low Loss Characteristics with High Short-Circuit Tolerance
Contributes to higher efficiency in automotive electric compressors and inverters for industrial equipment
*ROHM November 7th, 2024 study
November 7th, 2024
ROHM has developed automotive-grade AEC-Q101 qualified 4th Generation 1200V IGBTs that combine class-leading* low loss characteristics with high short-circuit resistance. This makes the devices ideal for vehicle electric compressors and HV heaters as well as industrial inverters. The current lineup includes four models - RGA80TRX2HR / RGA80TRX2EHR / RGA80TSX2HR / RGA80TSX2EHR - in two discrete package types (TO-247-4L and TO-247N), along with 11 bare chip variants - SG84xxWN - with plans to further expand the lineup in the future.
The increasing use of higher voltages in automotive systems and industrial equipment has led to a growing demand for power devices capable of handling high voltages in applications such as vehicle electric compressors, HV heaters, and inverters for industrial equipment. At the same time, there is a strong push for high efficiency power devices to improve energy conservation, simplified cooling mechanisms, and smaller form factors for a decarbonized society. Automotive electrical components must also comply with automotive reliability standards, while power devices for inverter and heater circuits are required to provide current interruption capabilities during short circuits, necessitating high short-circuit tolerance.
In response, ROHM redesigned the device structure and adopted an appropriate package to develop new 4th Generation IGBTs suitable for high voltage by delivering industry-low loss characteristics with superior short-circuit tolerance. These devices achieve an industry-leading* short-circuit withstand time of 10µs (Tj=25°C) together with low switching and conduction losses while maintaining a high withstand voltage of 1200V and meeting automotive standards by reviewing the device structure, including the peripheral design. At the same time, the new TO-247-4L package products, which feature 4 terminals, can accommodate an effective voltage of 1100V in a ‘Pollution Degree 2 environment’ by ensuring adequate creepage distance between pins. This enables support for higher voltage applications than conventional products.
Implementing creepage distance measures on the device side alleviates the design burden for manufacturers. On top, the TO-247-4L package achieves high-speed switching by including a Kelvin emitter terminal, resulting in even lower losses. In fact, when comparing the efficiency of the new TO-247-4L packages with conventional and standard products in a 3-phase inverter, loss is reduced by about 24% compared to standard products and by 35% over conventional products - contributing to higher efficiency in drive applications.
ROHM will continue to expand its lineup of high-performance IGBTs that contribute to greater miniaturization and high efficiency drive in automotive and industrial equipment applications.
Product Lineup - Discretes
Sheet
Emitter Voltage
VCES [V]
IC(TC=100°C)
[A]
Loss
VCE(sat)
(Typ.) [V]
Withstand Time
TSC(Tj=25°C)
[µs]
Recovery
Diode
Temperature
Range
Tj [°C]
Qualified
[mm]
to
+175
TO-247-4L
[16.0×23.45×5.0]
to
+175
TO-247N
[16.0×21.0×5.0]
☆: Under Development
Bare Chips
Emitter Voltage
VCES [V]
IC(TC=100°C)
[A]
Loss
VCE(sat)
(Typ.) [V]
Withstand Time
TSC
[µs]
[mm]
[mm]
[µm]
Application Examples
◇ Automotive electric compressors
◇ Automotive HV heaters (PTC/coolant heaters)
◇ Inverters for industrial equipment
Online Sales Information
Availability: Now
Pricing: $10.50/unit (samples, excluding tax)
Online Distributors: DigiKey™, Mouser™ and Farnell™
The products will be offered at other online distributors as they become available.
Applicable P/N: RGA80TRX2HR, RGA80TRX2EHR, RGA80TSX2HR, RGA80TSX2EHR
Online Distributors
Supporting Information
From ROHM’s official website, users can download various materials required for circuit design, including SPICE models that faithfully replicate the electrical characteristics of the products through simulation.
https://www.rohm.com/products/igbt/field-stop-trench-igbt#parametricSearch
Semikron Danfoss Power Semiconductor Modules Equipped with the RGA Series
ROHM’s RGA series of 1200V IGBTs has been adopted in Semikron Danfoss’ MiniSKiiP® series of power semiconductor modules featuring rated currents of 10A to 150A. Click here for more information.
https://www.rohm.com/news-detail?news-title=2023-04-25_news_semikron&defaultGroupId=false
*MiniSKiiP® is a trademark or registered trademark of Semikron Danfoss.
EcoIGBT™ Brand
EcoIGBT™ is ROHM’s brand of IGBTs consisting of both devices and modules designed to meet the needs of high-voltage applications in the power device field. ROHM independently develops technologies essential for the evolution of power devices, from wafer fabrication and production processes to packaging and quality control methods. At the same time, we have established an integrated production system throughout the manufacturing process, solidifying our position as a leading power device supplier.
EcoIGBT™ is a trademark or registered trademark of ROHM Co., Ltd.
Terminology
DigiKey™, Mouser™ and Farnell™ are trademarks or registered trademarks of their respective companies.
Latest News