Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
New 32bit D/A Converter IC for Hi-Fi Audio Equipment
March 1st, 2022
ROHM now offers a DAC chip lineup for high-end audio
ROHM developed the D/A converter IC (DAC chip) BD34352EKV and the corresponding evaluation board BD34352EKV-EVK-001 – supporting the playback of high-resolution sound sources in high fidelity audio equipment.
Designed to maximally extract and convert high resolution digital audio data to analog audio signals, audio DAC chips are one of the most important components for determining the quality in audio equipment.
Leveraging 50 years of expertise in developing audio ICs allowed ROHM to establish ‘sound quality design technology’ – capable of extracting the full amount of information from sound sources and offer products that deliver superior sound quality, including sound processor and power management ICs.
Among these is the BD34301EKV, the flagship DAC chip of ROHM’s MUS-IC series, which has been highly evaluated for its sound quality since its release in February 2021. It continues to see worldwide adoption. However, to meet the growing demand from manufacturers for a DAC chip that can be used in a wider range of audio equipment, ROHM developed the BD34352EKV.
The new DAC chip BD34352EKV is specially tuned to powerfully express the energy of sound sources while maintaining the natural flat sound characteristics of ROHM’s DAC chips design concept. At the same time, an advanced digital filter is included - the same as for BD34301EKV. That leads to superior numerical performance (S/N ratio: 126dB, THD+N: -112dB) of the DAC chip, making it ideal for high-end audio equipment. In addition, the BD34352EKV features pin compatibility with the BD34301EKV. It has the same customizable filter as the BD34301EKV. This enables different sound quality tunings for each audio device – reducing development load while contributing to the creation of ideal sound sought by audio manufacturers.
Key Features
Developed as a DAC chip for high-end audio equipment, the BD34352EKV not only maintains the natural flat sound characteristics of ROHM’s DAC chips design concept. It is also specially tuned to express the energy of sound sources more powerfully than the BD34301EKV, which emphasizes quietness and spatial reverberation.
To achieve the desired sound, the BD34352EKV provides the following features by leveraging sound quality design technology cultivated from identifying 28 parameters related to sound quality.
1. Achieves the demanded numerical and sound quality performance of DAC chips for high-end models The BD34352EKV achieves excellent numerical performance (S/N ratio: 126dB, THD+N: -112dB) while also improving sound quality in ways that cannot be defined by simple numerical values. For example, in the D/A conversion circuit consisting of current segments, the output current has been adjusted by adopting circuit technology used in the BD34301EKV. At the same time, the digital filter (FIR filter), a key function of the digital signal processing circuit, is designed to faithfully process even the smallest signals by achieving a rejection band attenuation of -150dB or less (a performance indicator of digital filters). This makes it possible to extract the full range of information from sound sources. It provides sound quality characteristics that allow listeners to hear more powerful, natural flat sound.
2. Customizable digital filter allows designers to tailor the sound to audio equipment The BD34352EKV enables customization of the digital filter (FIR filter) in the digital signal processing circuit which affects sound quality. Preset, custom, or external settings can be selected. Even the filter’s calculation coefficients and oversampling rate can be programmatically customized. As a result, it not only features pin compatibility but also has the same customizable filter as the BD34301EKV. That allows to achieve different sound quality tunings for each device. Overall, this reduces development load while contributing to the creation of ideal sound sought by audio manufacturers.
Created by combining the ‘sound quality design technology’ with ROHM’s company mission of ‘quality first’, ‘vertically integrated production system’, and ‘contribution to the musical culture’, MUS-IC™ (official name: ROHM Musical Device ‘MUS-IC™’) is an audio device brand that represents the ultimate IC solutions developed by ROHM’s team of experienced and dedicated engineers. For more information, please visit ROHM’s Musical Device ‘MUS-IC™’ web page. https://www.rohm.com/mus-ic/
* MUS-IC™ is a trademark or registered trademark of ROHM Co., Ltd.
ROHM’s Contribution to Music Culture
ROHM has contributed to popularizing and developing music cultures centering on classic music for more than 30 years with the foundation “Rohm Music Foundation”. As for scholarship assistance for young musicians, we have supported 507 young musicians by Nov 2021, its supporting musicians as "Rohm Music Friends" are active around the world, like winning prizes in international competitions and serving as the principal player of the orchestra. We organize the “Kyoto International Music Students Festival” to promote international exchange among young musicians and “ROHM Music Seminar” to foster professional musicians. We also offer financial support for music-related performances, research and more. In addition to that, we host and cooperate for concerts and operas, supporting the comprehensive theatre “ROHM Theatre Kyoto” representing Japan.
New 32bit D/A Converter IC for Hi-Fi Audio Equipment
March 1st, 2022
ROHM now offers a DAC chip lineup for high-end audio
ROHM developed the D/A converter IC (DAC chip) BD34352EKV and the corresponding evaluation board BD34352EKV-EVK-001 – supporting the playback of high-resolution sound sources in high fidelity audio equipment.
Designed to maximally extract and convert high resolution digital audio data to analog audio signals, audio DAC chips are one of the most important components for determining the quality in audio equipment.
Leveraging 50 years of expertise in developing audio ICs allowed ROHM to establish ‘sound quality design technology’ – capable of extracting the full amount of information from sound sources and offer products that deliver superior sound quality, including sound processor and power management ICs.
Among these is the BD34301EKV, the flagship DAC chip of ROHM’s MUS-IC series, which has been highly evaluated for its sound quality since its release in February 2021. It continues to see worldwide adoption. However, to meet the growing demand from manufacturers for a DAC chip that can be used in a wider range of audio equipment, ROHM developed the BD34352EKV.
The new DAC chip BD34352EKV is specially tuned to powerfully express the energy of sound sources while maintaining the natural flat sound characteristics of ROHM’s DAC chips design concept. At the same time, an advanced digital filter is included - the same as for BD34301EKV. That leads to superior numerical performance (S/N ratio: 126dB, THD+N: -112dB) of the DAC chip, making it ideal for high-end audio equipment. In addition, the BD34352EKV features pin compatibility with the BD34301EKV. It has the same customizable filter as the BD34301EKV. This enables different sound quality tunings for each audio device – reducing development load while contributing to the creation of ideal sound sought by audio manufacturers.
Key Features
Developed as a DAC chip for high-end audio equipment, the BD34352EKV not only maintains the natural flat sound characteristics of ROHM’s DAC chips design concept. It is also specially tuned to express the energy of sound sources more powerfully than the BD34301EKV, which emphasizes quietness and spatial reverberation.
To achieve the desired sound, the BD34352EKV provides the following features by leveraging sound quality design technology cultivated from identifying 28 parameters related to sound quality.
1. Achieves the demanded numerical and sound quality performance of DAC chips for high-end models
The BD34352EKV achieves excellent numerical performance (S/N ratio: 126dB, THD+N: -112dB) while also improving sound quality in ways that cannot be defined by simple numerical values. For example, in the D/A conversion circuit consisting of current segments, the output current has been adjusted by adopting circuit technology used in the BD34301EKV. At the same time, the digital filter (FIR filter), a key function of the digital signal processing circuit, is designed to faithfully process even the smallest signals by achieving a rejection band attenuation of -150dB or less (a performance indicator of digital filters). This makes it possible to extract the full range of information from sound sources. It provides sound quality characteristics that allow listeners to hear more powerful, natural flat sound.
2. Customizable digital filter allows designers to tailor the sound to audio equipment
The BD34352EKV enables customization of the digital filter (FIR filter) in the digital signal processing circuit which affects sound quality. Preset, custom, or external settings can be selected. Even the filter’s calculation coefficients and oversampling rate can be programmatically customized. As a result, it not only features pin compatibility but also has the same customizable filter as the BD34301EKV. That allows to achieve different sound quality tunings for each device. Overall, this reduces development load while contributing to the creation of ideal sound sought by audio manufacturers.
DAC Chip Lineup for High Fidelity Audio Equipment
BD34352EKV
DAC Chip BD34352EKV Availability
Pricing: $16.0/unit (samples, excluding tax)
Availability: Now (samples and mass production)
Online Distributors
Evaluation Board Information
Sales Launch Date: February 2022
Evaluation Board Part No: BD34352EKV-EVK-001
Online Distributors: Digi-Key, Mouser, and Farnell
Support Page: https://www.rohm.com/products/audio-video/audio-converters/audio-dacs/bd34352ekv-product#evaluationBoard
MUS-IC™ - ROHM’s Highest Grade of Audio ICs
Created by combining the ‘sound quality design technology’ with ROHM’s company mission of ‘quality first’, ‘vertically integrated production system’, and ‘contribution to the musical culture’, MUS-IC™ (official name: ROHM Musical Device ‘MUS-IC™’) is an audio device brand that represents the ultimate IC solutions developed by ROHM’s team of experienced and dedicated engineers.
For more information, please visit ROHM’s Musical Device ‘MUS-IC™’ web page.
https://www.rohm.com/mus-ic/
* MUS-IC™ is a trademark or registered trademark of ROHM Co., Ltd.
ROHM’s Contribution to Music Culture
ROHM has contributed to popularizing and developing music cultures centering on classic music for more than 30 years with the foundation “Rohm Music Foundation”. As for scholarship assistance for young musicians, we have supported 507 young musicians by Nov 2021, its supporting musicians as "Rohm Music Friends" are active around the world, like winning prizes in international competitions and serving as the principal player of the orchestra. We organize the “Kyoto International Music Students Festival” to promote international exchange among young musicians and “ROHM Music Seminar” to foster professional musicians. We also offer financial support for music-related performances, research and more. In addition to that, we host and cooperate for concerts and operas, supporting the comprehensive theatre “ROHM Theatre Kyoto” representing Japan.
Latest News
METI recognizes joint plan as supporting stable, sec ...