ROHM has developed high-speed, highly reliable thermal printheads: TE2004-QP1W00A / TE3004-TP1W00A. These devices are optimized for barcode label printers applied in logistics and inventory management.
In recent years, the growth of the e-commerce (EC) market and diversifying customer needs have increased the demand for logistics and inventory management labels. Conventional thermal printheads, however, are limited to printing speeds ranging from 250mm/s to 300mm/s. In response, ROHM developed high speed and highly reliable thermal printheads that leverage novel structures and technologies. The key goal: achieving a level of print quality and durability that exceeds conventional limits.
The TE2004-QP1W00A (203dpi) and TE3004-TP1W00A (300dpi) significantly improve on the substrate material, structure, and wiring pattern over existing products. In particular, the heating elements, which affect printing speed and quality, adopt a new design using ROHM’s original 3D processing technology to achieve an industry-leading print speed of 500mm/s - approximately twice as fast as conventional products.
On top, applying a two-layer high-hardness protective film to the head increases resistance to abrasion and static electricity for high-speed printing along with corrosion caused by moisture and salt, extending service life considerably.
In the future, ROHM will continue to improve the efficiency of label printing in various industries by applying these technologies to new products.
New Thermal Printheads Deliver the Industry's Fastest* Print Speed for Barcode Labels
High-speed, high-quality printing and superior durability: contributing to improved efficiency in logistics and inventory management label applications
*ROHM October 11th, 2023 study
October 11th, 2023
ROHM has developed high-speed, highly reliable thermal printheads: TE2004-QP1W00A / TE3004-TP1W00A. These devices are optimized for barcode label printers applied in logistics and inventory management.
In recent years, the growth of the e-commerce (EC) market and diversifying customer needs have increased the demand for logistics and inventory management labels. Conventional thermal printheads, however, are limited to printing speeds ranging from 250mm/s to 300mm/s. In response, ROHM developed high speed and highly reliable thermal printheads that leverage novel structures and technologies. The key goal: achieving a level of print quality and durability that exceeds conventional limits.
The TE2004-QP1W00A (203dpi) and TE3004-TP1W00A (300dpi) significantly improve on the substrate material, structure, and wiring pattern over existing products. In particular, the heating elements, which affect printing speed and quality, adopt a new design using ROHM’s original 3D processing technology to achieve an industry-leading print speed of 500mm/s - approximately twice as fast as conventional products.
On top, applying a two-layer high-hardness protective film to the head increases resistance to abrasion and static electricity for high-speed printing along with corrosion caused by moisture and salt, extending service life considerably.
In the future, ROHM will continue to improve the efficiency of label printing in various industries by applying these technologies to new products.
Product Lineup
Sheet
Density
[dpi]
Width
[mm]
Dots
[dots]
Speed
[mm/s]
[Ω]
Supply
Voltage [V]
Supply
Voltage [V]
to
5.25
*For more information, please refer to the following URL on ROHM’s website:
https://www.rohm.com/products/printheads/ticket-or-scale-printers
Sales Information
Pricing
TE2004-QP1W00A (203dpi): $430/unit (samples, excluding tax)
TE3004-TP1W00A (300dpi): $470/unit (samples, excluding tax)
Availability: Now (OEM quantities)
Application Examples
Barcode label printers used for logistics and inventory management
Leaflet
High Speed and High Reliability Thermal Printheads
3D Head STPH series (PDF:1.1MB)
Latest News