Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
New RGB Chip LED for Automotive Interiors Minimizes Color Variations due to Color Mixing Contributes to accurate color representation in cabin function/status indicators and accent lighting
ROHM has developed an RGB chip LED, SMLVN6RGBFU ideal for automotive interiors, such as function and status indicators in instrument clusters, CID (Center Information Displays) and accent lighting for footwells and door handles.
In recent years, more driver assistance functions (i.e., automatic speed control, vehicle distance/white line detection) have been introduced as vehicles become progressively electronic and sophisticated. As such, the demand for RGB chip LEDs capable of expressing a range of colors to indicate operational status in instrument panels and meter clusters is rising. In addition, there's also an increasing need to create a comfortable and luxurious cabin space with decorative lighting using RGB chip LEDs.
In response, ROHM has developed an RGB chip LED that further minimizes color variation by precisely controlling the luminous characteristics of the RGB elements and improving color mixing through in-house device technology.
Generally, developing RGB chip LEDs that emit light at the specified color requires precise control of the wavelength and brightness of the mounted red, green, and blue (RGB) elements individually and methods to enhance color-mixing capability. ROHM has minimized element color variation over general products by utilizing a vertically integrated production system from the element fabrication stage - one of ROHM's strengths. At the same time, original element color mixing control technology reduces color variations caused by color mixing that tends to occur in RGB chip LEDs, resulting in accurate color expression required in automotive interiors. ROHM also supports detailed color matching tailored to user specifications with the chromaticity simulation system.
As we advance, ROHM will continue to contribute to improving in-vehicle comfort and safety by developing industry-leading products optimized for automotive lighting through a quality-first approach.
Chromaticity Simulation System
The SMLVN6RGBFU sets adjustment coefficients for each chromaticity rank while providing calibration support to bring the color closer to the desired target. This new RGB chip LED and high-accuracy chromaticity simulation allows precise color matching.
◇ Indicators for function/status display: Instrument clusters, CID, car audio/navigation, heater control, etc.
◇ Automotive Ambient lighting: footwells, roof, handles, cup holders, etc.
Online Sales Information
Sales Launch Date: June 2023 Distributors: DigiKey, MOUSER and Farnell
The LED will be offered at other online distributors as it becomes available. Pricing: $4.0/unit (samples, excluding tax)
Online Distributors
Terminology
CID (Center Information Display)
It typically comprises of a large LCD embedded in the center of the cockpit. In addition to displaying car navigation and In-Vehicle Infotainment (IVI), its role has expanded to include controlling the Air Conditioner and other vehicle functions in recent years.
Indicators
These are devices that notify the status of various vehicle operations.
RGB Chip LED
An LED that can produce the full range of colors by combining elements for the three primary colors of light: R (Red), G (Green), and B (Blue).
New RGB Chip LED for Automotive Interiors Minimizes Color Variations due to Color Mixing
Contributes to accurate color representation in cabin function/status indicators and accent lighting
July 6th, 2023
ROHM has developed an RGB chip LED, SMLVN6RGBFU ideal for automotive interiors, such as function and status indicators in instrument clusters, CID (Center Information Displays) and accent lighting for footwells and door handles.
In recent years, more driver assistance functions (i.e., automatic speed control, vehicle distance/white line detection) have been introduced as vehicles become progressively electronic and sophisticated. As such, the demand for RGB chip LEDs capable of expressing a range of colors to indicate operational status in instrument panels and meter clusters is rising. In addition, there's also an increasing need to create a comfortable and luxurious cabin space with decorative lighting using RGB chip LEDs.
In response, ROHM has developed an RGB chip LED that further minimizes color variation by precisely controlling the luminous characteristics of the RGB elements and improving color mixing through in-house device technology.
Generally, developing RGB chip LEDs that emit light at the specified color requires precise control of the wavelength and brightness of the mounted red, green, and blue (RGB) elements individually and methods to enhance color-mixing capability. ROHM has minimized element color variation over general products by utilizing a vertically integrated production system from the element fabrication stage - one of ROHM's strengths. At the same time, original element color mixing control technology reduces color variations caused by color mixing that tends to occur in RGB chip LEDs, resulting in accurate color expression required in automotive interiors. ROHM also supports detailed color matching tailored to user specifications with the chromaticity simulation system.
As we advance, ROHM will continue to contribute to improving in-vehicle comfort and safety by developing industry-leading products optimized for automotive lighting through a quality-first approach.
Chromaticity Simulation System
The SMLVN6RGBFU sets adjustment coefficients for each chromaticity rank while providing calibration support to bring the color closer to the desired target. This new RGB chip LED and high-accuracy chromaticity simulation allows precise color matching.
Product Lineup
Sheet
Color
Size
[mm]
Permissible
Loss
PD[mW]
Current
IF[mA]
Forward
Current
IFP[mA]
Temp.
Topr[°C]
Temp.
Tstg
[°C]
Voltage VF
Typ.
[V]
Wavelength λD
Typ.
[nm]
Intensity IV
[mcd]
Typ.
[mA]
[mA]
[mA]
to
+100
to
+100
3.5×2.8,
t=0.6
IFP conditions: Pulse Width ≤ 1ms, Duty ≤ 1/20
Application Examples
◇ Indicators for function/status display: Instrument clusters, CID, car audio/navigation, heater control, etc.
◇ Automotive Ambient lighting: footwells, roof, handles, cup holders, etc.
Online Sales Information
Sales Launch Date: June 2023
Distributors: DigiKey, MOUSER and Farnell
The LED will be offered at other online distributors as it becomes available.
Pricing: $4.0/unit (samples, excluding tax)
Online Distributors
Terminology
Featured Products
Achieve accurate your image color
RGB Chip LED for Automotive Interiors
SMLVN6RGBFU (PDF: 1.1MB)
Latest News
METI recognizes joint plan as supporting stable, sec ...