ROHM has recently developed wide terminal shunt resistors, LTR10L. They are optimized for a variety of applications in the automotive, industrial, and consumer sectors, while also strengthening its considerable lineup with two updated general-purpose MCR series shunt resistors (MCR10L and MCR18L).
In recent years, high efficiency operation is required from the viewpoint of energy conservation – not only in battery-driven applications such as mobile devices and EVs, but in consumer and industrial equipment as well powered by electrical outlets. For high efficiency, it is important to accurately detect parameters such as current and voltage in order to operate devices optimally. This requires shunt resistors that combine high accuracy with high reliability current detection. At the same time, manufacturers of applications utilizing higher board densities are demanding even smaller shunt resistors. To meet these needs, the new LTR10L series delivers the industry's highest rated power and best-in-class temperature coefficient of resistance (TCR) in a compact 0508-size (0.5inch × 0.8inch) / 1220-size (1.25mm × 2.0mm) that contributes to both high reliability and greater miniaturization.
Improving the resistive element material and applying terminal temperature derating method allowed LTR10L to deliver an industry-leading 1W rated power in the 0508-size - 88% smaller than existing products. In addition, high-accuracy ±0.5% resistance tolerance has been achieved, together with best-in-class TCR and anti-sulfuration characteristics. These features make them ideal for applications exposed to harsh conditions, including telecommunication base stations requiring high durability and automotive LED headlamps that demand high accuracy current sensing along with long-term reliability. On the other hand, the MCR10L and MCR18L series of general-purpose shunt resistors utilize an improved element structure and materials to increase rated power to 0.5W and 0.75W, respectively, over their conventional MCR series rated power (0.25W). Higher rated power enables the same performance in a smaller size, contributing to product miniaturization.
Going forward, ROHM will continue to expand its lineup of resistors (its founding products) that leads to improved miniaturization and reliability while striving to ensure long-term stable supply.
ROHM Industry’s Highest Rated Power Shunt Resistors in the 0508 Size: Contributes to Greater Miniaturization
Lineup also expanded to include 2 updated general-purpose MCR series shunt resistors
*ROHM December 8, 2022 study
December 8th, 2022
ROHM has recently developed wide terminal shunt resistors, LTR10L. They are optimized for a variety of applications in the automotive, industrial, and consumer sectors, while also strengthening its considerable lineup with two updated general-purpose MCR series shunt resistors (MCR10L and MCR18L).
In recent years, high efficiency operation is required from the viewpoint of energy conservation – not only in battery-driven applications such as mobile devices and EVs, but in consumer and industrial equipment as well powered by electrical outlets. For high efficiency, it is important to accurately detect parameters such as current and voltage in order to operate devices optimally. This requires shunt resistors that combine high accuracy with high reliability current detection. At the same time, manufacturers of applications utilizing higher board densities are demanding even smaller shunt resistors. To meet these needs, the new LTR10L series delivers the industry's highest rated power and best-in-class temperature coefficient of resistance (TCR) in a compact 0508-size (0.5inch × 0.8inch) / 1220-size (1.25mm × 2.0mm) that contributes to both high reliability and greater miniaturization.
Improving the resistive element material and applying terminal temperature derating method allowed LTR10L to deliver an industry-leading 1W rated power in the 0508-size - 88% smaller than existing products. In addition, high-accuracy ±0.5% resistance tolerance has been achieved, together with best-in-class TCR and anti-sulfuration characteristics. These features make them ideal for applications exposed to harsh conditions, including telecommunication base stations requiring high durability and automotive LED headlamps that demand high accuracy current sensing along with long-term reliability. On the other hand, the MCR10L and MCR18L series of general-purpose shunt resistors utilize an improved element structure and materials to increase rated power to 0.5W and 0.75W, respectively, over their conventional MCR series rated power (0.25W). Higher rated power enables the same performance in a smaller size, contributing to product miniaturization.
Going forward, ROHM will continue to expand its lineup of resistors (its founding products) that leads to improved miniaturization and reliability while striving to ensure long-term stable supply.
LTR10L Lineup and Features
● LTR10L Features
LTR10L is a 0508-size (0.5inch × 0.8inch) / 1220-size (1.25mm × 2.0mm) model with an industry-leading rated power of 1W. The lineup includes high accuracy (D Class) products that provide a resistance tolerance of 0.5% along with class-leading TCR, making them ideal for automotive LED headlamps and other applications requiring high accuracy current detection. At the same time, high sulfuration resistance enables suitability with telecommunication base stations requiring long-term reliability even when operating continuously in harsh outdoor environments and automotive powertrain where sulfuration from exposure to exhaust gases is a concern.
● LTR10L Lineup
Sheet
inch
[mm]
[W]
(Rated Terminal
Temperature: 125°C)
Tolerance
of Resistance
TCR [ppm/°C]
Temperature
Range [°C]
Grade
AEC-Q200
[1220]
F (±1%)
MCR10L / MCR18L Lineup and Features
● MCR10L / MCR18L Features
The MCR10L (0.5W rated power) and MCR18L (0.75W rated power) are low-resistance models in the general-purpose MCR series. Power rating is not only significantly improved, but TCR as well compared with the conventional 0.25W rated MCR10 and MCR18. Additional updates include a revised element structure and materials that increase performance and allow us to continue to ensure stable supply.
● MCR10L / MCR18L Lineup
Sheet
inch
[mm]
[W]
(Rated Ambient
Temperature: 70°C)
Tolerance
of Resistance
TCR [ppm/°C]
Temperature
Range [°C]
Grade
AEC-Q200
[2012]
F (±1%)
[3216]
F (±1%)
Application Examples
The new products are ideal for a wide range of circuits requiring current detection for motors, batteries, and LCDs in the automotive, industrial equipment, and consumer device sectors
Online Sales Information
Pricing: $0.6/unit (samples, excluding tax)
Availability: Now (in mass production)
Online Distributors: Digi-Key, Mouser, and Farnell
These three series are offered in the following
resistance values. (All units in mΩ)
Additional resistance values will be added as needed.
Online Distributors
(mΩ)
300, 330, 470, 510
Support Page
Product pages can now be searched by series or resistance value, and samples are available for purchase.
https://www.rohm.com/products/resistors
Terminology
Leaflet
Class-leading* 1W rated power in the 1220 sizeHigh Power Wide Terminal Thick-Film Shunt Resistors
LTR10L (PDF:900KB)
New MCR series shunt models significantly increase rated power
General-Purpose Low Resistance · High Power Shunt Resistors
MCR10L/MCR18L (PDF:1MB)
Latest News