Germany
Our Contribution in Recycling Plastic Bottle Caps to Help more People Obtain Polio Vaccinations
ROHM Semiconductor GmbH(SiCrystal GmbH) recycle caps from the plastic bottles we use each year, and donate them to a non-profit organization that helps more people in Africa to receive vaccinations against polio.

Joined in the Charity Run Event "B2RUN“
In July 2019, the charity run event "B2RUN (Business to Run)" was held in Nuremberg, Germany.
B2RUN is held in 17 cities in Germany, and 5 euros per runner will be donated to DKMS*, an organization that supports patients with blood cancer such as leukemia. In Nuremberg, 18,500 runners from 670 companies participated in this run event.
18 members from SiCrystal participated and ran through 6.3km starting from FC Nuremberg's home stadium in the heat above 30℃.
"It was a great event and with paying an extra amount per runner we support the "DKMS to fight against blood cancer. That is what the red bracelets mean." One of the members said.
ROHM Group will continue to engage in such activities and fulfill its responsibilities as a corporate citizen.
*DKMS (Deutsche Knochenmarkspenderdatei)
An NPO corporation based in Tubingen, Germany that supports blood cancer and hematopoietic stem cell transplantation.


Donation of Work Clothes and Shoes
SiCrystal selected some of the unwanted work clothes and shoes in good condition and donated them to the non-profit organization "Caritas". The donation was greatly appreciated and quickly distributed to those in need.

Tree-planting Activities on the Factory Grounds
SiCrystal planted a commemorative tree on the factory grounds to celebrate its 25th anniversary. Employees have voluntarily taken care of this tree and it has grown to a large size. An insect hotel, a hedgehog hideout, and nest boxes have also been installed to provide a place for nature observation.


Questionnaire