Part Number Search

FAQ Category 

FAQ's
Show All Answers
Hide All Answers
showing 1 to 10 of 29
  • What are some features of SiC power devices?
    • SiC features 10x the breakdown field strength compared with silicon, resulting in breakdown voltages in the thousands of volts.
      In addition, ON resistance per unit area is considerably lower, significantly improving power loss.
      In order to minimize the increase in ON resistance associated with higher breakdown voltages, silicon IGBTs are primarily used. However, SiC has been shown to provide superior high-speed switching performance.
  • What factors need to be taken into consideration when connecting SiC MOSFETs in series?
    • - The ground isolation of The upper device can only guarantee The dielectric withstand voltage
      - A floating power supply is required for series gate voltages
      - When connected in series, since The temperature coefficient of The on resistance is positive, in order to prevent thermal runaway it is necessary to consider sufficient derating
      - taking into account product variations
      - When used as A single high voltage switch in series it is recommended to implement appropriate voltage dividing measures such as inserting A large resistance in parallel
      - The switch timing must be matched to prevent destruction due to breakdown voltage
  • Why is there undershoot/overshoot of the gate signal during SiC device drive?
    • The effects of parasitic capacitance and inductance on the board can be considered a type of LC resonance. Please confirm the following items.
      1) External resistance connected to the gate drive circuit
      2) Output capacitance of the gate drive circuit
      3) Parasitic inductance of the gate drive circuit wiring
      4) SiC MOSFET gate capacitance
      5) Internal gate resistance of hte SiC MOSFET etc.
      When the resistance is small the overshoot/undershoot peak value will increase and prolong the ringing decay time.
      Also, when the capacitance is large the peak value deceases, slowing down the switching speed.
      Plus, a larger inductance will cause the inductance to rise.
  • Please explain how to mitigate overshoot and undershoot of the gate signal when using SiC products.
    • The effects of parasitic capacitance and inductance on the board can be considered a type of LC resonance.
      Please confirm the following conditions.
      1) Increased external gate resistance connected to the gate drive circuit
      2) Smaller gate drive circuit output capacitance
      3) Reduced wiring parasitic inductance of the gate drive circuit
      When the resistance is small the overshoot/undershoot peak value will increase and prolong the ringing decay time.
      Also, a higher capacitance will slow down the switching speed.
      And we recommend that the inductance be as small as possible.
  • What happens to the gate voltage drive in SiC MOSFETs and modules when deviating from the recommended values (ON time: 18 to 22V, Off time: -3 to -6V)?
    • If the drive gate voltage while ON is less than 15V it may be impossible to maintain ON operation, and when less than 14V the temperature characteristics of the ON resistance will change from positive to negative.
      As a result, the ON resistance will decrease at high temperatures, increasing the risk of thermal runaway.
      Therefore, please ensure that the voltage is greater than 15V.
      ROHM's TZDB series features a withstand voltage greater than 40V, preventing gate breakdown and ensuring worry-free operation.
      However, continuing to provide more than the rated voltage (-6V/+22V) will gradually change the threshold value due to the effects of the traps that exist on the gate oxide film interface.
      However, because the effects from threshold voltage fluctuations during momentary voltage surges (under 300nsec) are small, the acceptable range is actually -10V to +26V.
  • Is a negative bias required for the gate drive voltage in SiC MOSFETs and modules?
    • When the drain potential increases in the FET OFF state, there is a chance that the gate potential will rise due to the effects of AC coupling of the gate-drain capacitance.
      A typical example is a bridge drive connected in series.
      In order to prevent short-circuit damage due to erroneous ON, we recommend using negative bias.
      Gate potential rise can also be mitigated by adding gate-source capacitance.
      In addition, connecting a Miller clamp MOSFET between the gate and source can prevent an increase in gate potential through reliable short-circuit operation.
      However, please note that malfunctions may occur when driving the Miller clamp MOSFET due to noise.
showing 1 to 10 of 29
of 3