Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
The Industry's First Dual-Mode LPWA (Low Power Wide Area) Compliant Wireless Communication LSI
Supports both Sigfox and IEEE802.15.4k standards and expands transmission range by more than 10 times for IoT equipment
Yokohama and Santa Clara, Calif., – September 5, 2017 – ROHM Group company LAPIS Semiconductor has recently announced the availability of an RF LSI optimized for LPWA (Low Power Wide Area), which is expected to usher in a new area of wireless IoT communication.
The ML7404 is the first wireless communication LSI in the industry to feature LPWA dual-mode functionality, supporting both the Sigfox standard (subscription-based LPWA using unlicensed sub-GHz), which has been adoped in more than 30 countries and expanding in metropolitan areas including Japan, and the international protocol IEEE802.15.4K that is extremely robust against interference from the same system and has the capacity to cover more terminals under one network. This dual-mode capability enables use in a wide range of applications/specifications.
Communication modules containing this device will be released from partner companies to simplify the development of LPWA-compatible devices that contribute increased IoT adoption. In addition, the protocol stack for IEEE802.15.4k will be provided as open-source from our partner stack vendors.
In recent years, LPWA using the sub-GHz band (which is not subject to RF licensing) is attracting attention for IoT applications. However, because the specific communication protocol varies from one country/region to the next, as of yet no method has been standardized from among the diverse array of IoT networks currently in use.
LAPIS semiconductor has previously released wireless communication LSIs for sub-GHz specified low power radio base stations ahead of the competition, helping to achieve a smarter world through IoT. This time we developed an LPWA device that supports multiple methods, facilitating the early launch of IoT networks and the effective spread of applications and services.
Availability: Now
Key Features
1. Supports dual LPWA modes (Sigfox and IEEE802.15.4k) The ML7404 is a dual-mode LPWA wireless communication LSI compatible with both IEEE802.15.4k and the Sigfox standard utilized predominately in Europe.
Compatible with Sigfox Sigfox, a type of LPWA wireless communication system currently being employed in more than 30 countries around the world.
Supports IEE802.15.4k The 802.15.4k standard defined by IEEE is characterized by DSSS based on orthogonal spreading codes and features high interference tolerance from the same system compared with other spread spectrum communication methods. Plus it can accommodate more terminals under the same network. This protocol utilizes the high reliability sub-GHz band that does not require a license.
2. The industry's first hardware-based BPSK modulation circuit for Sigfox contributes to lower set power consumption
Sigfox uses the BPSK modulation method which is not employed by conventional sub-GHz communication. However, because standard Sigfox compliant LSIs do not support BPSK modulation, it is necessary to create BPSK symbol data utilizing control MCU software. Unfortunately, this requires that the control MCU be activated each time wireless communication is performed, resulting in unnecessary set power consumption. In contrast, the ML7404 integrates a BPSK modulation circuit that eliminates the need for the control MCU to operate (in the physical layer) during wireless communication, reducing system power consumption.
3. Development support An optional evaluation kit bundles sample programs (simple MAC) and various test scenarios, with reference module designs currently being prepared. In addition, full support is offered, including manuals and tools that can be downloaded from LAPIS' website (registration required). And in the future, communication modules integrating the ML7404 along with low power protocol stacks for IEEE802.15.4k will be released from partner companies.
Specifications
Parameter
ML7404
Sigfox
IEEE802.15.4k
Sub-GHz
Frequency Band
750MHz~960MHz
315MHz~960MHz
Base Modulation Method
BPSK
4GFSK/4GMSK, GFSK/GMSK, FSK/MSK
Long Distance Method
UNB
DSSS
—
Data Rate
100bps
0.625k~25kbps
0.1k~200kbps
Tx Power
Max +17dBM
Rx Sensitivity
—
-121 dBm@200kbps, 400kHz
-120 dBm@2.4kbps, 433Mhz -109 dBm@38.4kbs, 920MHz
Coding Method
NRZ, Manchester, 3 out of 6
Other
Wakeup, address filter, antenna diversity
Supply Voltage
1.8V~3.6V (1mW)
Transmission Current
34mA@20mW
34mA@20mW
34mA@20mW
Reception Current
—
13.6mA
13.6mA
Transmission Distance*
~10Km
~1Km
Sleep Current (Timer-ON)
1.2µA
Package
32pin WQFN
*May vary depending on reference values, communication conditions, and the ambient environment
Sales Plan
Part No: ML7404 Sample Availability: Now Mass Production: December 2017 Production Quantity: 100,000pcs./month Packaging: T&R (1000pcs/reel)
Recommended Applications
Gas and water meters, sensor networks, building health monitoring, smart agriculture, security systems, and other industrial applications requiring long-distance wireless communication.
Terminology
IEEE802.15.4k A long-range wireless protocol part of the IEEE family of standards. Sensitivity is improved using the direct sequence spread spectrum method (DSSS). The IEEE802 series standardizes physical layers such as wireless LAN, Bluetooth, ZigBee, and Wi-SUN.
DSSS (Direct Sequence Spread Spectrum) A type of spread spectrum method that spreads and transmits baseband signals within a wider band. Pseudo noise is frequency diffused and de-spread during reception, providing greater resistance against interference.
The Industry's First Dual-Mode LPWA (Low Power Wide Area) Compliant Wireless Communication LSI
Supports both Sigfox and IEEE802.15.4k standards and expands transmission range by more than 10 times for IoT equipment
Yokohama and Santa Clara, Calif., – September 5, 2017 – ROHM Group company LAPIS Semiconductor has recently announced the availability of an RF LSI optimized for LPWA (Low Power Wide Area), which is expected to usher in a new area of wireless IoT communication.
The ML7404 is the first wireless communication LSI in the industry to feature LPWA dual-mode functionality, supporting both the Sigfox standard (subscription-based LPWA using unlicensed sub-GHz), which has been adoped in more than 30 countries and expanding in metropolitan areas including Japan, and the international protocol IEEE802.15.4K that is extremely robust against interference from the same system and has the capacity to cover more terminals under one network. This dual-mode capability enables use in a wide range of applications/specifications.
Communication modules containing this device will be released from partner companies to simplify the development of LPWA-compatible devices that contribute increased IoT adoption. In addition, the protocol stack for IEEE802.15.4k will be provided as open-source from our partner stack vendors.
In recent years, LPWA using the sub-GHz band (which is not subject to RF licensing) is attracting attention for IoT applications. However, because the specific communication protocol varies from one country/region to the next, as of yet no method has been standardized from among the diverse array of IoT networks currently in use.
LAPIS semiconductor has previously released wireless communication LSIs for sub-GHz specified low power radio base stations ahead of the competition, helping to achieve a smarter world through IoT. This time we developed an LPWA device that supports multiple methods, facilitating the early launch of IoT networks and the effective spread of applications and services.
Availability: Now
Key Features
1. Supports dual LPWA modes (Sigfox and IEEE802.15.4k)
The ML7404 is a dual-mode LPWA wireless communication LSI compatible with both IEEE802.15.4k and the Sigfox standard utilized predominately in Europe.
Sigfox, a type of LPWA wireless communication system currently being employed in more than 30 countries around the world.
The 802.15.4k standard defined by IEEE is characterized by DSSS based on orthogonal spreading codes and features high interference tolerance from the same system compared with other spread spectrum communication methods. Plus it can accommodate more terminals under the same network. This protocol utilizes the high reliability sub-GHz band that does not require a license.
2. The industry's first hardware-based BPSK modulation circuit for Sigfox contributes to lower set power consumption
Sigfox uses the BPSK modulation method which is not employed by conventional sub-GHz communication. However, because standard Sigfox compliant LSIs do not support BPSK modulation, it is necessary to create BPSK symbol data utilizing control MCU software. Unfortunately, this requires that the control MCU be activated each time wireless communication is performed, resulting in unnecessary set power consumption. In contrast, the ML7404 integrates a BPSK modulation circuit that eliminates the need for the control MCU to operate (in the physical layer) during wireless communication, reducing system power consumption.
3. Development support
An optional evaluation kit bundles sample programs (simple MAC) and various test scenarios, with reference module designs currently being prepared. In addition, full support is offered, including manuals and tools that can be downloaded from LAPIS' website (registration required). And in the future, communication modules integrating the ML7404 along with low power protocol stacks for IEEE802.15.4k will be released from partner companies.
Specifications
FSK/MSK
-109 dBm@38.4kbs, 920MHz
*May vary depending on reference values, communication conditions, and the ambient environment
Sales Plan
Part No: ML7404
Sample Availability: Now
Mass Production: December 2017
Production Quantity: 100,000pcs./month
Packaging: T&R (1000pcs/reel)
Recommended Applications
Gas and water meters, sensor networks, building health monitoring, smart agriculture, security systems, and other industrial applications requiring long-distance wireless communication.
Terminology
IEEE802.15.4k
A long-range wireless protocol part of the IEEE family of standards. Sensitivity is improved using the direct sequence spread spectrum method (DSSS). The IEEE802 series standardizes physical layers such as wireless LAN, Bluetooth, ZigBee, and Wi-SUN.
DSSS (Direct Sequence Spread Spectrum)
A type of spread spectrum method that spreads and transmits baseband signals within a wider band. Pseudo noise is frequency diffused and de-spread during reception, providing greater resistance against interference.
Latest News