Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
The conditions listed in the upper row of the electrical characteristics table are measurement conditions common to each parameter. If separate measurement conditions are applicable they will be listed. Please check the datasheet.
Bipolar linear regulators are characterized by high withstand voltage and large current, while CMOS types feature low voltage operation and low current consumption. We are also utilizing Bi-CDMOS processes that combine low current with high withstand voltage.Related Link:Technical Document
Standard regulators are also called 3-pin regulators, with the BA178/178M series considered industry-standard products. LDO is short for 'Low Drop Out', and is characterized by a smaller input/output voltage difference vs standard regulators, making it possible to suppress power loss. In recent years, the use of LDOs that support ceramic capacitors is increasing, and models featuring low current consumption, low voltage operation, high withstand voltage, and increased miniaturization are being developed.Related Link:Technical Document
When replacing with a different output voltage the amount of amp feedback will change, making it necessary to re-confirm the stability of the output capacitor, load, temperature range, and supply voltage range. When changing packages the permissible loss and thermal resistance will change, requiring verification of heat loss under usage conditions and thermal design of the final set. In the case of replacing with characteristics-equivalent models the ESR conditions of the output capacitor may differ depending on the product, so please check the stable operating range in the datasheet.Related Link:Technical Document
The power loss Pd=(Vin-Vo)×Io+Vin×Icc, where Vin is the supply voltage, Vo is the output voltage, Io the output current, and Icc the circuit (bias) current.Related Link:Technical Document
It can be effective to change to the same product or one with similar characteristics in a larger package with higher power loss. Or if the package cannot be changed, the permissible loss can be increased by making the area of the copper foil connected to the backside heat radiating pad as large as possible, increasing the thickness of the copper foil, or using copper foil for the inner layer of the multilayer substrate. There is also a method for improving the heat sink in screw stop package products. Refer to the technical materials for details on backside heat dissipation and heat sink.
The permissible loss listed under the maximum ratings is the value at steady state. For the transient thermal resistance against transient loss, contact ROHM using the online inquiry form [Home/Technical Information/Inquiry Form]