Contact Us

Thank you your interest in ROHM. Please fill in the following information and a representative will contact you to answer your questions and provide the information you requested.
* Required Fields
Error - 15 characters or less.
Enter a first name, 15 characters or less.
Error - 30 characters or less.
Enter a last name, 30 characters or less, can include hyphens, apostrophes and spaces.
Error - 20 characters or less
Enter a company name, 20 characters or less.
Error - 15 number or less
Please enter a valid telephone number. Telephone number must be the following format
  • Within 15 Digits are allowed
Error - 50 characters or less
Enter a address, 50 characters or less.
Error - 10 characters or less
Enter a zipcode, 10 characters or less.
Error - 20 characters or less
Enter a city, 20 characters or less.
Error - Select Country Name
Select a Country Name From Dropdown
Error - Select Inquiry Type
Select a Inquiry Type From Dropdown
Error - 300 characters or less.
Enter a Description, 300 characters or less, can include hyphens, apostrophes and spaces.
Error - This field is required.
This field is required.
Error - Select Preferred Method of Contact
Select a Preferred Method of Contact From Dropdown
Reload-Capcha
Please enter the number in the image - Error (If you can not read should be updated with the button on the right)
Please enter the number in the image - Error (If you can not read should be updated with the button on the right)