Short-Range Wireless Communication

Short-Range Wireless Communication Standards

Although there is no detailed classification for short-range wireless communication, it generally refers to communication distances on the level of WPAN and WLAN.

Recently, there has been a shift to wide range communications such as FAN (Field Area Network) utilizing multi-hop technology.


Compared to single-hop where nodes communicate directly with each other, multi-hop enables communication over a wider range by transmitting data using multiple nodes.

Relay Function Single-Hop Multi-Hop

Features of Short-Range Wireless Communication

The ROHM Group offers a variety of devices and modules covering a range of short-range wireless technologies, including Bluetooth®, ZigBee®, Wi-Fi, EnOcean, and specified low power (Wi-SUN).

Here we compare features of short-range wireless communication protocols.


The graph below shows the short-range wireless standards offered by the ROHM Group, with the horizontal and vertical axes indicating the communication distance and data rate (speed), respectively.

The further to the right and up the faster the speed and greater the communication distance.

[Short-Range Wireless Communication Comparison 1]
Short-Range Wireless Communication Comparison 1
[Short-Range Wireless Communication Comparison 2]
  Bluetooth® ZigBee® Wi-Fi EnOcean Specified Low Power
Broadband Narrow Band
Frequency Band 2.4GHz 2.4GHz 2.4GHz 5.0GHz 315/868/905/
Communication Distance ~10m Tens of m Several hundred m ~200m ~1km
Transmission Speed 1Mbps~ 250kbps~ 11Mbps~ 125kbps ~9600bps 50kbps~
79 16 13 19 - 46
Transmission Time Limit No No No Yes Yes

Please refer to the next page for an explanation of modulation methods

Bluetooth® and ZigBee®

Examples of WPAN include Bluetooth® and ZigBee®. Both use the 2.4GHz band.

ZigBee® has been adopted in Japan for remote control applications that demand response.

For applications that continuously transmit data (i.e. sensor information from a gaming controller or music from a mobile device to a speaker) the fast communication speed of Bluetooth® is particularly effective.


EnOcean is a system for transmitting data wirelessly that requires no power supply or maintenance, and instead uses energy harvesting technology to generate the small amount of energy needed from the environment (i.e. light, temperature difference).

The frequency varies depending on region. In Japan this is classified as specified low power wireless using the 315MHz and 928MHz frequencies. In the US 315MHz and 902MHz are employed while the EU adopts 868MHz.


Wi-Fi utilizes the 2.4GHz and 5GHz bands and features fast communication speeds.

This, combined with a communication distance of about 100m, make it the preferred method for implementing a wireless network for connecting to the internet in the home.


This standard has been attracting increased attention since its adoption by power companies in Japan for smart meter communication.

Japan uses the 920MHz band referred to as specified low power, which is characterized by slower communication speeds than Wi-Fi but features longer communication distance, lower power consumption, simpler connection, and greater performance against obstacles.

Wireless Communication ModulesProduct Group Page