Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
ROHM’s Battery Charger IC: Powering the Latest Low-Voltage Rechargeable Batteries
November 16th, 2021
ROHM developed a battery charger IC, BD71631QWZ, designed to provide low-voltage charging of wearables like wireless ear buds and thin, compact IoT devices such as smart displays powered by rechargeable batteries.
In recent years the need for safer, higher density rechargeable batteries has led to the development of new battery types. This includes all-solid/semi-solid types models using novel materials for the electrode part and batteries that adopt different terminal compositions. However, many of the latest rechargeable batteries are small and thin, requiring low voltage charging in the 2V to 3V range. Moreover, there are currently no battery charger ICs that can handle a wide voltage range.
Based on this market demand, ROHM developed a battery charger IC that supports low voltage charging of not only li-ion, but also new types of rechargeable batteries such as all-solid and semi-solid state. The BD71631QWZ achieves low voltage charging over a wide range from 2.0V to 4.7V by improving the stability of the internal circuit.
Unlike general battery charger ICs that provide a fixed voltage, ROHM’s new product allows the charge voltage to be easily set by simply changing the external resistor, reducing design load when changing batteries. Additionally, original package technology results in a compact package just 0.4mm thickness, which is 60% lower than conventional products in market. This is contributing to smaller, thinner devices. In addition, each charging characteristic like charge/termination current can be set for CCCV charging, providing an optimal charging environment for thin, compact IoT and wearable devices utilizing the latest rechargeable batteries.
Going forward, ROHM will continue to contribute to providing greater application convenience by supplying more efficient charging solutions.
Key Features
1. Compatible with new all-solid/semi-solid state rechargeable batteries requiring low voltage charging
The BD71631QWZ allows the charging voltage to be easily set from 2.0V to 4.7V by simply changing the external resistor, ensuring compatibility with not only single-cell li-ion batteries, but also all-solid/semi-solid and other new rechargeable battery types that demand low voltage charging.
2. Package size optimized for applications equipped with thin rechargeable batteries
ROHM’s new product utilizes original package technology to achieve a thin, compact 1.8mm × 2.4mm × 0.4mm form factor. As a result, mounting height has been reduced by 60% and footprint by 50% compared to standard products in a 3.0mm × 3.0mm × 1.0mm package. Ensuring that the height is the same as peripheral components contributes to smaller, thinner devices. This makes it particularly suitable for wearables and compact IoT devices equipped with ultra-thin sheet-like rechargeable batteries.
3. Achieves optimal CCCV charging according to the characteristics of the rechargeable battery
The BD71631QWZ enables the charge characteristics to be independently set, like charge current/voltage, termination current, recharge voltage for CCCV using an external resistor to achieve optimal charging based on the characteristics of rechargeable batteries. In addition, even if the battery needs to be changed during application design, it can be designed without reselecting components, reducing the number of workload required. Moreover, reducing the battery standby current down to 0μA in the standby state and incorporating various protection functions contributes to longer operating times in devices equipped with rechargeable batteries and improved safety during charging.
New Rechargeable Batteries:
Compact rechargeable batteries (i.e. all solid-state, semi-solid state) equipped with new materials for the electrolyte and electrodes to achieve higher safety and density.
CCCV Charging:
A charging method that switches between CC charging, which charges with a constant current to prevent overcurrent charging, and CV that charges with a constant voltage to prevent overcharging, depending on the voltage of the rechargeable battery.
ROHM’s Battery Charger IC: Powering the Latest Low-Voltage Rechargeable Batteries
November 16th, 2021
ROHM developed a battery charger IC, BD71631QWZ, designed to provide low-voltage charging of wearables like wireless ear buds and thin, compact IoT devices such as smart displays powered by rechargeable batteries.
In recent years the need for safer, higher density rechargeable batteries has led to the development of new battery types. This includes all-solid/semi-solid types models using novel materials for the electrode part and batteries that adopt different terminal compositions. However, many of the latest rechargeable batteries are small and thin, requiring low voltage charging in the 2V to 3V range. Moreover, there are currently no battery charger ICs that can handle a wide voltage range.
Based on this market demand, ROHM developed a battery charger IC that supports low voltage charging of not only li-ion, but also new types of rechargeable batteries such as all-solid and semi-solid state. The BD71631QWZ achieves low voltage charging over a wide range from 2.0V to 4.7V by improving the stability of the internal circuit.
Unlike general battery charger ICs that provide a fixed voltage, ROHM’s new product allows the charge voltage to be easily set by simply changing the external resistor, reducing design load when changing batteries. Additionally, original package technology results in a compact package just 0.4mm thickness, which is 60% lower than conventional products in market. This is contributing to smaller, thinner devices. In addition, each charging characteristic like charge/termination current can be set for CCCV charging, providing an optimal charging environment for thin, compact IoT and wearable devices utilizing the latest rechargeable batteries.
Going forward, ROHM will continue to contribute to providing greater application convenience by supplying more efficient charging solutions.
Key Features
1. Compatible with new all-solid/semi-solid state rechargeable batteries requiring low voltage charging
The BD71631QWZ allows the charging voltage to be easily set from 2.0V to 4.7V by simply changing the external resistor, ensuring compatibility with not only single-cell li-ion batteries, but also all-solid/semi-solid and other new rechargeable battery types that demand low voltage charging.
2. Package size optimized for applications equipped with thin rechargeable batteries
ROHM’s new product utilizes original package technology to achieve a thin, compact 1.8mm × 2.4mm × 0.4mm form factor. As a result, mounting height has been reduced by 60% and footprint by 50% compared to standard products in a 3.0mm × 3.0mm × 1.0mm package. Ensuring that the height is the same as peripheral components contributes to smaller, thinner devices. This makes it particularly suitable for wearables and compact IoT devices equipped with ultra-thin sheet-like rechargeable batteries.
3. Achieves optimal CCCV charging according to the characteristics of the rechargeable battery
The BD71631QWZ enables the charge characteristics to be independently set, like charge current/voltage, termination current, recharge voltage for CCCV using an external resistor to achieve optimal charging based on the characteristics of rechargeable batteries. In addition, even if the battery needs to be changed during application design, it can be designed without reselecting components, reducing the number of workload required. Moreover, reducing the battery standby current down to 0μA in the standby state and incorporating various protection functions contributes to longer operating times in devices equipped with rechargeable batteries and improved safety during charging.
Product Lineup
BD71631QWZ
1 to 100 (VIN≥4V)
1 to 30 (2.9≤VIN≤5.5V)
Thermal Protection
Under Voltage Lock Out
Overvoltage Protection
Battery Temperature Detection*
(1.8x2.4x0.4)
*Requires an external NTC thermistor
Online Sales Information
Pricing: $0.93/unit (samples, excluding tax)
Availability: In mass production
Online Distributors
Application Examples
Evaluation Board
Sales Launch Date: July 2021
Online Distributors: Digi-Key, MOUSER, and Farnell
Evaluation Board Part No: BD71631QWZ-EVK-001
User Guide: https://www.rohm.com/products/power-management/battery-management/battery-charge-management-ics/bd71631qwz-product#evaluationBoard
Terminology
New Rechargeable Batteries:
Compact rechargeable batteries (i.e. all solid-state, semi-solid state) equipped with new materials for the electrolyte and electrodes to achieve higher safety and density.
CCCV Charging:
A charging method that switches between CC charging, which charges with a constant current to prevent overcurrent charging, and CV that charges with a constant voltage to prevent overcharging, depending on the voltage of the rechargeable battery.
Latest News
METI recognizes joint plan as supporting stable, sec ...