Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
The Industry's First* Speech Synthesis ICs Dedicated for AVAS (Acoustic Vehicle Alerting System) in xEVs Optimized hardware configuration and GUI software significantly reduce development load
The ROHM group company LAPIS Technology has developed the industry's first speech synthesis ICs - ML22120xx series (ML22120TB, ML22120GP) - designed for AVAS in xEVs (electric vehicles).
In order to achieve a carbon neutral (decarbonized) society, the number of hybrid and electric vehicles that silently operate on motor power continues to increase - prompting AVAS regulations to be enacted requiring warning sound to be emitted to alert pedestrians of their approach. However, when generating warning sound using an MCU, the pitch and volume must be smoothly controlled and characteristics adjusted to match the vehicle geometry. This increases MCU software development load requiring verification with other software processes inside the MCU. In response, LAPIS Technology released new products that contribute to reducing the burden of AVAS development by leveraging experience and technology with speech synthesis ICs. The aim: achieving a high-fidelity sound using a novel hardware-based configuration.
The ML22120TB and the ML22120GP integrate hardware functions that include a warning sound generator, fader, and equalizer. Unlike MCU-based designs, the hardware configuration eliminates the need for software validation - significantly reducing development time. At the same time, dedicated GUI software makes it easy to comply with regulations for volume and frequency characteristics required for AVAS.
The system of new ICs can be controlled by simple commands, allowing warning sound to be started in less than one-tenth the time of conventional MCU-generated systems. An included fault detection function detects both erroneous communication with the main controller and erroneous oscillation caused by external components - contributing to vehicle reliability.
An evaluation board along with a Sound Device Control Kit [SDCK3] that includes dedicated GUI software are available, enabling easy evaluation of everything from sound generation to correction and trial listening of alert sounds.
Online Sales Information
Online Distributors:DigiKey, Mouser and Farnell Pricing: $7.0/unit (samples, excluding tax) Availability: Now (OEM quantities)
The products and evaluation board will be offered at other online distributors as they become available.
A function that displays graphics and images on the computer screen to enable easy operation using a mouse or touch panel.
AVAS Regulation
The mandatory implementation of Acoustic Vehicle Alerting System (AVAS) was adopted by the United Nations Economic Commission for Europe’s (UN/ECE) World Forum for Harmonization of Vehicle Regulations (WP29) under UN Regulation No. 138 on Quiet Road Transport Vehicles. This regulation stipulates the volume of warning sound for approaching vehicles and frequencies at certain vehicle speeds.
The Industry's First* Speech Synthesis ICs Dedicated for AVAS (Acoustic Vehicle Alerting System) in xEVs
Optimized hardware configuration and GUI software significantly reduce development load
*LAPIS Technology January 17th, 2024 study
January 17th, 2024
The ROHM group company LAPIS Technology has developed the industry's first speech synthesis ICs - ML22120xx series (ML22120TB, ML22120GP) - designed for AVAS in xEVs (electric vehicles).
In order to achieve a carbon neutral (decarbonized) society, the number of hybrid and electric vehicles that silently operate on motor power continues to increase - prompting AVAS regulations to be enacted requiring warning sound to be emitted to alert pedestrians of their approach. However, when generating warning sound using an MCU, the pitch and volume must be smoothly controlled and characteristics adjusted to match the vehicle geometry. This increases MCU software development load requiring verification with other software processes inside the MCU. In response, LAPIS Technology released new products that contribute to reducing the burden of AVAS development by leveraging experience and technology with speech synthesis ICs. The aim: achieving a high-fidelity sound using a novel hardware-based configuration.
The ML22120TB and the ML22120GP integrate hardware functions that include a warning sound generator, fader, and equalizer. Unlike MCU-based designs, the hardware configuration eliminates the need for software validation - significantly reducing development time. At the same time, dedicated GUI software makes it easy to comply with regulations for volume and frequency characteristics required for AVAS.
The system of new ICs can be controlled by simple commands, allowing warning sound to be started in less than one-tenth the time of conventional MCU-generated systems. An included fault detection function detects both erroneous communication with the main controller and erroneous oscillation caused by external components - contributing to vehicle reliability.
Product Lineup
Sheet
Capacity
[Mbit]
Playback
Time [sec.]
Frequency
[kHz]
of Mixing
(Internal) [ch]
Temperature
[°C]
[mm]
Grade
Max. 128
Clock
synchronous
serial
to
+105
(9.0×9.0×1.2)
(4.0×4.0×0.8)
Note: Please contact a sales representative or visit the Contact Us page on ROHM’s website for more information on AEC-Q100.
Application Examples
Acoustic Vehicle Alerting System (AVAS), external vehicle alert sounds (sliding door open/close, charging completion), etc.
Support
Click on the link below for more information on the new speech synthesis ICs.
https://www.rohm.com/lapis-tech/product/speech/ml22120
Evaluation Board, GUI Software Information
An evaluation board along with a Sound Device Control Kit [SDCK3] that includes dedicated GUI software are available, enabling easy evaluation of everything from sound generation to correction and trial listening of alert sounds.
Online Sales Information
Online Distributors: DigiKey, Mouser and Farnell
Pricing: $7.0/unit (samples, excluding tax)
Availability: Now (OEM quantities)
The products and evaluation board will be offered at other online distributors as they become available.
Online Distributors
■ Product Information
Applicable Part No: ML22120TBZ0B-MXEvaluation Board Part No: RB-D22120TB32 - Online Distributors: DigiKey, Mouser and Farnell
Sound Device Control Kit Part No: SDCK3 - Online Distributors: DigiKey, Mouser and Farnell
Terminology
Latest News
METI recognizes joint plan as supporting stable, sec ...