Absolute maximum ratings are parameter limits that should never, under any circumstances, be exceeded. Doing so may result in component failure or, at the very least, deterioration, which will shorten life, leading to breakdown.
We must refer to the Pd-Ta derating curve for the particular model. Looking at the derating curve for the UDZS series below, at 25ºC the power dissipation is approximately 200mW, while at 87.5ºC this decreases to 100mW. The type of board must be taken into consideration as well.
This refers to the thermal resistance based on heat generated at the PN (or Schottky) junction. Specifically, Rth(j-a) is the thermal resistance from the junction to ambient and Rth(j-c) signifies the resistance from the junction to the terminal. The graph below is useful to determining Tj (junction temperature) during operation. Please note that Rth may vary depending on the size of the land pattern and board materials.
Please ensure the no stress is applied to the main body by using a chuck before bending the leads (see below). Also, please avoid bending the leads more than 90ºC and bending more than once.
Yes – for surface mount diodes. For leaded (through-hole) types, please perform flow (dip) soldering. Details are provided in the respective data sheets.
Yes, manual soldering can be performed for all diodes. However, please note that the soldering temperatures will vary depending on the package type. Please refer to the data sheets for more information.
(1)Do not store diodes under conditions that may affect solderability: •Exposure to briny/sea air or corrosive gases (i.e. Cl2, H2S, NHs3, NO2) •In areas out of the recommended temperature/humidity range (2)Solderability is guaranteed for a period of 1 year from the date of shipment from ROHM, provided that the products are stored under our recommended conditions: 5-40ºC, 30-80%RH.