Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
The output coupling capacitor requires a capacitance value of 470 μF to 1000 μF to correctly transmit the video sync signal, but a relatively small capacitance value can be achieved by using the sag corection function. For details on how to use the sag correction function, please refer to the application circuit examples and "Sag correction" in the Technical Note.
The use of a sag correction circuit may result in a response characteristic deterioration when the luminance level of the video signal changes significantly, such as white<->black, and may become out-of-sync depending on the signal reception performance of the connected device. In addition, the right side of the screen may become darker. Please determine the capacitor value after thoroughly evaluating the actual set.
It is possible, but DC current flows and each electrical characteristic tends to deteriorate slightly. For details, please refer to the Technical Note p.5, section 12 "Using after removing output coupling capacitor".