Attention to Internet Explorer users: ROHM website does not recommend browsing in IE 11. Please use latest browser to ensure the best performance on ROHM website.
The chart below shows the available products and is divided according to functions and features such as EQ (2-band, 3-band, no EQ), Power Supply (1 Positive Power Supply, 2 Positive Power Supplies, Positive and Negative Power Supplies), Surround, and Advanced Switches.
It can be connected to GND directly without a Coupling Capacitor. If a small current due to offset is a concern, connect it to GND via a Coupling Capacitor.
The ground isolation input is effective in removing Common Mode Noise superimposed on both the signal input and GND. For example, it is effective when the same noise is on the GND side and the signal side, such as when a signal from an external device is input via RCA cables.
When power is turned on, always perform system reset to initialize the registers. Be sure to set all the registers values even if they are default values.