Rohm Newslanding

Powervation Announces PowerSMART™ v1.1 Upgrade and New Firmware Release for PV3012 PMBus™ Compliant Digital DC/DC Controller

altController Firmware and Design Tool Releases Leverage the Flexibility of Digital Power Solutions to Bring DC/DC Controller Features to Market Quickly

Cork, Ireland, and San Jose, CA, February 19, 2013: Powervation Ltd (www.powervation.com), the pioneer in digital power IC solutions that deliver intelligent adaptive performance, increased system efficiency, and breakthrough design simplicity, today released PowerSMART v1.1, an updated version of their design tool, as well as, the release of a new PV3012 firmware for the PMBus compliant dual-phase digital controller.

The PowerSMART design tool allows users to communicate with and configure the Powervation digital power control ICs (e.g., PV3101 and PV3012) from their laptop using a standard USB connection. The design tool enables the user to program the controller and optimize its performance, while carefully monitoring key power supply status parameters. Designers may use the tool to make simple point-and-click or numeric entry changes to parameters and quickly configure/power-up the power supply. Additionally, users may take advantage of PowerSMART's advanced settings to access more than 60 parameters and finely tune the features to their specific needs within the GUI environment, with precision and flexibility beyond that of hardware programmed analog-based solutions. PowerSMART v1.1 builds upon the initial release of the platform introduced in 2011. The new release gives access to new parameters useful in power supply design, supports a new release of the PV3012 firmware, and provides additional flexibility and control of existing features.

Leveraging the company's core hardware and firmware technologies, Powervation's PMBus™ compliant single-phase and dual-phase digital controllers use a proprietary DSP/RISC dual-core architecture with a precision data acquisition engine running advanced control and power management algorithms in firmware. This architecture enables a rich set of features, and a high degree of flexibility within the firmware environment. The PowerSMART v1.1 release coincides with the new release of firmware for the company's PV3012 dual-phase controllers. The firmware upgrade provides additional features and flexibility related to: protection features, temperature sensing support, PMBus manufacturer specific commands, and performance enhancements for Powervation's digital stress share bus (DSS®). Additionally, users now have greater control over Powervation's Auto-Control® parameters and performance, which in demanding DDR3 and DDR4 voltage regulator designs, has proven to be an advantage for transient performance and thus BOM cost.

Comments Powervation's Director of Product Marketing, David New: "With these new releases, Powervation continues to improve upon the flexibility of our products and the features accessible with our PowerSMART design tool, while introducing greater performance for our PV3012 platform. With our recent success in DDR and our focus on high-end computing, the new firmware and design tool are designed to address the features and flexibility needed in computing, while providing a performance edge applicable in many applications."

The PV3012Q-A2 is designed to function with all leading driver and FET solutions to allow the designer maximum flexibility, powering ASICs, FPGAs, DDR memory, processors, and general POLs for networking and computing applications. The RoHS compliant PV3012Q-A2 is shipping now in 32-lead QFN packaging. The PowerSMART design tool is offered at no charge, and is available for download from the Powervation website at www.powervation.com/design-support/graphical-user-interface.

About Powervation
Powervation (www.powervation.com) delivers breakthrough Intelligent Digital Power™ IC solutions for designers of Communications, Computing, and power Point-of-Load systems. The company's digital DC/DC controllers with patented Auto-Control® technology provides intelligent adaptive compensation, delivering significant benefits in performance, efficiency, reliability and breakthrough design simplicity. Powervation is a private company backed by leading global VCs - SEP, Intel Capital, VentureTech Alliance, Braemar Energy Ventures and is headquartered in Cork, Ireland, with sales/applications offices in San Jose, California and Taipei, Taiwan.

 

Download Press Release in pdf format

 

For Further Information:

David New
Director, Product Marketing
Powervation Inc.
San Jose, CA 95134
Office: +1 408 837 0544
E-mail: david.new@powervation.com

For Press Enquiries:

Nick Foot
PR Director
BWW Communications
Henley-on-Thames, Oxfordshire, RG9 2AR
Office: +44-1491-636 393
E-mail: nick.foot@bwwcomms.com

 

Powervation Announces PowerSMART™ v1.1 Upgrade and New Firmware Release for PV3012 PMBus™ Compliant Digital DC/DC Controller