Rohm Newslanding

Latest Murata Power Solutions' DC/DC PoL Module Adopts Powervation's Digital Controller Technology

alt25 A DC/DC Module Leverages Auto-Control® for Stability & Ease of Use, While Providing Fast Transient Response and Precision Output Regulation

Cork, Ireland, and San Jose, CA, December 11, 2013: Powervation Ltd. (www.powervation.com), the leader in Intelligent Digital Power™ IC solutions, today announced that its PV3012 digital controller is being used by leading power supply innovator, Murata Power Solutions in a new DC/DC module. OKLF-T/25-W12N-C is a non-isolated, DC/DC converter delivering a maximum of 25 A at an output of 1.2 V, when operating up to 70°C with a 200 LFM airflow. The adjustable outputs provide precision regulation from 0.69 V to 3.63 V over a wide input range (6.5 V to 14 V).  The new modules are for powering the latest FPGAs and ASICs used in networking, telecom, and computing applications.

Murata Power Solutions' OKLF 25 A module, is the first device in the series and is a complete power solution that delivers ultra-fast load transient response, exceptional de-rating performance, and >90% typical efficiency in a high power density form-factor.  The module is a complete, stand-alone power supply; with the use of the PV3012 digital control IC, it provides a full-line of protection features and precision set-point accuracy. 

Comments Bill Smith, Director of Marketing, Board Mount Power, for Murata Power Solutions: "Our OKLF 25 A module extends the ease of design-in of POL converters.  With the Powervation controller, our module delivers precision set-point accuracy of ±0.5% over line, load, and temperature range – far better than analog options. Additionally, this new offering adds value by the use of space saving elevated inductors and Powervation's Auto-Control, while also achieving exceptional de-rating performance."

Powervation's Auto-Control is the industry's leading intelligent auto-tuning technology. The patented adaptive compensation technology optimizes dynamic performance and system stability in real-time without requiring any noise injection or the drawbacks of periodic techniques. This is a key benefit for modules and other designs that drive unknown or variable output loads, and addresses the challenges of load parameter drift that occurs over temperature and time. 

Comments Powervation's Vice President of Product Marketing, David New: "With the support of the Okami™ footprint and Auto-Control, the OKLF 25 A offers a solution that is stable over a wide range of applications, user loading, various capacitor types, and host board parasitics.  Additionally, many current module users following the DOSA standard are able to use this module to take advantage of the performance of digital power without redesigning their system."
 
The OKLF-T/25-W12N-C power module is available now from Murata Power Solutions.  The PV3012 and other digital control ICs are available from Powervation.

About Powervation
Powervation (www.powervation.com), the Intelligent Digital Power™ Company, delivers breakthrough intelligent digital IC solutions for designers of Communications, Computing, and power Point-of-Load systems. The company's digital DC/DC controllers with Auto-Control® technology provides intelligent adaptive compensation, delivering significant benefits in performance, efficiency, reliability and breakthrough design simplicity. Powervation is a private company backed by leading global VCs - SEP, Intel Capital, VentureTech Alliance, Braemar Energy Ventures and is headquartered in Cork, Ireland, with sales/applications offices in San Jose, California and Taipei, Taiwan.

About Murata Power Solutions
Murata Power Solutions (www.murata-ps.com) is headquartered in Mansfield, Massachusetts, with over 1,300 employees worldwide. Murata Power Solutions designs, manufactures and distributes DC/DC Converter, AC/DC Power Supply, Magnetic and Digital Panel Meter product lines, and offers these products in custom, standard and modified-standard variations. Murata Power Solutions products are typically used within electronic applications serving major global market sectors including telecommunications, computing and industrial controls.

Murata Power Solutions is a division of Murata Manufacturing Co., Ltd., a worldwide leader in the design, manufacture and sale of electronic components and power supply modules. Murata's devices are found in a wide range of applications including consumer and automotive electronics, and wireless devices. The company has employees and manufacturing facilities throughout the world.

Download Press Release in pdf format

For Further Information:

David New
Vice President of Product Marketing
Powervation Inc.
San Jose, CA 95134
Office: +1 408 837 0544
E-mail: david.new@powervation.com

For Press Enquiries:

Nick Foot
PR Director
BWW Communications
Henley-on-Thames, Oxfordshire, RG9 2AR
Office: +44-1491-636 393
E-mail: nick.foot@bwwcomms.com

 

Powervation Announces PowerSMART™ v1.1 Upgrade and New Firmware Release for PV3012 PMBus™ Compliant Digital DC/DC Controller