Rohm Newslanding

Industry's First No-Bus Self Compensating Digital Point-of-Load Modules

CUI Inc releases the industry's first self-compensating No-Bus digital point of load dc-dc module family. The modules are specifically designed for customers who value the efficiency and compensation advantages inherent in digital power but do not want to incorporate digital bus communication in their systems. The NSM2P series will allow customers to access many of the same features as a fully digital POL, however the access will be via header pins that will connect to a USB dongle and CUI's Digital Power GUI. The designer can dynamically test and manipulate the desired functions within their system, monitor the results, and set the desired fault management functions. In production, the engineering header is pulled and the specified parameters are loaded into the module by CUI based on the customer's specific requirement.

The NSM2P has the same features and functions of the recently announced NDM2P series without the need for a serial bus connection on the board, also offering true cycle-by-cycle self compensation, autonomously balancing the trade-offs between dynamic performance and system stability. With this feature, designers are able to bypass the traditional practice of building-in margins to account for factors such as component ageing, manufacturing variations, and temperature, which inevitably lead to higher component cost and longer design cycles. The NSM2P's take full advantage of Powervation's cycle by cycle self compensation feature, the module is able to dynamically set optimum stability in real time as conditions change.

electronica hall B2 at booth 518

Download pdf of the article as published in Bodo's Power Magazine