ROHM Expands Its Full SiC Power Module Lineup

New 1200V/400A and 600A models contribute to greater efficiency and miniaturization in high-power applications

ROHM New Car Audio Sound Processor

ROHM has recently announced the development of 1200V 400A/600A rated full SiC power modules [BSM400D12P3G002 / BSM600D12P3G001] optimized for inverters and converters in solar power conditioners, UPS, and power supplies for industrial equipment.

The BSM600D12P3G001 achieves a rated current of 600A by utilizing a new package featuring an original internal structure and optimized heat radiation design, enabling support for higher power applications such as large-scale power supplies for industrial equipment. In addition, switching loss is reduced by 64% (at a chip temperature of 150°C) compared with IGBT modules at the same rated current, improving energy savings considerably. And along with reducing the size of peripheral components through high-frequency operation, the effects of reducing switching loss are greater when driving at high frequencies, contributing to the miniaturization of cooling and other systems. For example, from preliminary calculations based on loss simulation in cooling systems, adopting SiC modules can reduce the size of water-cooled heat sinks by up to 88%* compared with equivalently rated IGBT modules.

In recent years, SiC has seen increased adoption in a greater number of markets, including the automotive and industrial sectors, due to its superior energy-saving performance, and products that can handle larger currents are being demanded. However, in order to maximize the high-speed switching characteristics of SiC – particularly in products with large current ratings such as power modules – it is necessary to develop a new package that suppresses the effects of surge voltage during switching.

In March 2012 ROHM was the first in the world to mass produce full SiC power modules integrating power semiconductor elements composed entirely of silicon carbide. Since then, we developed high-power products up to 1200V/300A that have been adopted in a variety of fields. These latest modules utilize a new package design that expands our SiC module lineup to cover the key current range from 100A to 600A to meet the growing demand in the IGBT market.

*1200V/600A product, PWM inverter drive, 20kHz switching frequency, less than 40um thermal grease thickness, heat sink specifications obtained from products available on the market, other temperature conditions, etc. remain the same

Availability: June, 2017 (samples and OEM quantities)

Key Features

1. Reduced switching loss contributes to greater energy savings

Achieving full SiC power modules equipped with ROHM SiC SBDs and MOSFETs makes it possible to reduce switching loss by 64% (at a chip temp. of 150°C) vs IGBTs at the same current rating. This minimizes power conversion loss in applications, contributing to increased energy savings.

Reduced switching loss contributes to greater energy savings
 

2. High frequency drive supports smaller peripheral components

Loss simulations conducted with PWM inverter drive resulted in a 30% reduction at 5kHz drive and an even more substantial reduction in total loss of 55% at 20kHz PWM vs equivalently rated IGBT modules. In the case of 20kHz operation the size of the heat sink can be reduced by 88%. High frequency drive also supports the use of smaller passive peripheral components.

High frequency drive supports smaller peripheral componets

Technical Challenges for Achieving Larger Currents

1. Reducing package inductance
Increasing the current rating of power modules also increases the surge voltage during switching, making it necessary to minimize inductance within the package. However, optimizing the internal placement of the SiC device along with terminal configuration and pattern layout allows ROHM to reduce internal inductance by 23% vs conventional products. ROHM's new G Type package suppresses surge voltage by 27% at the same loss compared with standard packages, enabling the development of 400A and 600A modules. In addition, this new package decreases switching loss by 24% under the same surge voltage drive conditions.

Switching Loss vs Surge Voltage
 

2. Improving package heat dissipation
Achieving a rated current of 600A entails not only reducing internal inductance but heat generation as well. By improving the flatness of the base plate section that significantly contributes to the heat dissipation of the module, ROHM was able to decrease the thermal resistance between the cooling mechanism and the customer's base plate by 57%.

In addition to SiC modules, ROHM also offers a gate driver board that enables quick and easy evaluation.

Case-Fin Thermal Resistance
Part NumberAbsolute Maximum Ratings (Ta=25ºC)Inductance (nH)PackageThermistorInternal Circuit Diagram*
VDSS (V)VGS (V)ID (A) [Tc=60ºC]Tj max (ºC)Tstg (ºC)Visol (V) [AC 1min.]
BSM080D12P2C0081200-6 to 2280175-40~125250025C Type
45.6 x 122 x 17mm
N/AInternal Circuit Diagram
BSM120D12P2C005120
BSM180D12P3C007-4 to 22180
BSM180D12P2E002-6 to 2218013E Type
62 x 152 x 17mm
AvailableInternal Circuit Diagram
BSM300D12P2E001300
BSM400D12P3G002-4 to 2240010G Type
62 x 152 x 17mm
BSM600D12P3G001600
 

NEW     *Chopper types also offered. Please contact a ROHM sales office for details.