Rohm Breadcrumb

Resistor manufacturing flow example

SMD Resistor
<Chip Resistor Structure>

Resistor Manufacturing Flow Example

The following illustrates the manufacturing flow of a typical SMD Resistor (MCR Series).

Raw Materials Next

In actuality the entire alumina substrate is processed at one time, but for illustrative purposes only one chip will be shown.

Printing I (Conductor/Resistive Element/Undercoat) Next Laser Trimming Next Printing II (Middle Coat/Overcoat/Marking Code) Next Bar Break/Side Electrode Formation/Chip Break Next Plating Next Resistance Measurement/External Inspection/Taping Next Shipping

What is Screen Printing?

Each layer of a ROHM chip resistor is formed by screen printing. Screen printing involves creating a print pattern on the mesh surface of a screen mask, then applying paste, then transferring the pattern onto a target object (alumina substrate) by scraping the paste with a squeegee.

Screen Printing Flow

1.A screen mask is placed on top of the alumina substrate 2.Paste is applied on top of the screen, then scraped by a squeegee screen printing 3.Printing Completed

Laser trimming

The Need for a Laser Trimming Process

Screen printing is used to form each layer of a thick film chip resistor and involves placing paste on the alumina substrate. Hundreds of chips are processed at the same time, inevitably leading to slight variations in printing conditions (i.e. paste thickness).

This results in varying resistance values, making it impossible to ensure optimum resistances. Therefore, an additional process is required to adjust the resistance values to within specified tolerances.

Laser trimming Resistance Value Distribution Graph

The Laser Trimming Process

A laser cuts the resistive element while the resistance is measured in order to achieve target resistance values with minimal variation. Laser trimming narrows the current pathway, which increases resistance. Once the target resistance has been met the laser is stopped to reduce variations between chips.

Resistance Increase Resistance Value Distribution (Before Trimming/ After Trimming)

electronics_tips_menu

Loading