Rohm Breadcrumb

pi_what3

Ir LED vs Photointerrupter

Ir LED (Infrared LED)

Ir LED (Infrared LED) is a photoelectric conversion element that converts electrical energy into optical energy, with an emission wavelength between 800nm to 950nm.

Materials used include GaAs and GaAlAs.

Infrared LED (IrLED)

Infrared LEDDownload datasheet

Photointerrupter

Since photointerrupters (or phototransistors) combine a photodiode and transistor, the base current of the transistor is input as light. Silicon with a sensitivity between 400nm and 1100nm is used.

phototransistors combine a photodiode and transistor

PhototransistorDownload datasheet

electronics_tips_menu

Loading