Rohm Breadcrumb

tc_what1(Capacitor Types)

Capacitor Basics

What is a capacitor?

With the ability to store electrical charge, block DC signals, and pass AC signals capacitors are play a pivotal role in electronic circuits.
As such they are used for backup (battery), decoupling (reduce noise), and coupling (remove DC bias voltage).
At type of passive component like resistors and inductors (coils), capacitors are used in everything from smartphones, wearables, and data centers to base stations, industrial equipment, and automotive systems.
Although the term capacitor is common in most parts of the world, in Japan it's often referred to as a condenser.

Structures and Features of Different Capacitors

Capacitors come in various types, but the basic structure consists of an insulator (dielectric) sandwiched between electrodes, capable of storing charge when a voltage is applied.
Actual products include single-layer, trench, multilayer, electrolytic, and wound types.
Capacitors can be differentiated by the following characteristics depending on the dielectric and electrode materials used.
Polarity, small/large size, thin/low-profile, operating temperature range, capacitance size, rated voltage range, high-frequency performance, capacitance stability, presence/absence of noise due to piezoelectric effects, etc.
Therefore, when selecting a capacitor, it is necessary to understand the characteristics of each type.

[Types and Characteristics of Different Capacitors】

*Scroll horizontally

  Silicon Capacitor Multilayer Ceramic Capacitor Tantalum Capacitor Aluminum Electrolytic Capacitor
Capacitor Appearance
Electrode ① Capacitor Structure  Doped silicon Nickel Tantalum
(anode)
Aluminum
(anode)
Dielectric Silicon oxide or
Silicon nitride
Temperature compensating ceramic High dielectric constant ceramic Tantalum pentoxide Aluminum oxide
Electrode ② Doped silicon Nickel Manganese dioxide
(cathode)
Conductive polymer
(cathode)
Electrolyte
(cathode)
Conductive polymer
(cathode)
Polarity No No Yes Yes
Compact × ×
Thin/Low Profile × ×
Operating
Temperature Range
Large Capacitance ×
High Rated Voltage
High Insulation
Resistance
(Low Leakage Current)
High Frequency
Characteristics
× ×
Capacitance Stability DC
Bias
×
Temperature × ×
High Reliability × ×
Noise (Ringing) No Yes No No
Advantages
  • Compact
  • Low profile
  • Good high frequency characteristics
  • High operating temp
  • High capacitance stability
  • High Reliability
  • High EMI immunity(can include TVS protection element)
  • No noise since no piezoelectric effects
  • Compact
  • Good high frequency characteristics
  • High capacitance stability
  • Compact
  • Good high frequency characteristics
  • Large capacitance in a compact size
  • High capacitance stability
  • Large capacitance in a compact size
  • High capacitance stability
  • Lower ESR and higher allowable ripple current than manganese dioxide products
  • Large capacitances
  • Broad lineup
  • Large capacitances
  • High capacitance stability
  • Lower ESR and higher allowable ripple current than electrolytic products
Disadvantages
  • Small capacitances
  • Limited lineup
  • Small capacitances
  • Ringing noise generated due to piezoelectric effect
  • Prone to cracking during substrate partitioning and temperature changes
  • Low capacitance stability
  • Ringing noise generated due to piezoelectric effect
  • Prone to cracking during substrate partitioning and temperature changes
  • Failure in short mode
  • Polarized
  • Failure in short mode
  • Polarized
  • Large product size
  • Short lifespan due to liquid leakage
  • Polarized
  • Large product size
  • Polarized

◎: Excellent 〇: Very Good △: Average ×: Poor

About Capacitance

Capacitance is a typical characteristic of a capacitor.
And is generally expressed by the following formula.
Capacitance=εr×ε0×S/d
(εr:Relative permittivity of the dielectric, ε0:Permittivity of a vacuum =8.9×10-12[F/m], S:Electrode surface area, d:Dielectric thickness)

Capacitance
Capacitor Circuit Symbol

As the above equation shows, capacitance is proportional to the surface area of the electrode and dielectric constant of the dielectric and inversely proportional to the dielectric thickness.
Relative permittivity is an inherent value of the dielectric material used.
The unit of capacitance is F (farad), and in practice pF (picofarad), nF (nanofarad), uF (microfarad), mF (millifarad), etc. are commonly used.
( 10-12[F]=1pF, 10-9[F]=1nF, 10-6[F]=1[μF], 10-3[F]=1[mF] )

Capacitor Applications

Capacitors (including tantalum) are often used in the following applications.

Backup (Battery)

Backup Application

Utilizing as a battery

When the load current increases due to power supply interruption or a sudden rise in IC drive speed, the line voltage from the power supply may drop, possibly causing IC malfunction. To prevent this, charge stored in a capacitor is supplied to the IC, temporarily maintaining the line voltage.

Decoupling

Coupling Application

Utilizing AC characteristics

To supply stable DC voltage, capacitors are used to remove high-frequency noise caused by high-speed circuit drive or externally induced noise superimposed on the power supply line. Adopted in general power supply circuits.

Coupling

Coupling Application

In this application, the capacitor removes the DC bias voltage from the previous stage and only passes through the AC signal voltage.

Typically adopted in audio circuits.

What is a Tantalum Capacitor?

Tantalum is a metal, whose name is derived from Tantalus, an anti hero from Greek mythology.
Generally, surface mount tantalum capacitors are constructed by forming electrodes at both ends of the tantalum element using a lead frame, then sealing the structure with mold resin.

Tantalum Capacitor

CapacitorDownload datasheet

electronics_tips_menu

Loading