FAQ's
Show All Answers
Hide All Answers
showing 1 to 5 of 5
  • For Composite Video Amplifier BH76106HFV, BH76109HFV, BH76112HFV and BH76206HFV,
    How is the sag terminal used?
    • The output coupling capacitor requires a capacitance value of 470 μF to 1000 μF to correctly transmit the video sync signal, but a relatively small capacitance value can be achieved by using the sag corection function.
      For details on how to use the sag correction function, please refer to the application circuit examples and "Sag correction" in the Technical Note.

      The use of a sag correction circuit may result in a response characteristic deterioration when the luminance level of the video signal changes significantly, such as white<->black, and may become out-of-sync depending on the signal reception performance of the connected device.
      In addition, the right side of the screen may become darker. Please determine the capacitor value after thoroughly evaluating the actual set.
showing 1 to 5 of 5
of 1