2017-06-14_news_astar

14 June 2017 The chip is expected to enable more efficient prediction of machine failures by processing and analyzing data gathered by sensors in real-time, paving the way for greater...

2015-01-08_news

ROHM Co., Ltd.(headquarters in Kyoto, Japan) and ROHM Group as a whole have decided to contribute 150 thousand Malaysian ringgit (about 5 million JPY) as a reconstruction support for the...

2014-12-26-malaysia

The following is a report on the status of ROHM Group production location in the area affected by flooding in Malaysia as of 18:00 JST December 26, 2014. ROHM-Wako Electronics...

2014-12-29-malaysia

The following is a report on the status of ROHM Group production location in the area affected by flooding in Malaysia as of 11:00 JST December 29, 2014. ROHM-Wako Electronics...

2015-01-05-malaysia

The following is a report on the status of ROHM Group production location in the area affected by flooding in Malaysia as of 10:00 JST January 5, 2015. ROHM-Wako Electronics (Malaysia)...

2014-02-13_news

ROHM has developed the BD5291G and the BD5291FVE   low voltage, low offset opamps which are designed to amplify signals from motion sensors such as accelerometers and gyroscopes....

2013-07-05_news

2013-07-05 ROHM Semiconductor has been honoured with the „Bosch Global Supplier Award" by Robert Bosch GmbH. ROHM received the prize in the "Electronics" category. In total, Bosch...

News_Article1

ROHM's key encoder IC can monitor up to 64 keys (8x8 matrix), making it suitable for QWERTY keyboards. Only key changes are are encoded (8bit), reducing microcontroller load...

test-News

News News of 2012 Notice Regarding Effects of Tornado in Tsukuba Ibaraki 07.05.2012 The following is a report on the status of ROHM Group production locations in the...

Higher inverter efficiency in a smaller footprint

ROHM's high voltage resistance PrestoMOS™ series is ideal for power supplies with integrated inverter. High-speed switching combined with an internal diode with high trr...
2010-01-26

ROHM has announced the development of the TCS Series of compact, low-profile, ultra-high capacitance tantalum capacitors that utilize a new package structure, resulting in an industry-leading capacitance of 4V/100µF in the 1608 size (M Case: 1.6mm × 0.8mm, h=0.8mm). 2012-size products (P Case: 2.0mm × 1.2mm, h=1.2mm) are also offered.

Bottom Electrode High Capacitance Tantalum Capacitors TCS Series (PDF:265KB)

Key Feature

  • New package structure utilized, resulting in the industry's first 100µF/4V product in the 1608 size (M Case)

Structural Comparison (M Case)

Lineup

(Package Name and Size)
  AL Case: 3.2 × 1.6 × 1.1 (mm)
  P Case : 2.0 × 1.25 × 1.1 (mm)
  M Case : 1.6 × 0.85 × 0.8 (mm)

Specifications

TCS Series: M Case (1608 Size)

Rated Voltage
(V)
Capacitance
(µF)
tanδ at 120Hz(25ºC)
(%)
ESR(at 100kHz)
(Ω)
Part No.
4 100 40 4 TCS M 0G 107□
6.3 47 40 4 TCS M 0J 476□
10 22 30 5 TCS M 1A 226□
16 10 20 6 TCS M 1C 106□

TCS Series: P Case (2012 Size)

Rated Voltage
(V)
Capacitance
(µF)
tanδ at 120Hz(25ºC)
(%)
ESR(at 100kHz)
(Ω)
Part No.
2.5 330 40 3 TCS P 0E 337□
4 220 40 3 TCS P 0G 227□
6.3 100 40 3 TCS P 0J 107□
10 47 30 4 TCS P 1A 476□
16 22 30 4 TCS P 1C 226□
20 10 20 6 TCS P 1D 106□

□ Capacitance tolerance (M:±20%)