Rohm Breadcrumb

memory_what2

Types of Memory
<Semiconductor Device Principles>

Numerous types of memory exist for Semiconductor memory Device. Basic types of memory sich as 'DRAM', 'SRAM', 'Mask ROM', 'EEPROM' and 'Flash Memory' are explained below.

DRAM

Memory Cell Structure

Consists of 1 Transistor and 1 Capacitor.

Consists of 1 Transistor and 1 Capacitor

Data Write Method

In the Case of '1':

  1. Word Line potential is High
  2. Bit Line potential is High
  3. Word Line potential is Low
1??

The state of '1'

0??

The state of '0'

SRAM

Memory Cell Structure

  • 6-Transistor Cell Configuration
  • 4-Transistor Cell Configuration (High Resistive Load Cell Type)
Low Power and High Density Types

Low Power Type to the left, High Density Type to the right.

Data Write Method (see diagram below)

In the Case of '1':

  1. Word Line potential is High
  2. Assign a potential to the Bit Line (D=Low, D=High)
  3. The state of the flip-flop
  4. Word Line potential is Low

Data Read Method

In the Case of '1':

  1. Word Line potential OFF
  2. Bit Line precharge (same potential as D, D)
  3. Word Line potential is High
  4. If the Bit Line is Low the conditions will be High
  5. Amplified by the sense amp

The state of '1' to the left, The state of '0' to the right. '0', '1' stored by the flip flop circuit

Mask ROM

Mask ROM Memory Cell Configuration

Adopts a NAND structure for increased integration (1 transistor cell).

Mask ROM Memory Cell Configuration

Data Write Method

  • Information written in the wafer process
  • '1' : Ions implanted in the transistor
  • '0' : No ion implantation

Data Read Method

  • Word line potential of the Read Cell is 0V
  • Word line potential of non-Read Cell is Vcc
  • Voltage is supplied to the Bit Line
  • '1' is determined if current flows

EEPROM

EEPROM Memory Cell Configuration

Consists of 2 transistor cells.

Consists of 2 transistor cells

Data Write Method

Data Read Method

Data Erase Method

Data Erase Method

Flash Memory

Flash Memory Cell Configuration

  • NAND Type
NAND Type

4F2 area per bit when the minimum rule is F

  • NOR Type
NOR Type

10F2 area per bit when the minimum rule is F

Data Write Method

Data Read Method

Data Erase Method

Data Erase Method

electronics_tips_menu

Loading