Facebookflickr
ROHM Worldwide >>Quick Search >>

2003 News at ROHM Electronics

News: Go to>   Current | Library

News Release

12/03
ROHM Develops DDR I and II-compatible Power IC

ROHM CO., LTD. has developed a termination regulator IC (BD3531F / BD3532F) with outstanding high-speed transient response and output voltage precision designed to be the main memory for personal computers.

As personal computers continue to get faster, the main memory needs to get faster to keep up with the accelerated CPU processing speeds, and DDR-SDRAM has taken the place of SDRAM to become the norm thanks to its capacity to read and write data at very fast speeds. That is why ROHM has developed a termination regulator IC that delivers a reliable high-speed data transfer compatible with this kind of high-speed memory.

To speed up the transfer rate, the data transfer between DDR-SDRAM and the CPU involves converting the amplitude of the data from 2.5V to 1.25V using partial resistance (the SSTL circuit). The power is supplied by the termination regulator IC. As it is being transferred, the data undergoes extreme current fluctuation (in sending and receiving) between the high and low signals when they are in excess. If the voltage precision and the drive current orientation selection (transient response characteristics) are inadequate, there is insufficient area (amplitude) to determine whether the transfer data is high or low, and this can lead to rare instances of the wrong data being written to the DDR-SDRAM or an error.

The BD3531F / BD3532F, however, supplies sufficient current capacity (3A with the BD3532F and 1.5A with the BD3531F) to the MOSFET of the regulator output and raises the drive capacity of the termination regulator IC thanks to circuit technology. This makes high-speed transient response characteristics possible.

The termination voltage precision (VTT) has also been reduced to VREF ±30mV (about 1/3 of previous ICs), which ensures enough area to determine whether a signal is high or low and makes data transfer more reliable.

Also, the MOSFET output driver has been made with low ON resistance (200m ??typ), and the IC is compatible not only with DDR I, but also DDR II, the next-generation DDR-SDRAM standard.

Other features include: a built-in high-precision reference voltage circuit (VREF); a low-input error prevention circuit, a heat protector circuit, and a built-in enable function; and it’s ideal for notebook computers thanks to the SOP8 compact package

As the top maker of power ICs in the industry, ROHM offers a high-quality, high-reliability line-up of power ICs not only for computers, but also for AV devices, cellular phones, and more. This termination regulator IC was developed using power IC technology owned by ROHM.

Item
Specification

DDR II

DDR I

Supply voltage

1.8V

2.5V

Max. data transfer
rate per pin
(Mbits/sec)

400/533/667

200/266/333/400

 

News Release

11/03
ROHM Expands its Power Diode Lineup with 17 New Models

ROHM CO., LTD. announced the availability of 17 new power diode models. Power diodes are used for secondary-side rectification in the switching power supplies of products such as printers and power adapters.

With the RSX Series of high-performance, next-generation Schottky barrier diodes featuring low VF, low IR and high surge resistance, the RB Series of Schottky barrier diodes provide favorable overall characteristics at low IR. ROHM has expanded its catalog to offer coverage for voltages of 30 to 100 V and currents of 6 to 30 A. The new introductions represent the company's response to requests from power supply manufacturers for an expanded selection of high-performance diodes across key power regions. ROHM hopes to establish share leadership in this market by contributing to set efficiency.

The newly introduced RSX and RB Series take the performance characteristics of both series, which have already been well received in the small signal to middle power class markets and expand upon their power region coverage.

In designing these new models, ROHM deployed its proprietary fine processing technology to secure improved VF/IR characteristics - the balance of which has traditionally been a significant power diode issue. The company was able to avoid traditional trade-offs, achieving a low VF that ranks at the top of the class for power diodes (with the RSX1001T3, a reduction of about 10% compared to previous models) without sacrificing IR characteristics. The new models maintain the high avalanche tolerance and high surge voltage (about 2 times those of previous models) that have come to characterize the RSX Series.

The RB Series provides outstanding overall performance able to withstand voltages of between 40 and 100 V as well as offering improved IR characteristics, which are of key importance in power supply circuits. Regardless of the voltage rank, all new models feature specifications that are significantly improved over previous offerings while delivering top-class levels of performance in other areas.

This expansion in ROHM's lineup will contribute dramatically to the strength of the company's high-performance Schottky barrier diode offerings in the Io=30 mA to 30A range to meet customer needs and set applications that range from detection to cellular phones, printers and switching power supply current use.

ROHM has a history of leveraging its proprietary design technology, device technology, and in-house production technology in order to develop products that meet marketplace needs as quickly as possible. The company has positioned itself to respond favorably to the expectations and trust of its customers pushing ahead with products designed to complement the trend of smaller, portable and more energy-efficient sets.


News Release

9/03
ROHM Develops Industry's Top Level Speed (1.5 times quicker than conventional switching speed) Fast Recovery Diode

ROHM CO., LTD. recently completed the development of the RF073M2S (0.7 A type) and RF103L2S (1.0 A type) fast recovery diodes. These diodes used for the power supply blocks of electronic devices including plasma TV sets have a dielectric strength of 200 V and performs the industry's top level switching speed with a typical trr of 9 ns and a maximum trr of 20 ns, which is 1.5 times as short as the trr of conventional models.
Diodes with a low VF and high switching speed are in demand by the power supply blocks of a variety of electronic devices including plasma TV sets. Therefore, the fast recovery diode has been applied to these products. The fast recovery diode is a type of silicon diode with an improved short reverse recovery time (trr). Conventional fast recovery diodes have a trr ranging from 30 to 40 ns.

In order to increase the trr range, ROHM adopted a new process with optimized materials to make improvement in the trade-off relationship between the VF and trr and succeeded in the development of the RF073M2S (0.7 A type) and the RF103L2S (1.0 A type) fast recovery diodes. These diodes achieve high-speed switching with a typical trr of 9 ns and a maximum trr of 20 ns. These diodes ensure the low dissipation of power supply circuits and greatly suppress heat generation.

Features:

  • High speed: trr = 9 ns typ., 20 ns max IF = 0.5 A, IR=1 A, and Irr = 0.25*IR
  • Reverse breakdown voltage: 200 V
  • Compact packages: PMDU (RF073M2S), PMDS (RF103L2S)

ROHM has been making full use of its unique design technology, device technology and its own production technology to develop and release products to respond to market demands. ROHM will continue developing user-oriented products contributing to the downsizing of electronic devices with improvement in portability and energy-saving performance.


News Release

9/03
Industry's Top Level Super-Low ON Resistance (1/2 of conventional ON resistance) New-type Power MOS FET

ROHM CO., LTD. recently developed the RQW250N03, a power MOS FET in SOP8 that achieves the industry's top level super-low ON resistance of 2.4 m? (at an ID of 20A). In order to meet to the market demand and respond to expectations of an increase in the efficiency of the power supply with a space-saving feature, ROHM has developed the RQW250N03 as a new package device.

The power MOS FET is playing major roles in the power supply blocks of all types of applications. Due to the reduction of the operating voltage of electronic devices, in particular, there has been an increasing demand for low-voltage, high-current power supplies. The CPU of the notebook PC has the severest demand for a special power supply. There is a rapid tendency of the power supply block of the CPU to drop its output to a level as low as 1.3 V while it demands a current as high as 60A or over. With the adoption of multi-phase design, the power supply block uses a number of DC/DC converters of synchronous rectification type. As a matter of course, super-low ON resistance with a low Qgd is strongly demanded from the MOS FET units used for the synchronous rectification block. There was no single MOS FET model that achieved the required ON resistance in the past. Therefore, the conventional power supply needs two MOS FET units connected in parallel to meet the requirement.

The RQW250N03 achieves the industry's lowest ON resistance of 2.4 m?, i.e., a 50% reduction from the ON resistance (4.9 m?) of ROHM's conventional models. The RQW250N03 ensures a Qgd of 11 nC - a 20% reduction from that of ROHM's conventional models. The RQW250N03 is in a new package with a package power dissipation as high as 3 W. A single RQW250N03 unit used in the CPU power supply circuit demonstrates higher efficiency in power supply conversion than the conventional circuits that use two MOS FET units. This application has verified that the characteristics of the new package with a super-low ON resistance of 2.4 m? and a Qgd as low as 11 nC with the package power dissipation as high as 3 W has become closer to the ideal characteristics as an Nch MOS FET model used for the low-side synchronous rectification block of the DC/DC converter for the CPU power supply of the notebook-type PC excelling the characteristics of the conventional two MOS FET units. As a result, a single RQW250N03 replaces the conventional power supply circuits that use two MOS FET units connected in parallel.

The DC/DC converter of synchronous rectification type for the notebook-type PC is a typical application example of the RQW250N03. The RQW250N03 is suitable to all other applications that require super-low ON resistance as well. The RQW250N03 contributes to a reduction in the dissipation of the power supply and a decrease in loss of signal lines for a variety of applications.

The features of the RQW250N03 as a newly developed Nch MOS FET unit with super-low ON resistance include the following items.

1) A super-low ON resistance of 2.4 m? at an ID of 20 A (1/2 of ON resistance of ROHM's conventional models).
2) The Qgd as low as 11 nC (20% reduction from the Qgd of ROHM's conventional model).
3) The application of a single unit ensures power supply conversion at an efficiency rate of 80% or over (at Vout=1.3 V and Iout=20 A).
4) Compact package: SOP8
5) High heat radiation performance at a package power dissipation (PD) of 3 W (1.5 times as high as that of ROHM's conventional models).
6) Ideal for the DC/DC converter of synchronous rectification type used for the power supply of the PC.

ROHM will make use of the development technology applied to this device, further develop new MOS FET units for the high side and other circuit blocks and make efforts toward expansion of the MOS FET series to meet the market demand.


News Release

8/03
Dedicated Engine for Advanced Cellular Phones Incorporating Camera Multimedia Image Processor BU1594GS

ROHM CO., LTD. recently developed the BU1594GS, a multimedia image processor LSI. This product is a single-chip LSI designed cellular phone models that are becoming increasingly more functional with advanced features such as a camera feature. This single-chip LSI, which is ideal for flip phone models, makes it possible to process major signals in the LCD (liquid crystal display) panel (the upper panel) of the cellular phone. Therefore, the BU1594GS greatly reduces the number of wires currently necessary in cell phones. The BU1594GS will functionalize the entire cellular phone system and contribute to the efficient designing of the system.

The shipment of BU1594GS product samples started in July, and the mass production of the LSI will start in October 2003 at an initial monthly rate of one million units.

Recently, the cellular phone has incorporated advanced functions (e.g. camera, large-size LCD screen, and better image-processing) at a growing speed, which makes the internal system including the signal processing line more complicated. These advanced features greatly increase the burdens of the CPU and DSP and are becoming a large obstacle in furthering these enhancements.

The new BU1594GS is an excellent single-chip LSI that supports the system easily without imposing additional burdens to the CPU or DSP. Conventionally, the CPU, where the image signal is processed and the signal sent to the LCD panel, once captures the camera signal. Therefore, when the cellular phone is in camera mode, the CPU occupies itself with the processing of the signal. On the contrary, the newly developed LSI works as a dedicated engine, thus operating by temporarily receiving set commands (instructions) from the CPU. This means that the CPU is freed unless the CPU is making command settings, which alleviates the burdens of the CPU. As a merit, the CPU can afford to process other items. The CPU connects to this LSI through a host interface, and the LSI connects to the camera and LCD panel greatly reducing the number of wires in the hinge point. This LSI also incorporates an oscillation circuit as countermeasures against EMI (electromagnetic interference), thus downsizing the set and increasing the degree of design freedom of the hinge point.

The one-chip LSI includes the following functions. Camera interface, camera signal filter processing, image signal processing, main LCD interface, sub LCD interface, display memory, memory control, JPEG codec, backlight white LED control, illumination LED control (supporting RGB), and host interface functions.

The LSI has the following main features.

1) Displays 15 frames per second.
2) Power consumption as low as 7mW while in viewer mode (at the rate of 15 frames per second).
3) JPEG encode/decode functions are built in.
4) The JPEG compression of the VGA-size picture is possible at the rate of 15 frames per second.
5) Real-time image frame composition and overlay processing functions.
6) Provided with an LCD through mode that can be built into existing systems with ease.

The LSI has many other features as well as the above ones.

ROHM has an accumulation of high technology and know-how in the fields of the image signal processing of visual equipment along with the communications signal processing and control of communications equipment. ROHM's new product is the concentration of technologies at highly advanced levels in the respective fields.


News Release

8/03
64-Tone Polyphonic Hi-Fi PCM Sound Generator LSI Chips for Cell Phones

ROHM CO., LTD. introduces the BU8709KN, a PCM sound generator LSI capable of generating 64 hi-fi polyphonic tones at CD quality. This chip is designed for the rapidly expanding, global, multimedia cellular phone market.

There are many advantages to using the BU8709KN LSI chip in cellular phones. To start with, the number of tones available simultaneously jumped from 32 to 64 greatly increasing the range of possible ring sounds, and for CD-grade sound quality, the BU8709KN has a sampling rate of 44.1 kHz. This module also includes the industry’s first equalizer and reverb functions for cell phones by taking advantage of ROHM’s vast experience in a variety of digital and analog audio LSI chips. This feature allows users to make delicate adjustments to the sound quality of the ring tones according to the specific speakers and the housing structure of the cell phone.

Other features of the BU8709KN include 222 tones; PCM/MIDI core; sequencer core; programmable wave tones; built-in 2 channel ADPCM decoders, 1 channel ADPCM encoder, ROM, RAM, serial/parallel CPU interface, graphic equalizer, I2S digital audio output; and stereo and mono output.

ROHM, the world's largest component-only manufacturer was founded in 1958 in Kyoto, Japan. ROHM designs and manufactures integrated circuits and other electronic components including monolithic ICs, power modules, photo link modules, transistors, diodes, LEDs, LCDs, Laser diodes, thermal heads, image sensor heads, and LED displays. By building its manufacturing equipment in-house, developing highly automated production methods, and pioneering in advanced environmental friendly productions, ROHM has become a key player in custom LSI, and other semiconductor products.


News Release

7/03
IrDA Infrared Communications Module with Built-in LED Driver & Remote Control Functions

ROHM CO., LTD. introduces the RPM882-H7 IrDA infrared communications module that incorporates a built-in LED driver and remote control transmission function in a single-chip solution.

The increasing demand for using portable devices such as cell phones as a remote control for audio-visual equipment and home electronics has created a need for an IrDA infrared communications module with remote control abilities, which is why ROHM has built just such a chip.

There are many benefits of using the RPM882-H7. For one, the LED is positioned in the center of the module ensuring excellent directivity free of optical axis deviation. It also uses a GaAlAs LED with high luminous intensity, which provides a remote control distance of 9m (when the transmission LED current is 200mA). This distance is 1.8 times as long as the remote control distance of conventional models, which are approximately 5m. As a result of this feature, the current consumption is half that of conventional models making the RPM882-H7 ideal for cellular phones and PDAs that require modules with low power consumption. The single-chip package as compact as conventional models (2.2 mm high, 8.0 mm wide, and 2.9 mm deep), also makes these modules easily built into portable devices. Other features include built-in driver functions using a newly designed LSI chip and a digital interface that supports down to a minimum voltage of 1.5V.

There were two problems to be faced in building a remote control function into an IrDA communications module. The first problem was that the module had to support a transmission wavelength range of 900 to 950nm, which is different than the IrDA transmission wavelength (850 to 900nm). This caused the dispersion of directivity characteristics when two LED chips were used. The second problem was how to build the driver circuit for remote control use, which generally requires a higher current compared to the IrDA.

ROHM, the world's largest component-only manufacturer was founded in 1958 in Kyoto, Japan. ROHM designs and manufactures integrated circuits and other electronic components including monolithic ICs, power modules, photo link modules, transistors, diodes, LEDs, LCDs, Laser diodes, thermal heads, image sensor heads, and LED displays. By building its manufacturing equipment in-house, developing highly automated production methods, and pioneering in advanced environmental friendly productions, ROHM has become a key player in custom LSI, and other semiconductor products.


News Release

7/03
Supporting High-speed Communication at 480 Mbps Surge Protection Element with Industry's Lowest Capacitance Level

ROHM CO., LTD. has recently started the mass production of the RSB12JS2 surge protective element that achieves the industry's top-level capacitance of 1pF for high-speed interface applications, such as USB2.0 (at 480 Mbps). This new product is the industry's most compact multi-pin in a 1612-size package with a super-low pin-to-pin capacitance of 1pF. Its mass production has started at a monthly rate of one million units.

Presently, USB2.0 is spreading as a standard high-speed serial interface built into the PC. However, it seems that the full-fledged data transmission of peripheral devices at 480 Mbps as the highest specification of the USB2.0 has just started getting into its stride. One of the reasons is that there is difficulty in data waveform maintenance at the time of transfer and surge protection. As for medium- and low-speed USB standards at 1.5 and 12 Mbps, the required communications speeds are low with a data amplitude of 3.3 Vpp secured. Therefore, standard Zener diodes are used to provide sufficient surge protection. In the case of USB2.0 high-speed standards at 480 Mbps, however, the time constant of the surge protection circuit poses a big problem as a result of the increased communications speed with an accompanied amplitude as low as 400 mVpp. The market has been requiring a surge dielectric strength of 10kV or over and a super-low pin-to-pin capacitance of 1pF or below.

In the past, there was a problem awaiting the solution in the development of the surge protection element with super-low capacitance, i.e., the surge dielectric strength increased or decreased in proportion to the pin-to-pin capacitance. This meant that the surge dielectric strength dropped when an attempt was made to decrease this parasitic capacitance. The pin-to-pin capacitance increased when an attempt was made to maintain a sufficient surge dielectric strength. There were no surge protection elements satisfying these conflicting requirements.

To solve this problem, the RSB12JS2 surge protection element was developed with a fundamental review of the process of chip production. ROHM succeeded in developing this dedicated chip for high-speed data communication. As a result, the product offers a super-low capacitance of 1pF along with a surge dielectric strength of 10kV and over to satisfy the existing needs (IEC-6100-4-2 requirements) of the market. This product is the industry's first surge production element marketed with a capacitance of 1pF and a high surge dielectric strength of 10kV and over (Surge conditions applied: A charge and discharge capacitance of 150pF and a discharge resistance of 330 ? with 10 contact times). Other features include bidirectional for surge protection from GND and Subminiature mold model EMD6.

ROHM makes full use of its unique design technology, device technology and original production technology and responds quickly to the needs of the market. ROHM will continue the development of downsized, easy-to-carry, and energy-saving products from users' viewpoints.


News Release

6/03
First Ever Reflow Soldering-Enabled Surface Mounted Models Join ROHM's Market-Leading Lineup of LED Numeric Displays

ROHM CO., LTD. has recently developed the industry's first LED numeric displays that allow reflow soldering and automatic mounting. ROHM has released two new surface mounted LED single-digit numeric displays: the LF-301VA/VK with a peak emission wave length of 650 nm (in red) and the LF-301MA/MK with a peak emission wavelength of 563 nm (in green). The company will market anode and cathode common versions of both models for a total of four versions of the new LED. With a character height of 8 mm, the displays offer advantages in a variety of applications, including FA (factory automation), pachinko and other game machines, and ticket and vending machines. Mass production began at a monthly rate of 200,000 units this spring.

While the LED numeric format is less suited to intricate displays than LCD or organic EL technology, exceptional brightness and excellent visibility makes the LED ideal for an array of applications that require easy-to-see display.

Amid the trend toward downsizing FA equipment, most of which uses compact LED numeric displays, there has been a dramatic increase in the percentage of surface mounting components these machines incorporate. Most components aboard FA machines are the surface mounted variety with the exception of their LED numeric displays. Although demand for surface mounted LED numeric display models has been increasing as manufacturers seek to reduce production processes, the materials used in conventional versions present obstacles to their incorporation. The outer casings are melted by heat at the time of reflow soldering, while heating also softens the internal resin, putting stress on the elements, and resulting in failure of the displays to turn ON. Improving the heat resistance of these materials is the key to the widespread adoption of surface mounted LED numeric displays.

ROHM has developed a unique mixing technology for the external casings and internal resin to increase Tg (glass transition point), thus making reflow soldering possible. By improving the heat resistance of the internal resin and external casings, ROHM has sharply reduced the heat stress of reflow soldering on the internal elements of LED numeric displays enabling development of products with reflow soldered LEDs. The newly developed surface mounted LED numeric displays allow Pb-free reflow soldering. The terminals are coated with Sn-3Ag-0.5Cu solder and designed to withstand a variety of high-temperature Lead-free soldering conditions. Moreover, ROHM has adopted taping packaging that supports automatic mounting of these new models. Unlike their conventional counterparts with leads, ROHM's new LEDs do not require manual solder mounting reducing the number of mounting steps needed.

The newly developed surface mounted LED numeric display models offer a number of outstanding features:

  1. First models in the industry to support reflow soldering at a recommended peak temperature of 250°C and a peak time of 5s.
  2. Four versions in the model lineup: LF301VA/VK (anode/cathode common) single-digit display models (in red) and LF-301MA/MK (anode/cathode common) single-digit displays models (in green) , all with a character height of 8mm.
  3. Support lead-free soldering.
  4. Enable automatic mounting due to the adoption taping packaging.

ROHM has deployed unique semiconductor and surface mount package technologies in its efforts to meet the needs of the optical semiconductor element markets. ROHM will continue developing innovative products, cutting edge technologies and optical devices to increase customer satisfaction.


News Release

6/03
Breakthrough Rectifier Diode from ROHM Offers Top-Class Surge Resistance for On-Vehicle Applications

ROHM CO., LTD. is now mass-producing its new RR264M-400 rectifier diode, which achieves superior surge resistance in a 2616-size package. The compact RR264M-400 has a forward current of 1.0A and a reverse voltage of 400V, specifications that make it an excellent choice for applications that require surge protection, such as on-vehicle devices and digital cameras. Mass production began at a monthly rate of two million units this spring.

In the automobile industry, a major market for rectifier diodes, manufacturers have been adding functionality to cars with a variety of new features from safety devices like SRS dual airbags to cruise control, ETC and car navigation systems for greater driving ease and convenience. As the automobile becomes multi-functional, the number of modules incorporated will continue to increase, and with it, the number of rectifying diodes for electrostatic and other surge protection. Each module, in turn, mounts more and more components. The growing need for higher-density component mounting on automobile modules is driving demand for rectifier diodes with superior overall surge resistance.

Conventional rectifier diodes may offer either excellent surge current or surge voltage strength, but not both. That is why ROHM has been working to meet the formidable challenge of simultaneously improving the surge current strength and surge voltage strength of its rectifier diodes. With the development of a new diffusion process, ROHM has now achieved a breakthrough diode with surge current strength increased to 45A some 1.2 to 2.5 times higher than conventional rectifier diodes and surge voltage strength upped to 30KV, which is approximately 1.3 to 6 times as high.

The newly developed RR264M-400 rectifying diode offers the following main features:

  1. Compact, thin-profile PMDU package (2616 size)
  2. Forward current IF=1.0A, mean rectifying current IO=0.7A, and peak reverse voltage 400V
  3. Surge current 45A (Applied condition 60 Hz/1cyc)
  4. Surge voltage 30KV (Applied condition C=100pF/R=1.5 K?)

ROHM meets the needs of the market by taking advantage of its unique design, device and production technologies in designing and manufacturing diodes. The company will continue developing products from the user's viewpoint, working to fulfill the demand for compact, portable, energy-saving consumer technologies.


News Release

5/03
Thin, Lightweight, Full-color Dot Matrix LED Units with Wide Viewing Angle Utilizing RGB Emitters

Recognized as providing an excellent interface between people and information, ROHM’s LED displays are finding widespread applications in a variety of fields, such as arrival/departure information boards at train stations, information displays on trains, and various other information board applications.

For its new LED display products incorporating RGB emitters, ROHM has developed, in addition to the three-emitting-color types, full-color dot-matrix LED units, the LPM-5123BMU652 and the LPM-1153BMU602. By making optimum use of its distinctive potting lens development technology, we achieved high readability and high viewing contrast compared with conventional products.

By incorporating a 1,024-level grayscale driver for each color of red, green and blue, these modules are capable of producing a maximum of one billion colors for more realistic colors. It is expected that, besides conventional information board applications, they will also find an application in large displays for video images and the like.

ROHM's full color dot matrix units are ideal for train schedule displays, and message boards and graphic displays.

With 1024 gray levels per each color, wide viewing angle, thin structure and high contrast.