Facebookflickr
ROHM Worldwide >>Quick Search >>

2001 News at ROHM Electronics

News: Go to>   Current | Library

News - Archive 2001


11/01
AC/DC Converter Provides Regulated DC Output Without a Transformer

San Diego, California - ROHM Electronics, announced the introduction of the BP5038 series of power modules, which provide regulated 5V, 12V and 24V DC output without using a transformer. The form factor of the 4-pin SIP package is only 18 by 16.8 by 9.1 mm, reducing the footprint by a factor of 4 and the weight by a factor of 30 compared to a transformer-based power supply. Since no transformer is used, the power supply board is less vulnerable to splitting and cracking from impact or shock. The new hybrid device handles a wide range of input voltages, from 80 to 120 Vrms for AC voltage conversion. It provides a simple and inexpensive power supply for gas and smoke alarms, DC motors, sensors, microcomputers, relays, LEDs, vacuum cleaners, air conditioners, air purifiers, humidifiers, dehumidifiers, lighting devices and other electronic devices.

One of Rohm's chief advantages in the DC converter market is that it makes nearly all of the components used in the device, such as resistors and switching diodes. "The fact that we produce nearly all the components for the device eliminates supplier margins and helps us deliver the product at an extremely competitive price without worries about supply chain disruptions," said Mark Dorais, Product Engineer for Rohm. "The fact this is a hybrid device also lowers assembly cost by reducing the need for discrete components.

"The new hybrid regulator makes it possible to configure a DC power supply with just a few external components that are relatively inexpensive and small in size. Conventional regulators require large smoothing capacitors and a heat sink while the new Rohm device uses tiny capacitors and does not require a heat sink. Rectifying diodes selected for uses with the new converter have a reverse voltage rating of 400V or higher, average rectifying current of 0.5A or higher and forward surge current of 20A or higher. using a larger capacitor for input voltage smoothing produces a more stable output voltage, but increases the surge current when the power supply is turned on.

The capacitor should be able to withstand peak voltages of at least 200V. The capacitor used for output voltage smoothing should have a low effective series resistance. Capacitors designed for low-impedance switching power supplies are especially suitable.Samples of these products are currently available. Pricing starts at $1.39 each in quantity of 1000. Delivery is 8-12 weeks ARO.ROHM, the world's largest component-only manufacturer was founded in 1958 in Kyoto, Japan. ROHM designs and manufactures integrated circuits and other electronic components including monolithic ICs, power modules, photo link modules, transistors, diodes, LEDs, LCDs, Laser diodes, thermal heads, image sensor heads, and LED displays. By building its manufacturing equipment in-house, developing highly automated production methods, and pioneering in advanced environmental friendly productions, ROHM has become a key player in custom LSI, and other semiconductor products.


11/01
New ROHM Transient Voltage Suppression Diodes Provide ESD Protection

San Diego, California - ROHM Electronics, the world's largest diode supplier, has introduced two new transient voltage suppression (TVS) diodes (RSA 6.1EN and RSB6.8S) designed to provide noise suppression on a signal line to protect against electrostatic discharge (ESD). These new silicon epitaxial planar construction devices are offered in small packages (UMD5 and EMD2 respectively) designed specifically for surface mount applications. The new diodes offer stronger resistance to surge than ceramic capacitors and less clamping heat. Their low clamping factor and picosecond response time clamps transient pulses early and maintains them at an acceptable level for their entire duration.

Today's miniaturized electronics are increasingly susceptible to damage from voltage transients. When no problems exist, Rohm TVS diodes are basically invisible to the circuit they are protecting. They remain in a low-leakage, unbiased state presenting effectively no load to the circuit as long as the applied voltage is at or below the critical value. A transient voltage exceeding this value, typically caused by ESD, will cause the device to avalanche, beginning the clamping action across the lines to which it is connected. TVS diodes maintain the transient pulses at an acceptable level for their entire duration.

The RSA 6.1EN includes four diodes in a single 2 mm wide by 1.25 mm deep by 0.9 mm high package (UMD5) with a common anode configuration. The RSA 6.1EN has a zener voltage rating of 6.10 minimum and 7.20 maximum at 1 mA. Maximum power dissipation is rated at 200 mW, maximum junction temperature of 150°C and a typical junction capacitance of 90 pF and storage temperature between -55°C and 150°C. The device is rated for a maximum reverse current of 1 mA, forward current of 1.25V and an absolute maximum peak power of 30W for 1000 ms or 200W for 20 ms.

The RSB6.8S comes in a tiny 0.8 mm wide by 1.2 mm deep by 0.6 mm high package (EMD2). This device has a zener voltage rating of between 5.780 and 7.820 volts at 0.5 mA, a maximum reverse current of 1 mA and a typical junction capacitance of 30 pF. Absolute maximum ratings are 10W peak power, 150 mW power dissipation, and 150°C junction temperature. Both storage temperature and operating temperature are rated at between -55°C and 150°C.


11/01
ROHM Introduces High Precision Tolerance Thick Film Resistors in 0402 and 0603 Packages

San Diego, California - ROHM Electronics has introduced a new line of 0.5% tolerance thick film resistors in 0402 (1005 size) and 0603 (1608 size) rectangular packages for the most demanding high-precision applications. The accuracy of the resistors is tested under JIS C 5201-1 4.5 standards in order to assure high enough accuracy for nearly any critical requirement. The thick film makes the electrodes very strong, preventing damage during soldering. The new 0402 package resistor is especially small and light, with an area that is 60% smaller and a weight that is 75% lighter than the 0603 package resistor.

The compactness of the 0402 package resistors makes them perfect for use in portable electronic equipment such as cellular telephones, personal digital assistants and portable entertainment systems. External dimensions of the 0402 package resistors are only 1.0 mm wide, 0.5 mm deep and 0.35 mm high. External dimension of the new 0603 package resistors are 1.6 mm wide, 0.8 mm deep and 0.45 mm high. The flat top of both size resistors assures positive fit in face down mounting. Both resistors are available on recyclable reels, on tape or in bulk cases.

The Ruthenium oxide dielectric used in the new resistors provides superior resistance to the elements, delivering exceptionally high reliability. The 1608 size resistors also have a resin protection coating that absorbs impact to prevent damage in automated assembly. The new resistors have a voltage rating of 50V and a power rating of 0.063 watt at 70°C. They are designed to operate at -55°C to +125°C. They have been tested under JIC C 5201 to provide guaranteed values for variation of resistance with temperature, overload, solderability, resistance to soldering heat, rapid change of temperature, endurance, resistance to solvent and bend strength.

By building key manufacturing equipment in-house and developing highly automated production methods, ROHM has become the world's largest supplier of resistors. ROHM has six production facilities located throughout the world. World class manufacturing quality, lower prices, fast delivery and a continuous supply to virtually any location in the world are among the key advantages of ROHM resistors.


10/01
ROHM Introduces Small, High-Capacity Tantalum Capacitors for Portable Equipment

San Diego, California - ROHM Electronics, has introduced a new line of very small yet high capacitance Tantalum Capacitors, TC Series. Designed specially for use in portable electronic equipment. These low impedance devices are ideal for low voltage digital circuits used in cellular telephones. The new capacitors are offered in A and P-cases. External dimensions of the P-case are only 2.0 mm long, 1.25 mm wide and 1.2 mm high. Dimensions of the A-case are 3.2 mm long 1.6 mm wide and 1.6 mm high.

The new capacitors carry capacitance values ranging from 1µF to 47 µF and have rated voltages ranging from 4V.DC to 20V.DC. They are available with ±10% and ±20% capacitance tolerance. The new capacitors are offered on 8 mm tape 180 mm ET-7200A compatible reels for use on automated assembly lines. External electrodes are coated with eutectic solder, making this product ideal for solder mounting. The operating temperature of the new capacitors is -55°C to +125°C.

The new capacitors are designed to withstand a shear force of 5 Newtons with no mechanical damage to the capacitor. They are designed for capacitance to remain in tolerance after application of a force that causes the capacitor to bend by 1 mm for 5 seconds. These new capacitors voltage derate at 125°C ranges from 2.5VDC to 20VDC. The impedance of the new TC series does not increase after soldering because of the heat resistance of the silver paste.


5/01
ROHM Introduces the IA3008-CA10 New Letter-Size 300 DPI Full-Color Image Sensor

San Diego, California - ROHM Electronics has introduced the IA3008-CA10 New Letter-Size 300 dpi full-color image sensor for color sheet-fed scanners, and multi-function scanner/printers. By using its LSI design and thermal head mounting technologies, ROHM has designed a very small and lightweight full color image sensor (size: 224W18 mm W 12 mm, weight: 65 g).

ROHM has focused its efforts on developing this innovative miniature image sensor by employing its expertise in three areas: driver LSI circuit design, high-density mounting technology, and assembly techniques. This new development follows last year's release of the full color image sensor for fax machines. This new product was developed in response to the convergence of new technology and to manufacturers' needs for advanced components for personal computers and lightweight portable data terminals.

The specific features include:
1. Internal amplifier in each sensor IC operates off single power supply (5V) for superior noise resistance.
2. LED chips provide three-color (RGB) light source for superior color reproduction.
3. Unique ROHM prism that allows for short focal lengths within the head.
4. Innovative prism structure that reduces prism height.
5. Ceramic substrate for superior temperature characteristic, which improves optical characteristics.

ROHM recognizes that printheads and scan heads are key components in the multimedia and information technologies, and has focused development on advanced products for a broad spectrum of applications, including facsimile machines, label printers, ticket-vending machines, and card printers.

ROHM Electronics supplies a wide range of ASICs, gate arrays, standard cell custom ICs, industry-standard analog and logic ICs, and hybrid circuits, as well as discrete semiconductors. ROHM Electronics also offers a full line of LEDs, LCDs, Laser Diodes, and passive components.


3/01
ROHM Introduces BU8763FV & BU8766FV Melody IC For Cellular Phones

San Diego, California - ROHM Electronics has introduced the "MIDI" BU8763FV and BU8766FV 3-frequency tone generator ICs. These new ICs were designed for cellular phones, games and PCs. Enabling cellular phones with music ringer options, by selecting pre-installed or download from web ringer music, delivering messages with music, change the ringer music as the caller-ID or for personal and seasonal occasions.

With the increasing demand for new innovative ideas for cellular phones, ROHM's new product, BU8763FV and BU8766FV can fulfill customers' demands by generating 3 frequency tones simultaneously. Tone and volume in each sound source can be controlled separately by serial control. Output is generated from sine wave and special square wave. The sine wave is a waveform driving the speaker amplifier with 3 sine waves with different frequencies provides low sound pressure. The special square wave is a waveform that can generate sound pressure.

The specific features include:
1. Tone frequency: 110Hz (low A) ~ 4186Hz (high C)
2. Fade in, fade out with envelope curve
3. 9 bit DAC
4. Built-in LPF for Smoothing (fc=20KHz)
5. 3-wire serial interface
6. Voltage 2.7V ~ 3.6V

While satisfying manufacturers and customers' great demands for cellular phone products, ROHM's is also continuing its resources for innovative ideas for new enabling technologies that deliver the ever increasing sophisticated electronic needs of consumers and businesses worldwide.

ROHM Electronics supplies a wide range of ASICs, gate arrays, standard cell custom ICs, industry-standard analog and logic ICs, and hybrid circuits, as well as discrete semiconductors. ROHM Electronics also offers a full line of LEDs, LCDs, Laser Diodes, and passive components.


3/01
Rohm, Future Agree to Widen Distribution

Semiconductor manufacturer, Rohm Electronics, San Diego, CA, and components distributor Future Electronics, Pointe Claire, QC, reached an exclusive agreement covering the Americas, which follows a North American relationship between both firms since 1995.

Rohm manufacturers power modules, LCDs, passive components, custom LSI assemblies and discrete semiconductor devices such as diodes, LEDs and transistors. Design-in services performed by Future are seen as important to the manufacturer's plans for expansion of market-share.

"Improving service to all our customers in the Americas is a constant challenge at Rohm," says Ken Sykes, senior vice-president, eastern sales division." One way to do that is to make it easier for the customers, especially the emerging and growing customers, to design-in and purchase Rohm products."


3/01
ROHM Announces Transistors in a VMT3 Package with a 44% Smaller Mounting Area

San Diego, California - ROHM has announced the availability of small signal bipolar transistors in VMT3 packages that are 44% smaller in mounting area and 30% smaller in height than ROHM's previously available transistors. The new line includes 37 different devices including both conventional bipolar transistors and digital transistors that incorporate one or two resistors, providing additional space savings. The small size of these discrete devices makes them ideal for use in portable devices such as cellular phones, Internet appliances, personal digital assistants, pagers, etc. ROHM is the largest producer of discrete transistors in the world, making it possible to provide these devices on a very cost-efficient basis.

While most functionality in portable devices is provided by integrated circuits, the majority requires a number of discrete transistors to provide miscellaneous functionality, such as converting from 3V to 5V logic. The tight space required in these devices often means that their designers configure hybrids with bare dies. The problem with this approach is that assembly costs are increased by the need for wire bonding and other additional, often manual, assembly operations. Up to now, designers had to make a hard choice between the additional costs involved in this approach and the extra space required to use conventional discrete components.

ROHM's new bipolar transistors provide the best of both of these worlds by offering NPN and PNP bipolar and digital transistors in a package that takes up not much more than the same space as a bare die ¾ when you consider the additional space required for wire bonding. The VMT3 package has a mounting area of 1.2 by 1.2 mm and a height of 0.5 mm, compared to a 1.6 X 1.6 mm mounting area and 0.7 mm height for previous small signal bipolar transistors in EMT3 packages. Typical applications of the digital transistors include driving external circuits with on-off signals. Some have a single resistor in series with the base while the others have that resistor plus another between the base and emitter. In this second example, one of the new devices can replace three traditional components. Resistor values range from 4.7 KW to 100 KW.


2/01
Single-Chip Wireless IC Leverages Audio in Conventional FM Receiver

San Diego, California- ROHM Electronics has announced the first single-chip wireless IC that enables portable devices to take advantage of the audio system in a conventional FM receiver. MP3 players, portable CD players, personal digital assistants, video game players, cell phones and other devices can be connected to a more powerful audio system without the need for cables or even a line of sight connection. The receiver is simply tuned to the same frequency as the audio link IC and the audio generated by the portable device is played by the higher-quality audio system. This new device incorporates a stereo modulator, frequency synthesizer and high frequency transmitter onto a single IC, replacing the three chips that were previously required to achieve this functionality.

Applications of the new device are limited only by the designer's imagination. An MP3 player could broadcast onto a home stereo system, dramatically improving the power and quality of the output. A portable CD player could be connected to a portable stereo. A car stereo system could be used as the audio system for a video game player. In each of these cases, no cables or physical connections are required. The FM receiver is simply tuned to the same frequency that the wireless link IC is transmitting on. Other devices that could benefit from this IC include navigation systems, personal computers, fax machines, and many others.


In the past, enabling these features required a number of components such as ROHM's BA1404/BA1405 stereo modulator IC, BU26511A phase lock loop frequency synthesizer IC, a RF oscillator circuit and various high frequency circuits. Designing the wireless link required a considerable amount of time and expertise and the attachment of multiple external components to improve sound quality. Now, ROHM has incorporated all of this functionality onto a single BiCMOS IC, greatly reducing design time and the required board real estate. The board footprint is reduced by more than half compared to conventional two-chip formats and the number of external parts is reduced by about 60%.

The new wireless audio link ICs come in three styles, BH1414K, BH1415S/F and BH1416S/F. The first IC allows the transmission frequency as well as the input level setting, monaural operation and output on-off to be changed with a serial data link from a microprocessor. The second IC allows the transmission frequency to be controlled through the serial data link. The third IC omits the serial data link, but the transmission frequency can be controlled through a X4 DIP switch array.

2/01
ROHM Broadens Microminiature Infrared Communication Modules Line with Ultra Low Power Consumption Ideal for Cellular Phones; Conforming to IrDA 1.2 (Low Power) Specifications
These micro-mini packages operate at the lowest voltage in the industry.*

ROHM CO., LTD., Kyoto-based semiconductor manufacturer, has developed the microminiature infrared data communication module RPM872-H7, which complies with IrDA 1.2 specifications, suited to cellular phones and PDAs. The RPM872-H7 operates at a lower voltage than its predecessor the RPM870-H7, a well-received standard module housed also in a microminiature package. ROHM now offers a broader line of microminiature infrared data communication modules complying with IrDA 1.2, including the RPM871-H7 developed in November 2000, which offers options for setting transmission distance.

Samples of the RPM872-H7 are scheduled to begin shipping in March 2001 (sample price: 400 yen/unit) with mass production of 2,000,000 units per month expected to commence in June 2001.

Globally proliferating cellular phones have recently become capable of sending e-mail and providing access to the Internet, functioning as PDAs. Needs have now developed for communications between cellular phones and personal computers or other PDAs, along with further needs for increased transmission distance for infrared communications and low power consumption to extend battery life. IrDA modules that respond to these market needs are increasingly in high demand.

ROHM produces microminiature infrared data communication modules as its original differentiated products, with in-house development and fabrication of all necessary semiconductors and other electronic parts, such as LSI and photodiodes, for IrDA applications, making optimum use of its engineering and manufacturing technologies based on miniaturization and reduction of power consumption. The modules are primarily intended for use in portable devices such as cellular phones and PDAs. The RPM870-H7 is the standard version. The RPM871-H7 features options for setting transmission distance. The RPM872-H7 operates at a low voltage of 2 V and supports interface with CODEC at a low voltage (1.5 V). These products can be used in a variety of applications.

ROHM's three products in the field of IrDA 1.2-compliant microminiature infrared data communication modules also offer superb communication quality at a close range in layout-limited cellular phones and notebook PCs.

Other features include:

(1) Excellent electromagnetic noise protection.
(2) Development of a micro-package (8.0 ´ 2.9´ 2.2 mm) for an 80% size reduction of ROHM's previous product.
(3) Low current consumption (at reception standby) of 75 m A
(4) Operation at low supply voltages (2.0 to 5.5 V for RPM872-H7)
(5) Coverage of transmission distance twice that required by IrDA specifications (60 cm for RPM871-H7)
(6) Other features include a built-in Power Down, which reduces current usage to 0.01 m A (Typical).
   

ROHM continues to strive to develop the high performance transmission modules that are the key devices of the digital age.

(*Surveyed by ROHM)

Outline of the physical layer of the IrDA standard
Physical layer
version
Transmission rate
(kbps)
Distance
(cm)
Date of
compilation
Radiation
intensity
(mW/sr)
Irradiance
(mW/cm2)
Switching
time
(ms)
Ver 1.0 2.4~115.2 0~100 1994.4 40~500 0.004~500 10
Ver 1.1 576~4000 0~100 1995.10 100~500 0.01~500 10
Ver 1.2 2.4~115.2 0~20
0~30
1997.10 3.6~28.8 0.009~500 0.5
Ver 1.3 576~4000 0~20
0~30
1998.10 9~72 0.0225~500 0.5

Lineup of ROHM's Microminiature Infrared Communication Modules (IrDA 1.2-compliant) for Cellular Phones

Product code Operating
supply
voltage
(V)
Transmission
distance
(cm)
Current
consumption
( µA, typ.)
Current
consumption in power-down
mode
(µA, typ.)
Feature Dimension
(mm)
RPM870-H7 2.6~5.5 30 75 0.01 Standard
version
8.0´2.9´2.2
RPM871-H7 2.6~5.5 60 75 0.01 Doubled
transmission distance
8.0´2.9´2.2
RPM872-H7 2.0~5.5 30 75 0.01 Low-voltage
operation, low-voltage
interface
8.0´2.9´2.2

Lineup of IrDA 1.2-compliant ROHM microminiature IrDA modules

12/1/00
ROHM Electronics and Future Electronics sign exclusive North American Distribution Partnership...

Nashville, Tennessee - ROHM Electronics and Future Electronics today announced an exclusive distribution agreement for the Americas, effective January 2nd, 2001. The very successful relationship between ROHM and Future Electronics in North America has resulted in the two corporations encompassing their mutual long-term business objectives of expanding ROHM's market share in the Americas. Future has been a ROHM distributor since 1995.

“Improving service to all our customers in the Americas is a constant challenge at ROHM”, said Ken Sykes, Senior Vice President of Sales. “One way of achieving this goal is to make it easier for the customers, especially the emerging and growing customers, to design in and purchase Rohm products. Future is an ideal partner to help us with that task”.“Our exclusive relationship with Rohm is an exciting development for Future Electronics, and is consistent with our strategy of providing our customers with products from a world class supplier like Rohm” said E. Stephen Segal, Future Electronics' Chief Operating Officer and Executive Vice-President. “Our success depends on providing our customers with a wide range of quality products. Rohm offers a tremendous product portfolio which will assist us in continuing to provide very high levels of service to our customers”.

Founded in 1958, ROHM is a leading semiconductor manufacturer and has gained tremendous recognition for its innovative custom LSI capabilities. All manufacturing equipment at ROHM facilities around the world are designed and developed by ROHM engineers and consequently provide this company with remarkable flexibility in output capacity.

In addition to custom capabilities, ROHM maintains its position as a high ranking manufacturer of world's most innovative discrete semiconductor products such as diodes, light emitting diodes, and transistors as well as power modules, liquid crystal displays and passive components. Future Electronics is a world leader in electronic component distribution ranked 3rd in worldwide Distribution sales. Founded in 1968, Future Electronics has emerged as one of the most important entities in the electronics distribution industry and today, is recognized around the globe as a world leader in the industry. The Company employs over 5,500 employees in 220 offices in 35 countries around the world.

12/1/00
ROHM has entered into an alliance with U.S. Cree, Inc.
ROHM files Patent Infringement lawsuits on Blue LEDs against Nichia and Nichia America Corporation

ROHM CO., LTD. (Head office: Kyoto), a manufacturer of semiconductors, agreed on December 12, 2000 to form a technical alliance with Cree Inc. (Head office: U.S.A. North Carolina, CEO: Mr. Neal Hunter, Nasdaq: Cree) in the field of GaN-based blue LEDs and blue-violet semiconductor lasers based on silicon carbide (SiC). Cree, Inc. develops and manufactures semiconductor materials, such as Blue LEDs, and has the best SiC technology in the world. On the same day, Cree and ROHM signed a 5-year exclusive license agreement granting Cree rights in certain US patent of ROHM relating to LEDs/semiconductor lasers.ROHM and Cree plan to combine the strength of their companies by merging ROHM's mass-production technology of LEDs and semiconductor lasers, Cree's world-leading SiC technology, and GaN technology possessed by the two companies. This will allow ROHM to provide highly efficient, reliable, and long lasting blue LEDs and blue-violet semiconductor lasers. GaN-based blue LEDs and blue-violet semiconductor lasers are generally based on sapphire substrates. However, blue LEDs and blue-violet semiconductor lasers based on SiC substrate have the following features:

1. High efficiency: Since SiC substrate corresponds with the crystal structure of GaN, it will make the reflection inside of the laser more efficient.

2. High reliance: Since SiC substrate has high conductivity, it can radiate heat from LEDs and lasers more efficient.

3. Reduction of chip size: Since SiC substrate has high conductivity, electrodes from both the upper and lower parts of LED and laser tips may be removed, which helps to reduce tip size.

ROHM plans to develop and manufacture GaN-based blue LEDs based on SiC substrates. With regard to blue-violet lasers, the current plan is to develop them using sapphire substrates and SiC substrates.

With the partnership of ROHM and Cree, ROHM has taken legal action against Nichia Corporation in order to protect the patents which were licensed to Cree. Accordingly.

(1) ROHM CO., LTD. has filed patent infringement lawsuits against Nichia and Nichia America Corporation in the United States International Trade Commission (ITC) and the United States District Court for the Eastern District of Pennsylvania. In its complaints, ROHM alleges that Nichia is infringing its U.S. Patents 6,084,899 and 6,115,399 by manufacturing and selling certain GaN-based LED products. The district court lawsuit seeks damages and injunction against infringement.

The subject of the patents is a structure which allows high-brightness light emitting devices by lowering the operating voltage in a light emitting semiconductor such as GaN-based blue LEDs and GaN-based blue-violet semiconductor lasers.

(2) Date of the patent infringement lawsuit: December 15, 2000 (EST).

(3) Defendant of the lawsuit: NICHIA CORPORATION (CEO: Eiji Ogawa), Anan-city, Tokushima, Japan. NICHIA - AMERICA CORPORATION, 3775 Hempland Road, Mountville, PA 17554, USA.

Cree
Location: North Carolina, U.S.A.
Representative: Neal Hunter
Sales: US$108,562,000 (Fiscal Year of 2000)
Number of Employees: 680
Establishment: 1987
Business: Cree manufactures and develop semiconductor materials and devices that use silicon carbide (SiC), and gallium nitride (GaN) and its compounds. Cree's products include blue and green light emitting diodes (LEDs), RF Power Transistors used in radio communications, SiC crystals used in manufacturing jewelry in particular, and SiC wafers used for research and development. Cree takes the initiative in developing new products based on its experience in SiC and GaN semiconductors.

1/99
ROHM Introduces a new series of Serial EEPROMs

Nashville--ROHM has announced a new line of small capacity EEPROMs-the BR93 series. Devices in the BR93 series are available with memories from 1 kbit to 4 kbit. These devices are available in both an 8-pin SOP and an 8-pin SSOP envelope, the world's smallest package for this size EEPROM.This series of super general purpose EEPROMs are suitable for memory boards, cellular telephones, smart cards, monitors, pagers, air conditioners, auto and consumer audio equipment, and other similar applications where relatively small EEPROMs are needed.

The BR93 series devices are CMOS serial input/output-type electrically erasable memory circuits (EEPROMs). Each device consists of from 64 - 256 words x 16 bits, depending on its size. Each word can be accessed individually for reading or writing.Operation control is performed using four types of commands. The commands, addresses, and data are input through the DI pin under control of the CS and SK pins. When in write operation, the internal status (READY or BUSY) can be read from the DO pin.

Because these devices use the CMOS technology, they have a very low current consumption, typically 0.5 mA when active to less than 0.4 m A when in standby mode. They are designed with an auto-increment function for efficient data dumps, and automatically erase the data in each memory cell before writing to that memory cell.

The devices also incorporate both a hardware and a software write protect mode. The BR93 EEPROMs default to the write-disabled state at power up, and have software instructions for write enable and write disable. In addition, a low voltage detector prevents write operations if the power supply voltage is low.

All devices in the BR93 series can be used for 100,000 erase/write operations and will retain their data for at least 10 years.

The BR93 1024, 2048, and 4096 bit series of EEPROMs are TTL compatible and require a 2.7 - 5.5 V supply for operation. This allows the same device to be used in both 3 V and 5 V applications. These devices can be used in ambient temperatures from -40° C to +85° C. (The non-TTL BR93LL46F/FV 1024 bit devices can be operated with a 1.8 - 4.0 V supply, and can be used in ambient temperatures from -20° C to +70° C.).

2/98
ROHM Announces a Family of Low Drop-out Voltage Regulators

Nashville -- ROHM has expanded its range of low drop-out voltage regulators (LDOs), and is now offering a series of low current (150 mA), compact size (SOT-23) LDOs suitable for portable equipment. These devices have low power consumption in the standby mode and have excellent noise ripple rejection characteristics. Low-dropout regulators are linear power supply regulators with a minimized input-to-output voltage drop. As the input supply voltage changes, the integral operational amplifier references the output voltage to a standard reference and changes the drive to the pass-through transistor to maintain a constant regulated output voltage.

This series of LDOs are offered at output voltages from 2.8 V to 5.0 V, in increments of 100 mV, with a tolerance of 2.5%. This range is being constantly expanded. In addition, an adjustable version, 1.5 V ~ 10 V (± 4%), is also available. Because of the vertical-PNP transistor structure, the input voltage can vary from 90 mV above the rated dropout voltage up to 12 V. This significantly extends the useful battery life of the application that is driven by this device.

The devices are rated for a minimum current of 150 mA, with a typical output current of 280 mA. The package power dissipation is 170 mW maximum. In addition to the normal input, common, and output pins, the BAxxxLBSG series devices have a logic-controlled standby pin that turns off the output to that part of the circuit and reduces the quiescent current to less than 10 m A, typically only 0.1 m A. This function can also be used to extend the useful battery life of the application.

One of the key features of this family of products is the excellent ripple rejection and noise characteristics. ROHM has achieved a ripple rejection ratio of 56 dB, and with the addition of an external 0.01 m F, the ripple rejection falls to a very low 66 dB. The noise voltage is typically 56 mVrms. These characteristics are critical in RF circuits where ripple rejection and noise performance are a primary concern.

Integrated into the IC is an overcurrent (short circuit protection) and a thermal shutdown circuit to protect the devices in adverse operating conditions.

This series of LDOs is offered in the 5-pin SMP5 (1.6 ´ 2.9 mm) package, a standard package size in ROHM's state of the art, fully automated, high volume manufacturing facilities. This package is about half the size of other manufacturers equivalent products and typically has a current consumption of 65 mA. It is pin-compatible with existing ROHM devices as well as other manufacturers' designs.

In addition to portable communication equipment (GSM, CDMA, PHS, PDC), applications for these devices include notebook and palmtop computers, PC peripherals, PCMCIA cards, radio-control systems, battery chargers, USBs, hard drives, scanners, and LANs. All devices may be operated in the temperature range of -55° C to +85° C.

This family of low voltage dropout regulators are available in units of 3,000 pieces per reel, starting at $0.45. Typical lead time is 8 weeks ARO.

The part number assigned to this next-generation family of LDOs is BAxxxLBSG, where "xxx" is the desired output voltage. For example, the 3.0 V regulator has part number BA030LBSG.