News at ROHM Semiconductor
ROHM AND TRANSIM LAUNCH ONLINE ELECTRONIC LABORATORY
PROVIDES CUSTOMERS WITH LEADING ONLINE DESIGN AND SIMULATION POWERED BY WEBSIM®
07.08.09
KYOTO, JAPAN and PORTLAND, OR (June 16, 2009) – ROHM Co., Ltd. ("ROHM") and Transim Technology Corporation (“Transim”) today announced the availability of ROHM Electronic Laboratory, an interactive online design support tool powered by Transim’s industry leading WebSIM® technology.
ROHM Electronic Laboratory is the first online design support tool for power management applications. The tool supports ROHM’s customers in selecting and configuring system applications using ROHM’s industry-leading regulator ICs. Within a few minutes users can access customized design schematics, design reports, and perform instant design verification based on their design requirements. This instant verification is made possible by Transim’s leading WebSIM® technology, which allows a comprehensive analysis of the design under a variety of conditions, including AC, steady state, and transient operation. In addition, realistic scenarios can be analyzed under different load settings.
In addition to ROHM’s power management products the tool offers sophisticated design solutions for ROHM’s market-leading motor driver ICs. After entering a few key design requirements, such as supply and VREF voltage, application type (i.e. PWM, battery), and output peak current, the tool suggests suitable products from ROHM’s broad IC portfolio of high efficiency H-bridge motor drivers with VREF-PWM conversion function. Based on the user’s detailed design requirements, ROHM Electronic Laboratory generates an interactive schematic complete with components that can be changed on the fly. Transim’s WebSIM® technology allows instant verification of the proposed design using powerful remote simulation capabilities. Multiple design iterations can be analyzed in minutes without the hassles of software installation and virtually no learning curve.
The resulting waveforms, such as speed plots and voltage graphs, are available for analysis in the included interactive waveform viewer. As a final step the user can print a comprehensive design report including requirements, schematic, simulation results, and BOM. Designs can also be saved in a private storage location for later use.
In addition, ROHM Electronic Laboratory offers the capability to download design schematics as well as WebSIM Connect!™, a free simulation tool.
ROHM’s Online Design Capabilities:
- Detailed Input Requirements Product Selector
- Interactive Schematic
- Interactive Waveform Viewer
- High Performance Electrical Simulation
- Design Report and Bill of Material
Availability
The Online Design Center is currently available. Logon @ http://www.rohm.com
About Transim Technology Corporation:
Transim Technology Corporation is the worldwide leader developing online design solutions to manufacturers of analog and mixed-signal products, microcontrollers motor drives and other complex technical products. Corporate headquarters are located in Portland, Oregon. For more information see www.transim.com
About ROHM Co., Ltd.:
ROHM Co., Ltd. is the industry leader in system LSI, discrete components and module products, utilizing the latest in semiconductor technology. ROHM's proprietary production system, which includes some of the most advanced automation technology, is a major factor in keeping it at the forefront of the electronic component manufacturing industry. In addition to its development of electronic components, ROHM has also developed its own production system so that it can focus on specific aspects of customized product development. ROHM employs highly skilled engineers with expertise in all aspects of design, development and production. This allows ROHM the flexibility to take on a wide range of applications and projects and the capability to serve valuable clients in the automotive, telecommunication and computer sectors as well as consumer OEMs.