ICs

Discrete
 Semiconductors

Opto Electronics

Passive Components

Modules
 (Sub Systems)

  • LAPIS Semiconductor
  • Kionix
  • Distribution Inventory Search

Tantalum Capacitors

FAQ

General

What are the features of tantalum capacitors (TCs)?

TCs are electrolytic capacitors that use tantalum as the anode material and passivated tantalum pentoxide as the dielectric. The advantages include greater capacitance per unit area and stabler voltage and temperature characteristics than large capacitance ceramic capacitors.

·Capacitor Comparison
Type Aluminum Electrolytic Capacitor Multilayer Ceramic Capacitor Tantalum Capacitor Film Capacitor
Dielectric aluminum oxide several ceramics tantalum pentoxide plastic film
Working
Voltage
4 to 400V 6.3 to 250V 2.5 to 50V 50 to 1600V
Capacitance 47 to 10000µF 0.001 to 100µF 0.47 to 1000µF 0.001 to 10µF
Advantage Wide array of
breakdown voltages
and capacitances
Good high frequency
characteristics
No polarity
Small package,
Large,
stable capacitance
High breakdown level
No polarity
Disadvantage Electrolyte leakage limits life
Large package size
There is polarity
Capacitance varies
depending on voltage
and temperature
Cracking/chipping possible
Short-circuit possible
There is polarity
Small capacitance
Less package variety
Outline

What is the difference between standard and conductive polymer TCs?

The cathode terminal material differs between the two. Standard TCs use manganese dioxide (MnO2) while conductive polymer types (i.e. ROHM's TCO/TCTO series) feature an organic substance, which is less combustible and provides much lower ESR (Equivalent Series Resistance) characteristics (typically 1/10th). This makes them ideal for high frequency and large current applications.

Conductive Polymer TC Standard TC

What is the difference between standard and open-function TCs?

An open-function TC is specially constructed using a thermally sensitive wire to connect the die to the frame that acts like a fuse to prevent smoking and possible flames from being generated due to excessive heat caused by overcurrent.


The melted wire results in an open circuit within the capacitor.

What will happen if a TC is mounted with the wrong polarity?

Since tantalum capacitors are polarity based, smoking or flaming may occur due to short-circuiting, which will generate a significant amount of heat.

Do TCs have a lifetime?

The lifetime of TCs is not clearly defined, since the normal factors that contribute to aging – drying up or leaking of the electrolyte in aluminum electrolytic capacitors.

What are the recommended storage conditions and guarantee period?

The products are guaranteed for a period of one year from the date of shipment from ROHM, provided they are stored under to following recommended conditions:

Temperature;5 to 40ºC
Humidity;30 to 70%

What are the packing specifications?

TCT/TCFG/TC series: Tape and reel (embossed tape)

TCO/TCTO series: Tape and reel (embossed tape), moisture-proof package

Are ROHM TCs compliant with the RoHS directive?

Yes. Halogen-free products are available as well.

How is the solderability of bottom-surface electrode TCs?

The terminals of ROHM’s bottom-surface electrode TCs (TCT/TCTO series) protrude slightly from the edge of the package – unlike competitor products – making it possible to form a good fillet, resulting in superior solderability and junction reliability.


Do TCs require derating?

Yes, ROHM's TCs must be derated at temperatures exceeding 85ºC (see graph below). Since the voltage supplied to the TC can take many forms and include transients (and possible overshooting), enough margin must be designed in. Many TC manufacturers are recommending using the TCs at 50% of the rated voltage.


What are the allowable levels for ripple voltage and current?

The allowable ripple voltage must take a sine wave shape (see below). For other waveform types, please contact a ROHM representative.
The permissible temperature increase due to ripple voltage/current is 5ºC max. At temperatures above this level the dielectric will begin to deteriorate, resulting in possible short-circuits.

In order to determine the limits for the allowable ripple voltage at high temperatures, please refer to the following formulas:
  E=allowable ripple voltage
E Max.(at50ºC)=0.7×E Max.(at 25ºC)
E Max.(at85ºC)=0.5×E Max.(at 25ºC)
E Max.(at125ºC)=0.3×E Max.(at 25ºC)

What is the current limit?

The allowable ripple current is calculated from the following formulas, which take into account ESR and power dissipation, which differ depending on the package type.

P=I2R
I = √(P/R)

Please contact us for the ESR and power dissipation values.

Multi-layer ceramic capacitors

What temperature-based advantages do tantalum capacitors provide over multilayer ceramic capacitors?

Multilayer capacitors tend to decrease in capacitance as the temperature changes. TCs, on the other hand, are extremely stable under temperature fluctuations (see graph below), simplifying designs.


Do tantalum capacitors have advantages when it comes to voltage characteristics compared with multilayer ceramic capacitors?

Yes. Since multilayer ceramic capacitors are effectively piezoelectric devices, the capacitance may decrease when certain voltages are supplied. Furthermore, this behavior varies between production lots and manufacturers, making it impossible to predict. This can lead to IC malfunctions – one reason many users are switching to TCs.


Do TCs make sounds like multilayer ceramic capacitors?

No. Multilayer capacitors, being piezoelectric devices, tend to vibrate at specific voltages. This, along with possible sympathetic vibration with the circuit board, can cause sound generation. TCs, on the other hand, do not vibrate at different loads and voltages, making them ideal for audio/visual applications.

 Tantalum Capacitors