ICs
Discrete
|
ResistorsFAQShould the power dissipation value be considered a ‘peak’ or ‘effective’ value?Consider this the ‘effective’ value when used with commercial frequencies (50Hz/60Hz in Japan) and ‘peak’ value otherwise. Where are the resistors manufactured?We have 5 manufacturing facilities in Asia: Japan (Fukuoka), Philippines (Manila), Thailand (Bangkok), Korea (Daejeon), and China (Tianjin). What is ROHM's definition of the ambient temperature in the derating curves?ROHM defines the ambient temperature as the temperature surrounding a an isolated (unconnected) resistor based on a number of factors. For reference, we list the following excerpts from JIS (Japanese Industrial Standards) defining ambient temperature (similar to IEC 68-3-1 and 68-3-1A). [Source: JIS Handbook ‘Electronic Test Methods: JIS C 0010 Environmental Test, Part 1 – General and Guidance (IEC60068-1:88)].
JIS C 0095 Background Information, Section One – Cold and Dry Heat Tests
How is failure rate of chip resistors calculated ?According to MIL standards established by the Pentagon in the US, chip resistors are in the RM class, meaning the failure rate is calculated by the following formula:
What is the structure of the chip resistor electrodes and how are they plated?Rectangular chip resistors possess two electrodes consisting of three layers over a ceramic substrate (alumina). The bottom layer is a silver-based thick film material, the middle is composed of nickel, and the top layer is tin. Please note that all ROHM chip resistors are lead-free. What are the results of whisker studies?ROHM performs 3 types of tests:
What is the resistance value of ‘jumper’ chip resistors?Ideally jumper resistors have no resistance. However, every conductive element possesses a certain level of resistance. ROHM's jumper resistors normally have a resistance less than 50mΩ. What are the recommended soldering conditions for chip resistors?Please refer to the ‘Soldering Conditions’ section on our website for details. Generally, Pb-free solder paste (Sn-3Ag-0.5Cu) should be used. Flow and manual soldering is not recommended for ultra-compact chip resistors (0201 size) or chip networks (0402×2, 0402×4, 0603×2, 0603×8) due to possible solder bridging. However, if such methods will be used, ROHM recommends thorough testing under actual conditions before mass production.
How do you calculate the pulse current limit for chip resistors?The pulse limit is determined from the rated current or the maximum voltage per element, regardless of pulse time. In the case of a single pulse (one time voltage pulse), reference data is available. For continuous pulse operation data can be provided upon request. |
|