ICs
Discrete
|
High Performance Class-D Speaker Amplifier SeriesFAQGeneralWhat's a Class D speaker amp and how does it differ from an analog amp?The Class D speaker amp's drive output stage utilizes high efficiency PWM drive (H or L) based on the output signal level. This results in low power loss and high efficiency (85-90%).In contrast, conventional analog amps feature Class AB output, requiring (among other things) a bias current. The result is low efficiency and high heat generation, requiring an external heat sink. What is ROHM's Class D speaker amp lineup?A number of amps are offered, from 2W types optimized for portable electronics to 20W Class products designed for LCD TVs. What are the main features of ROHM's Class D speaker amps?Besides high efficiency and low heat generation, ROHM Class D speaker amps provide a number of advantages:
Is an output LC filter required?Based on the application a simple filter (i.e. ferrite beads, ceramic capacitor) can be used. For example, active speakers used for compact LCDs or iPod docks are products that use short speaker cables, while large-screen LCDs require longer speaker cables, resulting in the generation of unwanted radiation (EMI) requiring countermeasures (i.e. filters). Is a heat sink required?No. Applying solder between the backside and substrate will enable operation up to 20W+20W. Can a 10W+10W product be used for 20W+20W output?Of course. What is BTL output method?It is the abbreviation of Bridge Tied Load. What is the input type? Can the single be input?Analog input.
Is external parts/boot sequence necessary to decrease pop sound?Unnecessary. How about the package?Wafer Level CSP product (Min 1.5mm mouth) is best for the application as cellular phone etc that especially high density are demanded. Moreover, there are some space on PCB, and we also prepare usual plastic molding products with eight pins VSON packag for the customer who wants it. Is the back of the package connected internally to any pins?The back of the package is a heat sink and is not connected internally to any pins. In order to maximize thermal dissipation, it should be connected to ground on the board. Please explain the method of selecting the resistor and capacitor for output power control.This function prevents damage to the speaker due to excessive output. The circuit constants will vary based on the supply voltage, load, and other factors. Therefore, please inquire separately. How do you measure distortion?
In order to measure the distortion of a Class D speaker amp, first the PWM output signal (digital) must be converted to analog. DSP built in for digital input compatibilityWhy is a DSP built in? And what are the advantages? (Applicable model: BM5446EFV)LCD TVs are not only getting larger, they are becoming increasingly thin as well.
Is a DSP required in the Class D amp side if one is already included in the AV processor (scaler) side? (Applicable model: BM5446EFV)The main function of the AV processor is for image processing. Therefore, the audio processing capabilites of most AV processors is insufficient. In addition, the processing capability may not be enough to prevent audio degradation in thinner speakers. Is ROHM's original P2Audio function royalty-free? (Applicable model: BM5446EFV)Yes What are the advantages of the output feedback circuit? (Applicable models: BM5446EFV, BD5446EFV)Not utilizing an output feedback circuit may adversely affect the PWM signal amplitude in the event of power supply fluctuation. Oftentimes, this results in speaker noise. |
|