ICs

Discrete
 Semiconductors

Opto Electronics

Passive Components

Modules
 (Sub Systems)

  • LAPIS Semiconductor
  • Kionix
  • Distribution Inventory Search

Reversible Motor Drivers for Brush Motors

FAQ

What is reversible?

The DC motor with the brush can be controlled by a forward-rotation and reverse-rotation.
Because the transistor that works as a switch is composed by H type, it is called H-bridge.
Moreover, it is only called the bridge driver and the motor reversing driver.

Can the PWM control signal be input?

The PWM control signal cannot be input.
Please examine H-bridge driver series that PWM can control.

What is variable VREF?

The output voltage setting function enables setting of the output voltage (motor revolution speed), regardless of the power supply voltage.

What is the cross conduction prevention circuit?

It is a circuit that prevents a certain power transistor being turned on at the same time in the top and bottom of the output stages.
It achieves by adding the circuit delayed at time to have decided standing up of the voltage of the base of the transistor by which the output became "H" state by an external capacitor, and the penetration current can be decreased sharply.

How much waiting time is necessary for changing a forward-rotation and reverse-rotation?

When the direction of the rotation is switched with the motor rotates, should once by way of the state of the brake or the opening.
The following are recommended at time passing.
•When pass the brake: More than time that the voltage of output L side terminal becomes the potential of GND or less when the brake operates.
•When opening pass: 1ms or more.

Should the outside put up the Back-EMF absorption (for serge absorption) diode?

Diode is not necessary.
However, when the absolute maximum rating of driver IC might be exceeded, some, physical countermeasures (Clamp it by external Zener Di) are necessary.

What is 1.5ch?

This term is used becaause the circuit configuration is positioned between one channel and two channels.
Two motors cannot be driven at the same time.

Reversible Motor Drivers
for Brush Motors

H-bridge Drivers
Cross Reference

Find a ROHM product similar to the competitor product. Simply enter the part number and click the Search button.