News of 2008

News of 2007

News of 2006

News of 2005

News

News of 2007

The Industry's First HDMI ver.1.3a Switch IC Capable of 20m Transmission

08.31.2007
High-performance HDMI Switch IC BU16008KV

ROHM has developed the BU16008KV, a high performance three-input switch IC for digital TVs and multimedia monitors compatible with the newest HDMI standard, ver. 1.3a. Features include a built-in DDC buffer for ID signal display, an equalizer, a multiplexer, and a high-speed differential driver for highly reliable digital transmission during digital audio/video signal switching between digital source equipment and a digital TV or multimedia monitor. In addition, original RF circuit technology and optimized pattern layout have been utilized to integrate an equalizer capable of compensating for signal decay and degradation due to cables and connectors via high-precision impedance matching. As a result, high-quality transmission waveforms are possible - even during high-speed (2.25Gbps HDMI ver. 1.3a) audio/video communication through 20m long cable. The BU16008KV also integrates a bidirectional buffer  unprecedented in an HDMI switch IC  to protect against HDCP signal verification errors due to insufficient drive capacity in the DDC line. Set reliability is also improved due to an industry-best ESD resistance of 10kV (HBM).
Sample shipments will begin in September (sample price: 5.2US$), with mass production slated for November.


· Main characteristics of the BU16008KV

  1. Supports 1080p full HD with RGB 12-bit color depth
  2. HDMI ver. 1.3a-compliant 2.25Gbps high-speed transmission
  3. Built-in equalizer allows use of long cables
  4. DDC buffer integrated for HDCP communication
  5. 10kV (HBM) ESD resistance
  6. Easy-to-mount VQFP80 package (14mm × 14mm × max. 1.6mm)

· Glossary

  • HDMI (High-Definition Multimedia Interface)
    HDMI is the industry standard digital audio/video interface for television devices. Audio, video, and control signals are transmitted through one cable. HDMI ver. 1.3a increases transmission speed and increases color depth from 8 bits to 10 bits or more for improved image reproduction. It supports Blu-ray and HD DVD as well as uncompressed multichannel audio formats including Dolby True HD and DTS-HS. Compatibility is also provided for lip-sync functions for synchronizing audio and video.
  • HDCP (High-Bandwidth Digital Content Protection system)
    HDCP is a content protection system comprised of authentication and encoding protocols. If the display (TV) is not HDCP-compatible, HDMI video cannot be shown.
  • DDC (Display Data Channel)
    Standardized by VESA (Video Electronics Standard Association), DDC allows the acquisition of all types of attributes and automatic settings to match the capabilities of the display. An expanded version, DDC/CI (Command Interface), has bidirectional control capability.
  • Blu-ray Disc
    Jointly developed by nine companies, including Sony and Matsushita, Blu-ray is a rewritable high-capacity phase change optical disc. One of the 'next-generation' DVD standards, it features a capacity greatly surpassing that of current DVDs. Maximum recording capacity is 27GB, at a data transfer rate of 36Mbps.
  • Impedance matching
    Impedance matching is the practice of making the signal source and load impedances equal. If this is not performed high-speed waveforms cannot be correctly reproduced.
  • Full HD
    Regarding high-definition digital television (HDTV) broadcasts, full HD is the highest resolution format available, with at least 1080 effective scan lines. Generally 'full HD' compatibility indicates support for a resolution of 1920 × 1080 pixels.
  • Buffer
    A buffer is a circuit that compensates for differences in processing speed between communication lines, eliminating input/output interference.
  • Equalizer
    Longer cables result in proportional degradation of the digital signal, making it increasingly difficult to distinguish between ones and zeroes. An equalizer is a circuit that restores this degraded signal, so that subsequent digital blocks can correctly determine the digital value.
  • Multiplexer
    Multiplexing is the function of using a switch to select one signal from multiple signals. Required capabilities differ widely depending on frequency band and signal type (analog or digital).

Products HDMITM Switch LSI Series
Please do not hesitate to contact us if you need further information about the HDMI ver.1.3a Switch IC