News of 2008News of 2007News of 2006News of 2005 |
NewsNews of 2007The Industry's First High Intensity, High Dissipation White LEDs for Backlight and Illumination07.20.2007
ROHM has developed white LEDs in two types of high-intensity, high-radiation packages: PSML1 and PSML2. Developed as an alternative to CCFL (Cold Cathode Fluorescent Lamp) for backlight and illumination use in sets requiring relatively higher intensities, the products incorporate a novel high heat dissipation package in order to efficiently emit 7cd ? the highest in the industry ? using current in the medium range (50-150mA). Proprietary technology was utilized in order to solve the problems of excessive heat generation and low efficiency that have been plaguing mid-range LEDs by increasing the heat dissipation paths to the substrate and adopting an exposed copper frame with high thermal conductivity. The PSML1 features a heat dissipation of 70℃/W and the PSML2 60℃/W, life span is increased, and high temperature operation is possible with no degradation in light intensity or fluctuation in color. These characteristics make them ideal for any application requiring relatively high intensity backlights, such as car navigation systems, portable DVD players, illumination light sources, interior lighting, vehicle indicator displays, and gaming devices. Sample shipments began in July 2007 (sample unit price: 2US$) and mass production will begin in November 2007 with a monthly production of ten million units. · Major features of the PSML1/PSML2
· Glossary
|
||||