News of 2008News of 2007News of 2006News of 2005 |
NewsNews of 2006Ultra-high Performance, Low Power Dissipation SiC Power MOSFET03.10.2006
Kyoto, Japan - ROHM CO., LTD., has recently completed the development of a low power dissipation MOSFET using SiC (silicon carbide), a material whose characteristics make it more promising than silicon for use in high power devices. The newly developed SiC MOSFET can withstand voltages up to 900V and features an ON-resistance of 3.1mΩ/cm2 - currently the lowest in the industry. Power dissipation during conversion poses a significant problem in the power electronics field. SiC features greater thermal conductivity, electric field breakdown strength, and current density than Si, resulting in significantly lower power dissipation. ROHM has succeeded in decreasing the ON-resistance to 1/2 or less per unit area through utilization of novel technology. This has made it possible to reduce the required chip area by up to 2/3rds the original value, allowing SiC power components to be used in a wide variety of applications, such as household appliances, in-vehicle devices, and power transmission equipment, contributing to energy savings on a global scale. · Technology Features
· ApplicationsSiC power devices are suitable for power supplies and inverters that convert or control power. For example, they can be used to convert power to drive electric motors in energy-saving vehicles such as hybrid cars in order to reduce carbon dioxide emissions. In addition, their low power dissipation capability makes it possible to develop a wide variety of environmentally friendly products that contribute to energy savings on a worldwide scale. · BackgroundConventional Si-based power MOSFETs are problematic in that they cannot simultaneously satisfy four key characteristics required of switching components: high voltage resistance, low ON-resistance, high-speed switching, and high heat dissipation. However, the unique physical properties of SiC make it possible to develop products possessing characteristics that greatly exceed the performance of conventional Si power devices. ROHM's SiC MOSFETs not only satisfy all of the aforementioned requirements, but also feature high-temperature operation, contribute to increased miniaturization, and are resistant to radiation. · Glossary
IGBT is a power transistor that uses both electron holes and electrons for current flow, resulting in low ON-resistance. It combines the simple Gate drive characteristics of MOSFETs with the high current and low saturation voltage capabilities of bipolar transistors by combining an isolated Gate FET for the control input and a bipolar power transistor as a switch in a single device., High-speed switching operation, however, has been problematic due to the time required for the accumulation of electron holes. |